RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Digital Isolator Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 2747 subscribers
  • Views 5468 views
  • Users 0 members are here
  • digital isolators
  • adi
  • roadtest survey
Related

Seeking Your Interest in Roadtesting a Digital Isolator Board

rscasny
rscasny over 2 years ago

Hi All.

imageI had a call with one of suppliers who is interested in roadtesting one of its digital isolator boards. We have not done much with digital isolators in the roadtest program. But given the need for circuit isolation and the safety they provide, I wanted the community to roadtest this product. In addition, another reason was the learning experience the roadtesters can provide community members on this product.

Here is some basic information on this board:

The evaluation kits are designed to evaluate the MAX22563−MAX22566, a family of reinforced, six-channel, galvanic digital isolators in a 20-pin SSOP package.

Two types of evaluation boards are available:

  • The MAX22565CAEVKIT# is fully assembled and tested, and comes populated with the MAX22565CAAP+ (Not used in this roadtest)
  • The MAX2256XAEVKIT# is a generic board that has U1 unpopulated, allowing to select a device from the MAX22563−MAX22566 family. This is the kit that will be used for this roadtest. The MAX2256XAEVKIT# comes with U1 unpopulated and supports the following digital isolators: MAX22563BAAP+, MAX22563CAAP+, MAX22564BAAP+, MAX22564CAAP+, MAX22565BAAP+, MAX22565CAAP+, MAX22566BAAP+, and MAX22566CAAP+.

imageEquipment needed for roadtesting:

You need some test equipment to roadtest the MAX2256XA EV kit:
• MAX22563−MAX22566 device if U1 is unpopulated on EV kit. (The roadtester and I will get together to order the desired device needed.)
• Two DC power supplies with output range of 1.71V to 5.5V
• Signal/function generator
• Oscilloscope
Note: The EV kit should be powered from two independent isolated power supplies with nominal output voltage in the range from 1.71V to 5.5V. To evaluate the electrical parameters of the device without any isolation between the two sides, a single power supply can also be used.

Element14 would not provide the test equipment.

Roadtesters would need to have the bench equipment for this roadtest. If you are an electronic design engineer, you likely have access to most of these equipment. This seems like a lot to ask, and it is. But I think this is a valuable roadtest to offer the community. The reviews the roadtesters write would not only be good learning experiences, but would also provide customers more than a datasheet to select a digital isolator when the need arises. 

Here's some documentation on the board:

Datasheet
Manufacturer's page

For Additional Information

Here's a couple of polls for which to vote:



  • Sign in to reply
  • Cancel
  • ciorga
    ciorga over 2 years ago

    It looks to me that this product needs roadtesters specialized in signal integrity, power integrity, noise coupling, and high voltage isolation testing.  This work is very specialized and requires quite some effort and lab equipment.  I am asking myself what is the goal that the manufacturer has setup for this roadtest?  I bet the goal is not unboxing the product and setting up a signal that goes through from the input to output.  Is the goal exercising the specs limits or finding any bug in the product?  Does anyone know? 

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago

    Nice board ADI. Soldermask color? custom pantone please.

    image

    On rogers 4003.

    image

    image

    https://www.altium.com/viewer?token=0V%2BaOznrmkO2ry7Bs7xq46Su 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Andrew J
    Andrew J over 2 years ago in reply to rscasny

    Good oh.  An isolated DC/DC converted and a DC connector is only a few GBP as well so could be provided if needed I guess.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to Andrew J

    I am sure that the board can be tested in different ways. That's why I posted this pre-roadtest discussion, so you guys could hash it out. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to Andrew J

    Getting the roadtester a hot air gun along with the kit is not out of the realm of possibilities. And may be needed given the added task in this roadtest. Clearly, if a customert bought this board he/she would have to select and solder the chip onto the board, so it would be good to see it done in the roadtest and have the roadtester give some feedback on the level of difficult of the task. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 2 years ago in reply to misaz

    I see your point. But I also see why they "may" have chosen the MAX2256XAEVKIT#. The sponsor makes a range of these chips, so they likely hoped that different roadtests would use different U1s. In addition, if a customer purchased the X version, he would have to determine the chip he needed, which would make them study the sponsor's products more, which would be important to them. In other words, the X version requires more work and simulates the actual customer experience. That's my impression.

    Now, the key question is: can someone solder a 20-pin SSOP with the tools they currently possess? If I hear 'no' from everyone, then I'll have to go back to the sponsor and get the other version of the board. (I have the X versions of the board; I'll have to order the C version. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago

    My speed is a XR2206 signal generator and a USB scope. Good enough to play with, not enough to do a good test on corner points.  

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 2 years ago

    SMA connectors are not the most practical way to fit the hobbyist test bench. Perhaps geared toward a high end lab. In a modest home lab, I would expect the evaluation connecting an MCU and a peripheral, perhaps a serial port. So a simpler and pre-populated board with headers is a better fit.

    On the isolation voltage - most of our test benches do not have a way of having 50V or more to test the isolation. It’s another opportunity (and a risk) to get a supply that is going to 100V or so. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 2 years ago in reply to baldengineer

    I'm surprised that the AD2 and AD3 can't be powered just from the USB from a laptop, but it does seem that they are intended to be used with a separate 5V supply.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 2 years ago

    "Two DC power supplies..."

    Wouldn't a tester need a third to establish the voltage difference betwen the two sides? If you just let bench supplies float, small amounts of leakage will slowly pull the two sides together, and testing is then a bit meaningless.

    The MAX22563 can manage up to 200Mbps. So that also means a reasonably good oscilloscope and generator if you're going to look at the top end.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>