RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest in Roadtesting a Digital Isolator Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 2747 subscribers
  • Views 5470 views
  • Users 0 members are here
  • digital isolators
  • adi
  • roadtest survey
Related

Seeking Your Interest in Roadtesting a Digital Isolator Board

rscasny
rscasny over 2 years ago

Hi All.

imageI had a call with one of suppliers who is interested in roadtesting one of its digital isolator boards. We have not done much with digital isolators in the roadtest program. But given the need for circuit isolation and the safety they provide, I wanted the community to roadtest this product. In addition, another reason was the learning experience the roadtesters can provide community members on this product.

Here is some basic information on this board:

The evaluation kits are designed to evaluate the MAX22563−MAX22566, a family of reinforced, six-channel, galvanic digital isolators in a 20-pin SSOP package.

Two types of evaluation boards are available:

  • The MAX22565CAEVKIT# is fully assembled and tested, and comes populated with the MAX22565CAAP+ (Not used in this roadtest)
  • The MAX2256XAEVKIT# is a generic board that has U1 unpopulated, allowing to select a device from the MAX22563−MAX22566 family. This is the kit that will be used for this roadtest. The MAX2256XAEVKIT# comes with U1 unpopulated and supports the following digital isolators: MAX22563BAAP+, MAX22563CAAP+, MAX22564BAAP+, MAX22564CAAP+, MAX22565BAAP+, MAX22565CAAP+, MAX22566BAAP+, and MAX22566CAAP+.

imageEquipment needed for roadtesting:

You need some test equipment to roadtest the MAX2256XA EV kit:
• MAX22563−MAX22566 device if U1 is unpopulated on EV kit. (The roadtester and I will get together to order the desired device needed.)
• Two DC power supplies with output range of 1.71V to 5.5V
• Signal/function generator
• Oscilloscope
Note: The EV kit should be powered from two independent isolated power supplies with nominal output voltage in the range from 1.71V to 5.5V. To evaluate the electrical parameters of the device without any isolation between the two sides, a single power supply can also be used.

Element14 would not provide the test equipment.

Roadtesters would need to have the bench equipment for this roadtest. If you are an electronic design engineer, you likely have access to most of these equipment. This seems like a lot to ask, and it is. But I think this is a valuable roadtest to offer the community. The reviews the roadtesters write would not only be good learning experiences, but would also provide customers more than a datasheet to select a digital isolator when the need arises. 

Here's some documentation on the board:

Datasheet
Manufacturer's page

For Additional Information

Here's a couple of polls for which to vote:



  • Sign in to reply
  • Cancel
  • Andrew J
    Andrew J over 2 years ago

    Reminds me of this: /members-area/b/blog/posts/debugging-the-turing-welchmann-bombe

    They missed a trick by not providing an isolated DC/DC 5V voltage regulator to power both sides so only one supply is needed.  That would have been useful even for an evaluation board but if someone wanted to lump out for one to participate, they could jury rig a power input for a standard wall wart.  

    The roadtest could be achieved without a signal generator if it's possible for the tester to connect to a piece of equipment that doesn't share the same earth ground, like the Bombe.  It would need to generate fast signals to do the roadtest justice though.

    One other requirement for roadsters is of course the ability to solder a 20-pin SSOP package.  From the photo, the position looks accessible to get a soldering iron in, but hot air gun would probably be more useful.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 2 years ago

    I think the X kit without chip soldered is complication for RoadTest because it need RoadTester to have SMD soldering skills and can introduce several issues to board (cold joint, shorts, unconnected joints). It increases requirements on needed equipment even more and also some faults can affect board performance. MAX22563−MAX22566 differs in direction of channels. I think the MAX22565CAEVKIT with presoldered isolator with 5ch in one direction and 1ch in opposite direction is better choice for RoadTest. And if somebody for some reason need different channel configuration he/she can simply desolder the default chip efficiently turning kit to X variant and proceed with custom chip.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to baldengineer

    I have a mix of ground referenced and floating generators.

    This one is very handy: 

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago in reply to dougw

    There is no question that the Analog Discovery 2 and 3 are Earth-referenced. Nothing on either is isolated.

    The AD2's published schematics show that. (Digilent decided with the AD3 they would no longer share that information.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to baldengineer

    My Multicomp signal generator signals are definitely earth grounded. I am about to start a Digilent Analog Discovery 3 road test - I will check out its ground situation - running from a battery operated MS Surface. However I also have a hand held battery operated signal generator/scope that obviously is not connected to earth ground. I even have a hand held DVM that has some signal generator capability.

    Although I have enough equipment, I am still sorting out what I might learn from this road test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 2 years ago

    Are the outputs of signal generators generally isolated from Earth ground? I think I have always assumed they are Earth-referenced. If so, I suspect that's going to affect isolation results when the other side is connected to an oscilloscope. 

    If this becomes a test, I am going to have a strong interest in seeing the results!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<