RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Feedback -- Would You Be interested in Roadtesting a Bluetooth®︎5-capable Dev Board?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 2747 subscribers
  • Views 3866 views
  • Users 0 members are here
  • roadtester survey
Related

Seeking Feedback -- Would You Be interested in Roadtesting a Bluetooth®︎5-capable Dev Board?

rscasny
rscasny over 2 years ago

imageI am planning on running a roadtest on the following rapid development board for battery-optimized Bluetooth® 5 solutions with the MAX32666 Arm® Cortex®-M4 processor with FPU. The board also has a 6-axis accelerometer/gyro, RGB indicator LED, and pushbutton.

If you have the time, I'd appreciate you voting in the poll below. It helps me gauge interest and the number of kits needed.

Here is some documentation on the board:

MFR page: 
Datasheet: 
Video 

For More Info

RoadTester Poll

  • Sign in to reply
  • Cancel
Parents
  • embeddedguy
    embeddedguy over 2 years ago

    Yes, a good device it is.

    In Bluetooth, I think that Bluetooth SIG has already released standard 5.4. The bluetooth5 itself has several new features included than from previous one(Bluetooth 4). One of them is that it is capable of direction finding. There are basically two methods for direction finding AOA and AOD. Both require special antenna design requirements to be more accurate.

    This board in my understanding is similar to the one from SILabs that has EFR32 microcontrollers.

    www.silabs.com/.../thunderboard-gg12-kit

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 2 years ago in reply to embeddedguy

    It would be interesting to see someone blog about using BT5 in a direction-finding application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • misaz
    misaz over 2 years ago in reply to dougw

    Very hard to implement with Maxim MCU according to my experience. Open source BLE stack which they provide has very limited support for advanced features. Last year, they even removed text "supporting LE Audio, angle of arrival (AoA), and angle of departure (AoD) for direction finding" from MAX32655 datasheet (document rev. 2 has it, rev. 3 has not).

    I recommed setting goals lower. Working with such open-source stack is very hard and you will be happy when implementing basic GATT in less than 3 workdays (except running basic examples, of course). The minimalistics example has over 1700 lines of codes in multiple files, and it runs only basic build-in services.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • misaz
    misaz over 2 years ago in reply to dougw

    Very hard to implement with Maxim MCU according to my experience. Open source BLE stack which they provide has very limited support for advanced features. Last year, they even removed text "supporting LE Audio, angle of arrival (AoA), and angle of departure (AoD) for direction finding" from MAX32655 datasheet (document rev. 2 has it, rev. 3 has not).

    I recommed setting goals lower. Working with such open-source stack is very hard and you will be happy when implementing basic GATT in less than 3 workdays (except running basic examples, of course). The minimalistics example has over 1700 lines of codes in multiple files, and it runs only basic build-in services.