RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Your Interest In RoadTesting Ethernet or SMA Eval Kits
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 17 replies
  • Subscribers 2749 subscribers
  • Views 3364 views
  • Users 0 members are here
  • roadtester survey
Related

Seeking Your Interest In RoadTesting Ethernet or SMA Eval Kits

rscasny
rscasny over 2 years ago

Link to the second discussion. Click here

Hi All.

We've been talking with Broadcom about roadtesting one of their evaluation kits. Right now, two are being considered. I wanted to get your feedback and/or interest in roadtesting these peroducts. I also would like to know what are parts or equipment you would need to roadtest any of these products.

Let me briefly go through them. I have a poll at the bottom of this discussion.

imageEthernet Evaluation Kit

(AFBR-FSEK50B00E Gigabit Ethernet Evaluation Kit for the AFBR-FS50B00 Optical Wireless Transceiver)

The evaluation kit  for AFBR-FSEK50B00E gives the system designer a convenient means to evaluate the performance of the Optical Wireless Transceiver AFBR-FS50B00.

The evaluation kit includes:

  • Two PCBs with RJ-45 connector and IC BCM54210, which implements the functionality of a Media Converter
  • Two PCBs with Optical Wireless Transceiver AFBRFS50B00
  • One USB memory stick containing technical documentation.

The evaluation kit does not include:

  • CAT5 cables required for GbE communications between the evaluation kit and the user’s application.
  • Micro USB cables required for power supply.

Documentation

  • Datasheet

For More Information

SMA Evaluation Kit

imageBROADCOM AFBR-FSEK50B00S SMA Evaluation Kit, AFBR-FS50B00, Optical Wireless Transceiver, Wireless Communication
SMA Evaluation Kit for the AFBR-FS50B00 - 5 Gb/s

The Broadcom® AFBR-FSEK50B00S is an evaluation platform for the Optical Wireless Transceiver AFBR-FS50B00. The AFBR-FSEK50B00S evaluation kit provides the system designer a convenient means to evaluate the performance of the AFBR-FS50B00 optical wireless transceiver.

The evaluation kit includes:

  • Two PCBs with SMA connectors and AFBR-FS50B00 optical wireless transceiver
  • Two jumpers

The evaluation kit does not include:

  • Coaxial cables required for communication through the AFBR-FS50B00 optical wireless transceiver
  • Cables required to supply power to the boards included in the evaluation kit

Documentation

  • Datasheet

For More Information


About the Broadcom® AFBR-FS50B00 Transceiver

The Broadcom® AFBR-FS50B00 is a transceiver that communicates data over free space and thereby allows connector-less/cable-less
communication in a variety of applications. Full-duplex bidirectional communication, together with a small form factor, allows a compact system design. The device keeps full functionality over a 360° rotation around the optical axis, which reduces the complexity of alignment on the system level and allows the use in rotating systems. The component is designed to operate over a wide temperature range and with a potential data rate up to 5 Gb/s and a variable distance from 20 mm up to 100 mm. The AFBR-FS50B00, a Laser Class 1 product, is RoHS-compliant and is designed for SMT solderability standard processes

image

RoadTester Poll



  • Sign in to reply
  • Cancel
Parents
  • kmikemoo
    0 kmikemoo over 2 years ago

    While I'm interested, I don't have the skill set to do what I'm thinking - so I picked "not interested".  HOWEVER, for someone that does have the skill... 

    My scenario is the USB control connection between a HF radio and laptop computer.  The setup uses a SDRUno and the laptop runs SDRPlay software.  The radio is a Kenwood TS-590.  The laptop screen is projected onto a larger screen so more people (ideally visitors) can see what is going on.  If we use a cheap USB cable to connect the radio to the laptop, the software crashes when we key the microphone.  The USB cable that works is higher quality and has ferrite chokes on each end.  With optical isolation, would the quality of the USB cable matter?
    Just thinking out loud. Relaxed

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • kmikemoo
    0 kmikemoo over 2 years ago

    While I'm interested, I don't have the skill set to do what I'm thinking - so I picked "not interested".  HOWEVER, for someone that does have the skill... 

    My scenario is the USB control connection between a HF radio and laptop computer.  The setup uses a SDRUno and the laptop runs SDRPlay software.  The radio is a Kenwood TS-590.  The laptop screen is projected onto a larger screen so more people (ideally visitors) can see what is going on.  If we use a cheap USB cable to connect the radio to the laptop, the software crashes when we key the microphone.  The USB cable that works is higher quality and has ferrite chokes on each end.  With optical isolation, would the quality of the USB cable matter?
    Just thinking out loud. Relaxed

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 2 years ago in reply to kmikemoo

    Hi Mike,

    Isolation would definitely help. I'm wondering, if the root cause could be absence of a balun on the antenna end of the SDRuno. It could be worth upgrading the balun (or string a load of ferrites on that antenna cable). Otherwise, ferrites on the USB cable at a minimum would be needed (might be worth adding a couple more, just to be on the safe side).