RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Feedback on Your Interest in Roadtesting a Battery Fuel Gauge Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 2749 subscribers
  • Views 3330 views
  • Users 0 members are here
  • roadtester survey
  • Nordic Semi
  • nPM Fuel Gauge board
Related

Seeking Feedback on Your Interest in Roadtesting a Battery Fuel Gauge Board

rscasny
rscasny over 2 years ago

imageI have a sponsor interested in roadtesting its Fuel Gauge board. I'd like to get your interest. I've added some background information and documents to review.

Here's some info about the board:

The nPM Fuel Gauge board (nPM FG) connects to a compatible Nordic Semiconductor evaluation kit. The purpose of the board is to act as a constant current sink device during battery profiling with nPM PowerUP desktop software. The battery model generated in nPM PowerUP can be used for evaluation of fuel gauge in nPM PowerUP and exported as an include file for use in any application using the Nordic Fuel Gauge algorithm. To use the nPM Fuel Gauge board you also need the nPM1300 Evaluation Kit, which would be provided to you.

Here's some documentation:

Fuel Gauge Hardware

RoadTester Poll

Thanks for participating in element14's programs!

  • Sign in to reply
  • Cancel
Parents
  • rsc
    rsc over 2 years ago

    I'd be more interested in a product that would work in amps instead of mA.  My batteries are much larger, the last LiFePO4 I purchased was 100Ah.

    Something I could use would be for quadcopter or UAS batteries.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate over 2 years ago in reply to rsc

    Check out the MAX17261, I used it without any characterization and it works relatively well like that. Not sure what the highest capacity it can handle is, it might be 65535mAh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vmate
    vmate over 2 years ago in reply to rsc

    Check out the MAX17261, I used it without any characterization and it works relatively well like that. Not sure what the highest capacity it can handle is, it might be 65535mAh.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • vmate
    vmate over 2 years ago in reply to Jan Cumps

    Max capacity and chemistry type only

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 2 years ago in reply to vmate

    Did you give it the theoretical datasheet parameters of your battery?