RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Seeking Feedback on Your Interest in Roadtesting a Battery Fuel Gauge Board
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 20 replies
  • Subscribers 2749 subscribers
  • Views 3334 views
  • Users 0 members are here
  • roadtester survey
  • Nordic Semi
  • nPM Fuel Gauge board
Related

Seeking Feedback on Your Interest in Roadtesting a Battery Fuel Gauge Board

rscasny
rscasny over 2 years ago

imageI have a sponsor interested in roadtesting its Fuel Gauge board. I'd like to get your interest. I've added some background information and documents to review.

Here's some info about the board:

The nPM Fuel Gauge board (nPM FG) connects to a compatible Nordic Semiconductor evaluation kit. The purpose of the board is to act as a constant current sink device during battery profiling with nPM PowerUP desktop software. The battery model generated in nPM PowerUP can be used for evaluation of fuel gauge in nPM PowerUP and exported as an include file for use in any application using the Nordic Fuel Gauge algorithm. To use the nPM Fuel Gauge board you also need the nPM1300 Evaluation Kit, which would be provided to you.

Here's some documentation:

Fuel Gauge Hardware

RoadTester Poll

Thanks for participating in element14's programs!

  • Sign in to reply
  • Cancel
Parents
  • Anthocyanina
    Anthocyanina over 2 years ago

    i am interested, but this is completely new to me, i don't know if i'm missing something, but, is fuel gauge in this context referring to measuring the remaining capacity of a battery?(this without having looked at the datasheet or anything, just from the title and quick read of what Randall wrote) or is this something to do with fuel as in combustible fuel? this being something new to me is a big part in why i'm interested, tho i'm not sure how interested would nordic be in having a newbie roadtest this without any prior knowledge!

    edit: now having read more on this board, i'm definitely interested in applying. after my bike's battery died, i've been manually characterising the individual cells in what's been a very tedious process to try to rebuild the battery itself. It would be cool to see how this board does it, even if it's for much lower capacity batteries than a bike's

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Anthocyanina
    Anthocyanina over 2 years ago

    i am interested, but this is completely new to me, i don't know if i'm missing something, but, is fuel gauge in this context referring to measuring the remaining capacity of a battery?(this without having looked at the datasheet or anything, just from the title and quick read of what Randall wrote) or is this something to do with fuel as in combustible fuel? this being something new to me is a big part in why i'm interested, tho i'm not sure how interested would nordic be in having a newbie roadtest this without any prior knowledge!

    edit: now having read more on this board, i'm definitely interested in applying. after my bike's battery died, i've been manually characterising the individual cells in what's been a very tedious process to try to rebuild the battery itself. It would be cool to see how this board does it, even if it's for much lower capacity batteries than a bike's

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 2 years ago in reply to Anthocyanina

    There's a blog post here for a different fuel gauge chip, it contains some general info about fuel gauges, which might help understand what they are, and some example ways they can operate:

    MAX17260GEVKIT# Fuel Gauge EVM - Review

    That was a very good fuel gauge chip, and the approach it took, was to perform all the calculations on-chip, and doesn't require (significant) up-front configuration, apart from a few basic parameters about the battery, mostly derivable from battery datasheets.

     The Nordic chip takes a different approach from what little I've read; it doesn't perform the fuel gauge algorithm on-chip, instead, it relies on the connected microcontroller to do it, using a Nordic-supplied technique. That's no bad thing, since it means that their algorithm could be improved over time perhaps! It also requires some information up-front about the battery, and that information seems to be derived using that nPM Fuel Gauge Board. That may mean that the Nordic method is more accurate, but the Maxim algorithm has already set quite a high bar (typically, the Maxim method seems to be accurate to within a few percent), so it will be interesting to see what performance people achieve from the Nordic method. Even if the accuracy turned out to be lower, that doesn't make that feature useless. Lots of use-cases do not require extreme precision. There's a price-performance mix. And the Nordic chip does other features for a similar price to the single-purpose Maxim chip for example. 

    Another point is that the Nordic chip is actually marketed as a PMIC, the fuel gauge feature is just one of the functions that it happens to support. All the PMIC features of the chip and the low-cost, are very compelling. The fuel gauge feature is (extremely welcome) icing on cake, and it will be interesting to see it in operation with different batteries, and seeing if the Nordic code can run on any microcontroller or if there is some issue (e.g. licensing).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vmate
    vmate over 2 years ago in reply to Anthocyanina

    Fuel gauges are the thing that give you the battery charge percentage from past and present voltage/current readings. The characterization mentioned here is only for making sure the percentages it gives back are accurate, this isn't a general purpose tool for working with batteries. It also has a capacity limit of 3000mAh.

    Turns out giving an accurate percentage is really really difficult, so manufacturers don't like sharing how they did it.