RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum re: Seeking to Determine Who Will Enroll in SMA or Gigabit Ethernet Evaluation Kits
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 2663 subscribers
  • Views 1430 views
  • Users 0 members are here
  • roadtest survey
  • broadcom
Related

re: Seeking to Determine Who Will Enroll in SMA or Gigabit Ethernet Evaluation Kits

rscasny
rscasny over 1 year ago

imageMonths ago, I ran a discussion on roadtesting these kits:

  • BROADCOM AFBR-FSEK50B00S SMA Evaluation Kit
  • BROADCOM AFBR-FSEK50B00E Gigabit Ethernet Evaluation Kit

Here's the link to the original discussion. Click here

We are now at the decision point, whether to roadtest these kits if there is the interest or not.

The kits have a significant price, thus, the sponsor is making a considerable investment.

QUESTION: if you are interested in enrolling in the roadtest of these products, please leave a comment and I'll contact you.

Thanks.

Randall Scasny

imageRoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • saadtiwana_int
    saadtiwana_int over 1 year ago +1
    Hi, I was one of the commenters on the original discussion. My primary interest is in testing the kit to build an optical slip ring, since doing the same with fibers and traditional optics is quite difficult…
  • dougw
    dougw over 1 year ago in reply to saadtiwana_int +1
    I would be very interested to see how well the slip ring concept works.
Parents
  • JWx
    JWx over 1 year ago

    Hello!

    Is there a decision which one is going to be roadtested (Ethernet or SMA)?

    I think it is an interesting subject - the copper Gigabit Ethernet seems easier to test, but the results could be somewhat limited by copper PHY media converters. I have (long time ago) done a project about the possibility of use Gigabit Ethernet in High Performance Cluster interconnects in place of Infiniband (which provided significantly lower propagation times - there was no RDMA over Ethernet possibilities then - but was very expensive).  

    During my work I have started to wonder if copper Gigabit Ethernet physical interface introduces some additional delay - these times I was unable to find any solid information about this, but today it is clearly present in the Ethernet switch documentation (this one from one model of Netgear - different models may have different values, maybe it is also dependent on the chipset used):

    Latency (64-byte packets)
    1G Copper < 3.5us
    1G Fiber < 2.5us

    which difference may (or may not) introduce some artificial limit for the evalkit

    I think that SMA version can be tested (at hobbyist level of lab) using some sort of passive DAC (TWINAX) cable breakout (copper cable connecting two SFP sockets - commonly used for optical interfaces, thus probably directly connecting TX and RX pairs) and two Gigabit Ethernet switches - but the signalling level should be verified. At first glance it seems compatible, but only after about of hour of research.

    On the other hand, evalkit complete with Gigabit Ethernet media converters can be tested as optically isolated Gigabit Ethernet link - something very desirable to all kinds of Extreme Environment type scenarios (if power consumption is reasonable and it can work through the typical transparent lid [or dirty transparent lid] - but this remains to be tested)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • JWx
    JWx over 1 year ago

    Hello!

    Is there a decision which one is going to be roadtested (Ethernet or SMA)?

    I think it is an interesting subject - the copper Gigabit Ethernet seems easier to test, but the results could be somewhat limited by copper PHY media converters. I have (long time ago) done a project about the possibility of use Gigabit Ethernet in High Performance Cluster interconnects in place of Infiniband (which provided significantly lower propagation times - there was no RDMA over Ethernet possibilities then - but was very expensive).  

    During my work I have started to wonder if copper Gigabit Ethernet physical interface introduces some additional delay - these times I was unable to find any solid information about this, but today it is clearly present in the Ethernet switch documentation (this one from one model of Netgear - different models may have different values, maybe it is also dependent on the chipset used):

    Latency (64-byte packets)
    1G Copper < 3.5us
    1G Fiber < 2.5us

    which difference may (or may not) introduce some artificial limit for the evalkit

    I think that SMA version can be tested (at hobbyist level of lab) using some sort of passive DAC (TWINAX) cable breakout (copper cable connecting two SFP sockets - commonly used for optical interfaces, thus probably directly connecting TX and RX pairs) and two Gigabit Ethernet switches - but the signalling level should be verified. At first glance it seems compatible, but only after about of hour of research.

    On the other hand, evalkit complete with Gigabit Ethernet media converters can be tested as optically isolated Gigabit Ethernet link - something very desirable to all kinds of Extreme Environment type scenarios (if power consumption is reasonable and it can work through the typical transparent lid [or dirty transparent lid] - but this remains to be tested)