RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
RoadTest Forum Are you interested in RoadTesting NXP's S32K312MINI-EVB Evaluation Board for Automotive General Purpose ?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 2744 subscribers
  • Views 1154 views
  • Users 0 members are here
  • RoadTest
  • S32K312MINI-EVB
  • nxp
Related

Are you interested in RoadTesting NXP's S32K312MINI-EVB Evaluation Board for Automotive General Purpose ?

cstanton
cstanton over 1 year ago

image

The blurb:

The S32K312MINI-EVB is an evaluation board for general-purpose industrial and automotive applications.

Based on the 32-bit Arm®Cortex®-M7 S32K3 MCU in a 172 HDQFP package, the S32K312MINI-EVB offers a single core mode, HSE security engine, OTA support, advanced connectivity and low power.

The S32K312MINI-EVB offers a standard-based form factor compatible with the Arduino® UNO pin layout, providing a broad range of expansion board options for quick application prototyping and demonstration.

Details:

https://www.nxp.com/design/design-center/development-boards-and-designs/S32K312MINI-EVB

  • Sign in to reply
  • Cancel
Parents
  • veluv01
    veluv01 over 1 year ago

    Interesting evaluation board for some AUTOSAR applications and it has MATLAB support too! Including the Motor Control Shield and CAN/LIN Communications Expansion Board would be preferable for testing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 1 year ago in reply to veluv01

    The data sheet says it has CAN and LIN BUS onboard already.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rsc
    rsc over 1 year ago in reply to veluv01

    The data sheet says it has CAN and LIN BUS onboard already.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dang74
    dang74 over 1 year ago in reply to veluv01

    Ah so you have the spirit of the 'put it through its paces' crowd but may have voted 'I'd need some parts.'

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • veluv01
    veluv01 over 1 year ago in reply to rsc

    Yes but having additional channels allows to test by segmenting the bus, having no congestion? It also has some FLEXCAN connected to CAN's PHY making it effective to manage the bus so having more than one bus may help to test it?