RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest This Wireless Power Dev Kit?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 28 replies
  • Subscribers 2761 subscribers
  • Views 4405 views
  • Users 0 members are here
  • scasny
  • wurth electronik
  • rohm
  • dev kit
  • 760308mp
  • wireless power
  • energy_power
Related

How Would You RoadTest This Wireless Power Dev Kit?

rscasny
rscasny over 9 years ago

I'm often contacted my suppliers who are considering to participate in the RoadTest program. They ask me a lot of questions about the program and which products are the best to RoadTest. Well, it depends, right? Test equipment garners a lot of interest. So do SBCs or anything to do with IoT. So when I was contacted about this Wireless Power Dev Kit for a future RoadTest, I looked up what content the community already had on the topic. There is a some content, as expected, since wireless power solutions are only sure to grow. But I don't recall doing a RoadTest on this type of product, or at least recently. I just wondered how it would be RoadTested. So, here's my question: How would your Roadtest it?image

 

Here's a few facts about the product:

  • It's the result of the joint collaboration of Wurth Elektronik and Rohm Semiconductor.
  • It's used in devices with a large number of mating cycles to avoid connector damage such as smartphones, tablets, portable media players.
  • It comes with 5 parts: Transmitter module, Receiver module, LED load module, Quick start guide, Power adapter with EU, US and UK adapter.

 

Here's a few specs:

  • Plug & play wireless power design kit, medium power solution
  • Qi standard version 1.2 compliant with extended power profile
  • Based on the transmitter type MP-A7
  • Excellent performance due to use of litz wire coil
  • Operating temperature range from -20°C up to +105°C
  • Inductance of 12µH at 125KHz/10mA, Q-factor of 33 at 125KHz/10mA
  • Maximum rated current of 3A at ΔT = 40K, saturation current of 6A (typ)

 

More Information

Datasheet

Product Info

 

Here's a few More Photos:

image

 

image

 

image

  • Sign in to reply
  • Cancel
  • hlipka
    hlipka over 9 years ago in reply to DAB

    In the 'beyond the phone' challenge I build a charger for a remote controlled toy car, based on the predecessor of this kit. Being able to transfer a lot of energy of larger distances (and even when the receiver is not placed perfectly on the transmitter) was quite important there. This would be something to test - under which circumstances (distance, orientation, displacement, materials in-between) can you still get a reasonable amount of energy transferred? Can you really transfer 15W without heat problems (the manual says it does only 10W out-of-the-box and must be modified for 15W, tough)?

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 9 years ago

    Hi Randall,

     

    There was an interesting idea that Monty Chan (aka COMPACT) had during the first wireless road test that I thought was interesting.

     

    He did some testing by doing some remote charging through a glass window.

     

    That got me thinking about using the device to charge IOT devices, both inside and outside the house by just putting the charger up to the window to access the coil on the IOT device.

    You could do this with cameras, microphones, PIR sensors, night lights, and all types of sensors.

     

    So how about an remote IOT device charging challenge?

    People could identify the IOT device, where it is remotely located and how it could benefit from periodic wireless charging.

     

    Could be fun.

     

    DAB

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 9 years ago

    Mix and match testing is definitely the way to go. I'm sure the paired kit works well and the designers have published their own accurate and detailed specs. There's not really much benefit just repeating this.

     

    What really matters is how interoperable it is. I've got two Qi chargers and 4 devices - including a couple of Nook eReaders that have had a cheap eBay receivers hacked in. This is the reality of how these devices have to work.

     

    It might be interesting to see if it could be combined with NFC or whether the two would interfere with each other. I can't actually think of a good use case right now but it sort of seems logical to be charging a device and communicating with it at the same time. Maybe a data logger that's being recharged and uploading data at the same time?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 9 years ago in reply to mcb1

    Thanks Mark. It looks like e14 did it back in 2014.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago

    I've done quite a bit of work with Qi charging systems, and have a variety of both transmitters and receivers and devices I built that charge this way.

    This looks like a quality implementation.

    I would investigate performance of this system relative to others I have on hand, and mix and match performance with other devices.

    The "extended power profile" is intriguing - I would like to explore its performance.

    That said, I would likely let others tackle this road test - I have enough experience with Qi that more investigation is not a high priority.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ipv1
    ipv1 over 9 years ago

    This is an upgrade to the kit we got for the BeyonD the Phone and how. Some of us received some coils to make our own circuits and it was fun. Maybe someone could use variable coil sizes and do an analysis on the efficiency and how the circuit should be changed or remain the same.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    We did a Design Challenge using the Wurth branded version called Beyond the Phone.

    Wireless Power - Beyond the Phone

     

    It was a great eye opener to the capabilities of wireless power and Wurth were a really great supplier who went above an beyond during the challenge.

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • WarrenW
    WarrenW over 9 years ago

    I would use my Samsung S7 high rate charger physically connected to the phone (from a discharged state) and measure the charge time and rates, then compare this using the same charger via the wireless again with time and rate results.

     

    This should give a real world comparison of the efficiencies of the wireless system.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<