RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Are You Ready To Build A Project with the Pocket IO? I Got 5 to Giveaway
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 2755 subscribers
  • Views 2818 views
  • Users 0 members are here
Related

Are You Ready To Build A Project with the Pocket IO? I Got 5 to Giveaway

rscasny
rscasny over 9 years ago

Back in April, I wrote a blog asking the community what they would build with the PocketIO from Maxim Integrated. Some people responded.

 

image

 

Now, I've learned I am getting 5 of them. And the supplier would like to sponsor 5 projects.

 

If you are still interested and are available, please comment below.

 

If you didn't suggest a project in the original blog, please provide me some idea of what you would build. A summary of the project.

 

For technical information on the Pocket IO, go here.

 

Thanks.

 

Randall

  • Sign in to reply
  • Cancel
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    End of life for a key component in your system sucks. Which is why industry standards and having parts from multiple suppliers is important.

    They could be in exactly the same situation with a Pi compute module as there are no alternatives with the same pinout.

    There is the 96board standard but in the small form factor there are only 2 boards from Seeed so you'd still be in that single supplier situation.

    https://www.96boards.org/products/ie/

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to Workshopshed

    Edison was a really convenient module, I don't know of any easily-available computer for embedding at that size that runs full Linux and has wireless : ( It is really unfortunate it is end-of-sale. The next-nearest seems to be the Beaglebone system-in-packages, but they require a separate wireless module, or the Pi compute module, but both of these options are still a fair bit larger and as you say no similar pinout.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago in reply to shabaz

    Ah yes I'd forgotten about the Beaglebone SOC, also I suppose there are things like the Atheros "Wi-Fi System-On-Chip (WiSoC)" that are used in the Yun. I don't know if there is any standardisation of pins on those kind of modules.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 9 years ago in reply to shabaz

    Ah yes I'd forgotten about the Beaglebone SOC, also I suppose there are things like the Atheros "Wi-Fi System-On-Chip (WiSoC)" that are used in the Yun. I don't know if there is any standardisation of pins on those kind of modules.