RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest Reviews: A Discussion About The Rating System
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 2669 subscribers
  • Views 2592 views
  • Users 0 members are here
  • scasny
Related

RoadTest Reviews: A Discussion About The Rating System

rscasny
rscasny over 8 years ago

For any RoadTest Review, the reviewer not only provides his or her personal take on the product being reviewed but also a numbered ranking (10-point scale) for 6 different questions.

 

Here is a random example:

 

image

My gut feeling is that  I haven't clarified well enough what the 10-point scale means. As a result, there may be a lack of certainty when giving a grade. In addition, a lot of RoadTesters grade these questions in similar ways. So, I'd like to revisit our grading system. To start here's my idea:

 

  • 10 points: Outstanding
  • 9 points: Very Good Satisfaction
  • 8 points: Good Satisfaction
  • 7 points: Adequate but had to work through some programs
  • 6 points: Needs Work
  • 5 points  Barely Satisfactory
  • 4 points: Below Average
  • 3 points: Unsatisfactory
  • 2 Points:Totally Unsatisfactory
  • 1 point: Time to Rethink

 

I'd like to get the RoadTester Group's opinions on the rating system. Do you think it needs more clarification? Keep it the way it is?

 

Go ahead and suggest your own. Perhaps the problem is that we need to ask different questions?

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 8 years ago +4
    rscasny It's great that there is a guideline as some reviews are marked high, but the comments would suggest otherwise. Likewise we've seen low marks with nothing to substantiate why they are low. IMO…
  • dougw
    dougw over 8 years ago +3
    I always do a lot of homework to find out as much as I can about the product before applying for a road test and I won't apply if I don't think it will be enjoyable and useful. It would be rare for me…
  • michaelkellett
    michaelkellett over 8 years ago +3
    I would be in favour of dropping the rating to 5 stars. 5 much better than expected 4 better than expected 3 about what I expected 2 worse 1 a lot worse 0 dreadful but I note that where 5 stars are used…
  • Workshopshed
    Workshopshed over 8 years ago in reply to michaelkellett

    I agree, "Exceeds expectations" should be an possibility.

    But I would want the middle option to be a "it's ok", "can be used but does not fill me with joy"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • gecoz
    gecoz over 8 years ago in reply to michaelkellett

    Hi Michael,

    Perhaps I didn't explain myself well. Although I can see where you are coming from, and in principle I agree with you, my point was about what is in place now and how it is used. Unfortunately when you look around, just about all the star rating systems use the top rating for meeting expectation, and any less of a 5 rating is interpreted as somehow negative. Element14 could do differently, and use the "exceed" expectation for the 5 star, but by doing so it would generate ambiguity in the valutation, as a product meeting all the expectation would have to score only a 4 star.

    I suppose what I'm trying to say is when choosing a rating system, I think we should take into account how people are using other feedback systems out there, so that the system is more familiar and the valutation is less susceptible of interpretation.

    Fabio.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to gecoz

    I agree that being different from other systems could be  a problem - perhaps we shouldn't use stars but some other symbol ..........

     

    It is very tricky - in the end one has to read the text to get a real understanding of what the reviewer intends.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 8 years ago in reply to michaelkellett

    Perhaps

     

    ΩΩΩ

     

    or

     

    imageimageimage

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to michaelkellett

    I too consider the top score as more of 'delights the customer' rather than 'no room for improvement', because technology always evolves.

    There are cultural differences too, for example I sometimes see the 5-point scoring results for presentations, and invariably the score is higher presented in the US, whereas it is always slightly lower in Europe. Or there is the one mean person who scores 1/5 for everything because they attended the wrong presentation for them, and the others scored 5/5 : ) So the 5 points or stars means something different depending on the audience. With the product reviews some are scored extremely low but then it becomes apparent from the text that the user didn't apply the product to the same use-cases as expected, or had some difficulties which are unique to him/her and would not generally apply to that product, e.g. faulty item.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 8 years ago

    I tend to agree with the comments that having an "exceed" or "surprise and delight" option is a good idea as that gives balance (i.e. upside and just downside).

     

    However, I would suggest maybe rephrasing some of the questions to make it clearer or have an intro explaining how scoring should be carried out.

     

    So for example "Product performed to expectations" should be rephrased to something like "Degree to which product exceeded or failed to perform to expectations". The "Degree to which..." is now the key focus in the scoring and this part is now common to all questions and could be used as header, or something similar.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 8 years ago

    Hi Randall,

     

    When we evaluated proposals we used a simple color code.

    Red = Did not meet requirements.

    Yellow = Met part of the requirements.

    Green = Met requirements.

    Blue = Exceeded requirements.

     

    This system made it easy to summarize everyone's review and come up with a consensus rating for each item.

     

    Only after this process was the cost evaluated as only the green proposals were considered.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 8 years ago in reply to ninjatrent

    Sometimes documentation is provided but at the quality they might as well have left it out as the feeling you get from such bad documentation is worse than no documentation at all..

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gpolder
    gpolder over 8 years ago in reply to kas.lewis

    using the system I propose:

    image

    lacking communication is not counted while bad communication has a negative influence on the total score.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<