RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum RoadTest Preview: Yes, We Will RoadTest the New ULINKplus Debug and Trace Unit. HURRAH!
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 2751 subscribers
  • Views 997 views
  • Users 0 members are here
  • scasny
Related

RoadTest Preview: Yes, We Will RoadTest the New ULINKplus Debug and Trace Unit. HURRAH!

rscasny
rscasny over 8 years ago

Early last summer, I created a discussion regarding the ULINKplus Debug and Trace Unit and quite a few members joined in and offered their thoughts.

 

For those of who didn't have the opportunity to join in that discussion, I've created a new ones with two great pieces of news.image

 

Here's the brief on the product:

 

The ULINKPLUS from ARM is a an innovative universal debug/trace adapter. It enables test automation, software optimization for ultra-low power applications and isolation for high speed debug and SWV trace of sensitive hardware systems.The compact enclosure allows usage in harsh environments and provides standard target connectors for JTAG, power measurement and general purpose I/O. It connects users PC's USB port to their target system. It allows to program, debug and analyse applications and their power consumption using its outstanding power measurement technology. ULINKplus together with MDK provides extended on-the-fly debug capabilities for Cortex-M devices. A unique feature of ULINKplus is the power measurement capability. It utilizes two high precision 16bit sigma-delta A/D converters with 20MHz sample rate for high signal/noise ratio. This is essential for debugging applications such as motor control, power converters or systems with sensitive analogue processing.

 

It has some great features, such as:

 

Here's some specs:

  • Wide target voltage range: 1.2V - 5.5V
  • Electrical isolation from the target system is integrated up to 1 kV
  • USB 2.0 High-Speed connection using the CMSIS-DAP debug protocol
  • USB powered (no power supply required)
  • 10-pin (0.05") - Cortex Debug Connector
  • Hot-plugging to running targets

 

Devices Supported:

  • JTAG support for ARM Cortex processors
  • Serial Wire Debug (SWD) support for all ARM Cortex-M processors
  • Serial Wire Viewer (SWV) support for all ARM Cortex-M processors

 

Here's some more information to learn about the ULINKplus:

 

ULINKplus Overview

ARM blog on the ULINKplus

 

Great News #1: The Webinar

There's a webinar on the ULINKplus on Nov 30th. You can go here to sign up.

 

Great News #2: The RoadTest

We will be roadtesting this product. I will be setting up the RoadTet page soon after I receive the product so stay turned.

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • jlangbridge
    jlangbridge over 8 years ago

    Hey, that's great news! I love the exception view, and seeing the systicks. Awesome work, Randall! I'm sure everyone here is as excited as I am to see what happens (and to get a shot at roadtesting it ourselves!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jlangbridge
    jlangbridge over 8 years ago

    Hey, that's great news! I love the exception view, and seeing the systicks. Awesome work, Randall! I'm sure everyone here is as excited as I am to see what happens (and to get a shot at roadtesting it ourselves!)