RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum In Search of RoadTesters to Take On The All Programmable SoC (AVNET MiniZed RoadTest)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 2759 subscribers
  • Views 4283 views
  • Users 0 members are here
  • scasny
Related

In Search of RoadTesters to Take On The All Programmable SoC (AVNET MiniZed RoadTest)

rscasny
rscasny over 8 years ago

I'm in search of a few more roadtesters who would like to experiment with the Avnet MiniZed board.

 

What do you need?

 

1. Got to be Clever.

2. Inventiveness Helps

3. A Thirst for Learning

4. A love for Electronics

5. A Wish to Say "Hello World"

6. Beauty is not a requirement

7. A knack for tinkering is preferred

8. The ability to enter into the world of FPGA SoCs are pure magic.

9. A Messy Benchtop

10. A devotion to new technology. That's music to our ears.

 

image

 

(Here's something you should know about the MiniZed: "The board aims to showcase the power of Zynq, where the Cortex A9 processor core integrates seamlessly with the programmable fabric to provide signal

processing and control solutions."

 

Sign Up for the RoadTest Here: AVNET MiniZed

  • Sign in to reply
  • Cancel
Parents
  • reinouddelange
    reinouddelange over 8 years ago

    Randall,

     

    I just browsed a bit through the Zynq book (but it's a lot 484 pages), and I wondered how you use that thing...

     

    Is it like a raspberry pi and can you run python code on it? Or is it more like an Arduino and you'll need an IDE for it? How does this device compare to the previous mentioned platforms?

     

    It looks nice, but up to now I don't know what to do with it.

     

    kind regards,

     

    Reinoud

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kas.lewis
    kas.lewis over 8 years ago in reply to reinouddelange

    Its an FPGA... So no not Arduino or Raspberry Pi. This you need to implement the digital logic. Therefore everything runs in hardware and not software making the overall system run alot faster as well as having the ability to run multiple threads truly simultaneously not using time division or anything like that. This is a very different beast. FPGAs powerful, efficient but a whole different world when it comes to programing.

     

    Kas

     

    Disclaimer, this is based om my basic understanding of FPGAs and not from any indepth understanding or usage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kas.lewis
    kas.lewis over 8 years ago in reply to reinouddelange

    Its an FPGA... So no not Arduino or Raspberry Pi. This you need to implement the digital logic. Therefore everything runs in hardware and not software making the overall system run alot faster as well as having the ability to run multiple threads truly simultaneously not using time division or anything like that. This is a very different beast. FPGAs powerful, efficient but a whole different world when it comes to programing.

     

    Kas

     

    Disclaimer, this is based om my basic understanding of FPGAs and not from any indepth understanding or usage.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • awneil
    awneil over 8 years ago in reply to kas.lewis

    kas.lewis  wrote:

     

    Its an FPGA... So no not Arduino or Raspberry Pi. This you need to implement the digital logic.

    Actually, it's an FPGA plus a microprocessor (Cortex-A); so that's like having a Raspberry-Pi plus an FPGA - but all in one chip.

     

    everything runs in hardware and not software

    Because it is an FPGA plus a Cortex-A, you can have some stuff running in software plus some stuff in the hardware!

     

    image

     

    The downside is that you have to learn the software development environment plus the hardware development environment plus how to stitch it all together!

     

    None of those is trivial on its own - doing all 3 at once is, as noted, a very large task!

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • awneil
    awneil over 8 years ago in reply to hlipka

    hlipka  wrote:

     

    FPGA are not the kind of devices you program in software.

    Ha ha - so now we get into a deep, philosophical argument about what "software" is ... !!

     

    image

     

    It is "software" in the sense that you write "source code" in a "language" (eg, VHDL) which gets "compiled" and then loaded into the FPGA to define its operation.

     

    But it is nothing like the kind of software you write to run on a processor.

    It is not a sequence of instructions that a processor follows, one after the other; rather, it is a definition of the hardware itself.

     

    You could actually create a processor in the FPGA, and then have that processor run "conventional" software that you write for it...

     

    image

     

    As already noted, this particular FPGA also has an actual microprocessor ready-made and built-in.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 8 years ago in reply to jlangbridge

    Just opened it with FF57, and it worked fine. Any plugins which might cause this (e.g. NoScript)?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 8 years ago in reply to reinouddelange

    FPGA are not the kind of devices you program in software. They are no CPUs or MCUs. These are devices where you can create the hardware you need, and then it interacts with the software on a CPU (e.g. via I2C or SPI or UART). Vivado is the tool you need to program the hardware, and you define your hardware in e.g. Verilog or VHDL (which kind of look like a program, but this is very misleading).

    If you never did something like that before (or worked with e.g. the programmable hardware in a Cypress PSoC), then a FPGA roadtest will have a steep learning curve. It could be better to look at the CPLDs from Xilinx (e.g. you can get rather cheap boards with the XC9572XL), which are programmed by Xilinx ISE. And there you can also define your hardware as a schematic which might be easier to understand at the beginning.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jlangbridge
    jlangbridge over 8 years ago in reply to reinouddelange

    Interesting... I can't even open that page because my Firefox (version 57.0.1) is "too old", despite being installed this morning. I was curious about looking into the IDE, but this roadtest clearly isn't for me

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • reinouddelange
    reinouddelange over 8 years ago in reply to kas.lewis

    I browsed a little further, it seems that you'll need an IDE like tool for it: Vivado.

     

    https://www.xilinx.com/video/hardware/getting-started-with-the-vivado-ide.html

     

    https://www.xilinx.com/support/download.html

     

    But I agree with some others: there's quite a learning curve here...

     

    I guess this is not for me...