RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 100 replies
  • Subscribers 2757 subscribers
  • Views 12309 views
  • Users 0 members are here
  • scasny
  • xilinx
  • fpgafeatured
Related

What's Stopping You Building Your Next Project with an FPGA? (Please, Don't Blame the Cost!)

rscasny
rscasny over 8 years ago

The community does a ton of projects with MCUs. If they do the job for you, that's great. But the element14 community is about learning, experimenting and roadtesting. In this spirit, I am proposing that you should try building your next project with an FPGA (SoC), if it suits the application, of course. What's stopping you? Oh, some members have voiced the cost issue. Granted, some FPGAs do cost a lot. But chip manufacturers are rolling out economical chipsets that most makers, pro-makers or experienced hobbyists can afford. (If you can't, then apply to a RoadTest and if you win you can get a dev board for FREE.) I think FPGA / SoCs will move into a more important place for electronic designers, especially for IoT applications. Perhaps it's time to experiement with one. What's stopping you?

 

Here's a link to a current roadtest:Digilent ARTY S7 Dev Board (Xilinx Spartan 7)   Apply today!

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • ntewinkel
    ntewinkel over 8 years ago

    I just noticed FPGAs can be used for HDMI output, which would be a very interesting use case: fpga4fun.com - HDMI

    But the assembly-like language used on that example website makes me run for the hills.

     

    My hope is something like this: Basic Arduino to output video and sound (https://playground.arduino.cc/Main/TVout ), with the outputs connected to an FPGA that converts it to HDMI.

     

    The ultimate goal is to show images and play mp3s from an SD card on a TV using an HDMI connection.

     

    Would this be possible? (question is to the FPGA experts image re the HDMI part - I can handle the Arduino to TV-out and Audio-out part)

     

    -Nico

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to ntewinkel

    Have you tried the Arduino TVout? By the looks of that page, it can only be one bit per pixel and big, chunky pixels at that.

     

    The FPGA could do the HDMI part at 25MHz quite easily. You'd need to look at the signalling levels on the HDMI - I'm not familiar with it hardware-wise, but you could probably work with one of the many differential standards that FPGAs provide. It would need a proper PCB.

     

    A better architecture (than having the Arduino struggling to produce the video timing) would be to have a frame store in the FPGA (or a memory attached to the FPGA if there wasn't enough internal RAM going spare) that got scanned and output. The Arduino would then write to it once (setting or resetting pixels) and the FPGA would then deal with refreshing the display. It would be similar to an old CGA graphics card in a PC, except you'd be designing the graphics chip. The interface between the Arduino and the FPGA could be whatever you wanted, but SPI might work well.

     

    Another fun idea, taking a further step back in history, would be to do a vector display. The Arduino could write a sequence of line end-point pairs to the FPGA and the FPGA could draw the vectors on-screen (you might decide to get the Arduino to sort them into a favourable order first). You could then do Asteroids in it's original form.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to jc2048

    Thanks Jon!

     

    >Have you tried the Arduino TVout? By the looks of that page, it can only be one bit per pixel and big, chunky pixels at that.

     

    Eww, no I had not looked at it in that much detail, but that doesn't sound very good. I wonder if they only just meant it to be used for the old 80's style arcade games.

     

    I like your idea of frames being sent to the FPGA, seems much nicer.

     

    -Nico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    >All bets are off in a full emergency

     

    Right. In that case we buy a new trailer image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    ntewinkel

     

    I guess the 7808 in between is just to take the bullet in case of a voltage spike on the dirty-automotive-power ?

    The specs for the Digispark regulator say 35v, but yes it was "just in case".

     

     

    Battery or Capacitor would work.

    You have LED's so they are almost instant, and the startup lag is very little. (worth an experiment)

    You're likely to be be braking earlier than normal which gives more time for anyone following, and the indicator only cycle is going to be a little shorter.

     

    All bets are off in a full emergency so even 250mS is not really going to be the final deciding factor IMO.

     

     

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    Ah! I didn't think of using transistors for inputs. So then it's the 12v switching the 5v instead of the other way around when powering LEDs or such. That makes much more sense.

     

    And I guess the 7808 in between is just to take the bullet in case of a voltage spike on the dirty-automotive-power ?

     

    Oh and the small battery - also a way to clean up the power? Or to keep the power on?

    I was thinking of using a capacitor (maybe of the super variety), to keep power on for an intermediate amount of time - that way if there's any startup lag, subsequent use will be quicker.

    Not sure if that would make any real-life difference though, now that I think of it - it's the reaction time on the first lighting of brake lights that counts!

     

    But maybe if a battery or cap keeps it powered long enough for the down-time for city traffic, that might be useful.

    That's another interesting project in itself - can we store enough power during the start of a journey, to last for the next 5 or 10 minutes? The start of a journey usually involves holding the brakes while starting and putting the car in gear, and then a fair bit of brake use while leaving the driveway.

     

    But first things first, though not necessarily in that order image

     

    Thanks,

    -Nico

     

    ps, mcb1

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    Ah! I didn't think of using transistors for inputs. So then it's the 12v switching the 5v instead of the other way around when powering LEDs or such. That makes much more sense.

     

    And I guess the 7808 in between is just to take the bullet in case of a voltage spike on the dirty-automotive-power ?

     

    Oh and the small battery - also a way to clean up the power? Or to keep the power on?

    I was thinking of using a capacitor (maybe of the super variety), to keep power on for an intermediate amount of time - that way if there's any startup lag, subsequent use will be quicker.

    Not sure if that would make any real-life difference though, now that I think of it - it's the reaction time on the first lighting of brake lights that counts!

     

    But maybe if a battery or cap keeps it powered long enough for the down-time for city traffic, that might be useful.

    That's another interesting project in itself - can we store enough power during the start of a journey, to last for the next 5 or 10 minutes? The start of a journey usually involves holding the brakes while starting and putting the car in gear, and then a fair bit of brake use while leaving the driveway.

     

    But first things first, though not necessarily in that order image

     

    Thanks,

    -Nico

     

    ps, mcb1

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ntewinkel
    ntewinkel over 8 years ago in reply to mcb1

    >All bets are off in a full emergency

     

    Right. In that case we buy a new trailer image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to ntewinkel

    ntewinkel

     

    I guess the 7808 in between is just to take the bullet in case of a voltage spike on the dirty-automotive-power ?

    The specs for the Digispark regulator say 35v, but yes it was "just in case".

     

     

    Battery or Capacitor would work.

    You have LED's so they are almost instant, and the startup lag is very little. (worth an experiment)

    You're likely to be be braking earlier than normal which gives more time for anyone following, and the indicator only cycle is going to be a little shorter.

     

    All bets are off in a full emergency so even 250mS is not really going to be the final deciding factor IMO.

     

     

     

    Mark