RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Do You Think of This: Aaware’s Far Field Voice Development Platform?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 2751 subscribers
  • Views 1690 views
  • Users 0 members are here
  • avnet_dev
  • scasny
  • xilinx
  • iot_design
  • fpgasocminized
Related

What Do You Think of This: Aaware’s Far Field Voice Development Platform?

rscasny
rscasny over 8 years ago

A few weeks ago I received an invite to a webinar on a Far Field Voice Dev Platform by a company called Aaware. I was curious so I attended. Basically, the Aaware far field voice development platform is a single-chip voice and sound capture solution for applications where strong interfering sources and high ambient noise are present.

 

It can be used to develop far-field voice interfaces for artificial intelligence (AI) applications including digital assistants, robotics, home automation and automotive. The platform can also be used to develop voice-based cloud services, including Amazon Alexa and Google Home.

 

The Aaware Sound Capture Platform integrates algorithmic acceleration technology and a flexible microphone array board with Avnet’s MiniZedTm Zynq SoC development platform, using dual-core XilinxRegistered  ZynqRegistered-7000 All Programmable SoC devices.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Aaware’s Acoustically Aware sound capture algorithms, paired with wake word detection technology, allow systems to adapt to differing noise interference, without requiring calibration for different environments or integration of the reference signal. The Aaware platform has a concentric circular array of 13 microphones that may be configured in different combinations, allowing for performance tuning. Its sound capture algorithms include source localization, proprietary spatial/spectral/temporal source separation, and noise suppression to deliver low distortion audio of acoustic sources in the sound field.  Some of the features include:

 

Microphone Array Shield

  • 13 MEMs microphones (MP34DB02TR)
  • 15 LEDs
  • Stereo audio DAC output
  • Arduino-compatible shield interface

 

MiniZed (7010)

  • Xilinx Zynq 7010 SoC
  • Micron 512 MB DDR3L
  • Micron 8 GB eMMC
  • Murata WiFi and Bluetooth
  • Arduino-compatible shield interface

 

Aaware reference design Aware sound capture algorithms

  • Source localization and separation
  • Interference cancellation of nearby sources without a reference

 

What do you think? How would you use it? What would you design?

 

You comments are appreciated.

  • Sign in to reply
  • Cancel
Parents
  • dougw
    dougw over 8 years ago

    For a long time I've been trying to improve Skype conversations when using my TV, which is 10 feet away. I don't want microphone cables running all over the living room, so it needs good performance at a distance and some way to effectively control feedback from the speakers. I've tried directional mics with lots of gain, but so far I'm not happy with performance. Maybe this array type of solution would work. I will be looking to obtain one of several mems array mics that have started to appear.

    Another application is project blogging where I need to use an external mic with my camera - it is always a problem with tangling up microphone cables and apparatus cabling.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 8 years ago

    For a long time I've been trying to improve Skype conversations when using my TV, which is 10 feet away. I don't want microphone cables running all over the living room, so it needs good performance at a distance and some way to effectively control feedback from the speakers. I've tried directional mics with lots of gain, but so far I'm not happy with performance. Maybe this array type of solution would work. I will be looking to obtain one of several mems array mics that have started to appear.

    Another application is project blogging where I need to use an external mic with my camera - it is always a problem with tangling up microphone cables and apparatus cabling.