RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Heads Up on an Upcoming RoadTest: Ultra96
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 2756 subscribers
  • Views 3921 views
  • Users 0 members are here
  • avnet_ultra96
  • scasny
  • xilinx
  • fpgafeatured
  • avnet_rt
  • avnet_featured
Related

Heads Up on an Upcoming RoadTest: Ultra96

rscasny
rscasny over 8 years ago

I wanted to give everyone in the RoadTest group some info on a new development board that will be roadtested in the near future: the Ultra96Tm. This board is a great fit for anyone involve in AI or machine learning applications.

 

What follows is a brief overview of the Ultra96Tm.

 

Ultra96Tm is an ARM-based, Xilinx Zynq UltraScale+Tm MPSoC development board based on the Linaro 96Boards specification. The 96Boards’ specifications are open and define a standard board layout for development platforms that can be used by software application, hardware device, kernel, and other system software developers.image

 

Features include:

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Delkin 16 GB MicroSD card + adapter
  • Pre-loaded with PetaLinux environment
  • Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible

 

Ultra96 boots from the provided Delkin 16 GB MicroSD card, pre-loaded with PetaLinux. You have the option of connecting to Ultra96 through a Webserver using integrated wireless access point capability or to use the provided PetaLinux desktop environment which can be viewed on the integrated Mini DisplayPort video output.

 

Ultra96 provides four user-controllable LEDs. Engineers may also interact with the board through the 96Boards-compatible low-speed and high-speed expansion connectors by adding peripheral accessories such as those included in Seed Studio’s Grove Starter Kit for 96Boards.

image

 

What do you thinking about roadtesting this board? What would you do with it?

  • Sign in to reply
  • Cancel
Parents
  • yosoufe
    yosoufe over 8 years ago

    This seems to be amazing. Is it coming with license of SDSoC Development Environmen? If the license is available, one can test it with xilinx revision and run for example VGG16 network and compare it with other hardware or make some useful computer vision tasks, like kaggle's competitions or traffic sign detector and a lot more.

     

    The key is to run first the simplest network on it to learn it. I do not know how difficult would be to learn the Xilinx revision. You should know Caffe as well. I guess it should not be difficult if you know tensorflow. Do we have anybody here having experience of using deep learning on FPGA in the community?

     

    I would compare its performance with Intel Movidius Compute Stick on a raspberry pi or a gaming GPU. But first of all, I have to review xilinx revision in more details. Are there any online tutorial available except this??

     

    There are some challenges in this area like this. Hopefully after the challenge, people would open source theirs solutions and you could try it on this board image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gpolder
    gpolder over 8 years ago in reply to yosoufe

    I doubt whether it is possible to do deep learning on this board.

    AI is mentioned in the video below, but AI is a much broader field than deep-learning, in which case this board should compete with the Nvidia Jetson (https://en.wikipedia.org/wiki/Nvidia_Jetson ).

    Anyway, I would rather like to do some AI or image processing on the Ultra96.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • yosoufe
    yosoufe over 8 years ago in reply to gpolder

    Right. I meant as well just for the inference time. Not learning.

    https://www.xilinx.com/support/documentation/backgrounders/revision-overview.pdf

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • yosoufe
    yosoufe over 8 years ago in reply to gpolder

    Right. I meant as well just for the inference time. Not learning.

    https://www.xilinx.com/support/documentation/backgrounders/revision-overview.pdf