RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Heads Up on an Upcoming RoadTest: Ultra96
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 2756 subscribers
  • Views 3923 views
  • Users 0 members are here
  • avnet_ultra96
  • scasny
  • xilinx
  • fpgafeatured
  • avnet_rt
  • avnet_featured
Related

Heads Up on an Upcoming RoadTest: Ultra96

rscasny
rscasny over 8 years ago

I wanted to give everyone in the RoadTest group some info on a new development board that will be roadtested in the near future: the Ultra96Tm. This board is a great fit for anyone involve in AI or machine learning applications.

 

What follows is a brief overview of the Ultra96Tm.

 

Ultra96Tm is an ARM-based, Xilinx Zynq UltraScale+Tm MPSoC development board based on the Linaro 96Boards specification. The 96Boards’ specifications are open and define a standard board layout for development platforms that can be used by software application, hardware device, kernel, and other system software developers.image

 

Features include:

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Delkin 16 GB MicroSD card + adapter
  • Pre-loaded with PetaLinux environment
  • Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible

 

Ultra96 boots from the provided Delkin 16 GB MicroSD card, pre-loaded with PetaLinux. You have the option of connecting to Ultra96 through a Webserver using integrated wireless access point capability or to use the provided PetaLinux desktop environment which can be viewed on the integrated Mini DisplayPort video output.

 

Ultra96 provides four user-controllable LEDs. Engineers may also interact with the board through the 96Boards-compatible low-speed and high-speed expansion connectors by adding peripheral accessories such as those included in Seed Studio’s Grove Starter Kit for 96Boards.

image

 

What do you thinking about roadtesting this board? What would you do with it?

  • Sign in to reply
  • Cancel
Parents
  • hlipka
    hlipka over 8 years ago

    I think whoever is doing this road test is in for some heavy work. We have seen that with the recent MiniZed board and the Basys3, and this board can do even more. It really is a single-board computer (4 ARM cores) with an attached FPGA. And the latter is quite powerful (with 150k logic cells). Using this for AI or machine learning will be a challenge.

    What I would like to do with that board is building a stand-alone logic analyzer. With the OLS there is a quite powerful FPGA core available (and with the DemonCore there is a variant adding extensive triggering). The Ultra96 adds an even faster FPGA and much more memory to the mix, and the ARM cores can run the GUI. The UltraScale+ comes with its own Mali 400 GPU, and even has DSP elements for post-processing. That would be cool, although probably not the intended use case (the product selector lists flight navigation and missiles...)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • hlipka
    hlipka over 8 years ago

    I think whoever is doing this road test is in for some heavy work. We have seen that with the recent MiniZed board and the Basys3, and this board can do even more. It really is a single-board computer (4 ARM cores) with an attached FPGA. And the latter is quite powerful (with 150k logic cells). Using this for AI or machine learning will be a challenge.

    What I would like to do with that board is building a stand-alone logic analyzer. With the OLS there is a quite powerful FPGA core available (and with the DemonCore there is a variant adding extensive triggering). The Ultra96 adds an even faster FPGA and much more memory to the mix, and the ARM cores can run the GUI. The UltraScale+ comes with its own Mali 400 GPU, and even has DSP elements for post-processing. That would be cool, although probably not the intended use case (the product selector lists flight navigation and missiles...)

    • Cancel
    • Vote Up +4 Vote Down