RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Heads Up on an Upcoming RoadTest: Ultra96
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 2752 subscribers
  • Views 3964 views
  • Users 0 members are here
  • avnet_ultra96
  • scasny
  • xilinx
  • fpgafeatured
  • avnet_rt
  • avnet_featured
Related

Heads Up on an Upcoming RoadTest: Ultra96

rscasny
rscasny over 8 years ago

I wanted to give everyone in the RoadTest group some info on a new development board that will be roadtested in the near future: the Ultra96Tm. This board is a great fit for anyone involve in AI or machine learning applications.

 

What follows is a brief overview of the Ultra96Tm.

 

Ultra96Tm is an ARM-based, Xilinx Zynq UltraScale+Tm MPSoC development board based on the Linaro 96Boards specification. The 96Boards’ specifications are open and define a standard board layout for development platforms that can be used by software application, hardware device, kernel, and other system software developers.image

 

Features include:

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Delkin 16 GB MicroSD card + adapter
  • Pre-loaded with PetaLinux environment
  • Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible

 

Ultra96 boots from the provided Delkin 16 GB MicroSD card, pre-loaded with PetaLinux. You have the option of connecting to Ultra96 through a Webserver using integrated wireless access point capability or to use the provided PetaLinux desktop environment which can be viewed on the integrated Mini DisplayPort video output.

 

Ultra96 provides four user-controllable LEDs. Engineers may also interact with the board through the 96Boards-compatible low-speed and high-speed expansion connectors by adding peripheral accessories such as those included in Seed Studio’s Grove Starter Kit for 96Boards.

image

 

What do you thinking about roadtesting this board? What would you do with it?

  • Sign in to reply
  • Cancel
Parents
  • weiwei2
    weiwei2 over 7 years ago

    i was reading this article on Xilinx about A section about training the BNN is in progress and will be added soon.

    May I know if is it available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • as_mle
    as_mle over 7 years ago in reply to weiwei2

    Hi

     

    Andreas Schuler here.

    The design is basically a transformation of the PYNQ design. As PYNQ is Python and Jupiter Notebook based, the Accererated Image Classification (AIC) is based on Petalinux (with Ubuntu on top) and C.

     

    You can use following Link as a guidline for training and generating binary weights:

    https://github.com/Xilinx/BNN-PYNQ/tree/master/bnn/src/training

     

    We used a script from here:

    German Traffic Sign Benchmarks to read in the road sign images (readTrafficSigns.py), unfortunately we can not publish the modified script as it has no legal disclaimer from the original Autor.

    Further more:

    As we do a brute force search within the image, we need to dismiss random background. To achieve this, we added a "junk class" and ignored it.

     

    Another unfortunate point is: Xilinx changed the hoster of the Wiki, so we try to get the permissions again to update the Wiki, as we already have the update for the next Vivado version.

     

    Andreas

     

    (Employee at Missing Link Electronics, Project Lead of the AIC Demo)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nixiefairy
    nixiefairy over 7 years ago in reply to as_mle

    Sorry had a quick question Andreas, does the PYNQ image fully utilize all the hardware present on the Ultra96 board? Like is there fully developed IP for each of the hardware components of the Ultra96. Or like, there are just some loose ports in the overlay design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • nixiefairy
    nixiefairy over 7 years ago in reply to as_mle

    Sorry had a quick question Andreas, does the PYNQ image fully utilize all the hardware present on the Ultra96 board? Like is there fully developed IP for each of the hardware components of the Ultra96. Or like, there are just some loose ports in the overlay design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • nixiefairy
    nixiefairy over 7 years ago in reply to as_mle

    I was looking for the specialized IP for the PYNQ image.Looks like someone has to explain it. Will give a thorough look into it in my review.  Haven't seen much of the advanced outputs. Looks interesting!

    Thanks for the wonderful tips!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • as_mle
    as_mle over 7 years ago in reply to nixiefairy

    First: We used the PYNQ design as a starting point for the neuronal network, as far as I know the original PYNQ Design was for ZYNQ7000.

     

    Which hardware components do you refer to?

    Interfaces deployed on the PCB? -> Xilinx showed design examples at embedded World 2018 to integrate sensors like buttons, temperature, humidity or outputs like a small LCD. Mostly GPIO and IIC if I'm not wrong. Pynq only offers specialised IP (for example the Neuronal Network as IP), all other IO's are utilised by the Processing System in SW. But those specialised IP's are created with mightier tools like Vivado, HLS and SDSoC.

     

    For more advanced outputs, like Display port, you will need to work with Linux. In the AIC Demo we used PetaLinux with an Ubuntu on top, means you have a full GUI, check it out ;-)

     

    To fully utilise the Zynq Ultrascale+ (ZU+), there is no design out which utilised the entire Chip with all components (or we did't found it yet). ZU+ is simply to complex. 

     

    Best regards

    Andreas