RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum Heads Up on an Upcoming RoadTest: Ultra96
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 2669 subscribers
  • Views 3345 views
  • Users 0 members are here
  • avnet_ultra96
  • scasny
  • xilinx
  • fpgafeatured
  • avnet_rt
  • avnet_featured
Related

Heads Up on an Upcoming RoadTest: Ultra96

rscasny
rscasny over 7 years ago

I wanted to give everyone in the RoadTest group some info on a new development board that will be roadtested in the near future: the Ultra96Tm. This board is a great fit for anyone involve in AI or machine learning applications.

 

What follows is a brief overview of the Ultra96Tm.

 

Ultra96Tm is an ARM-based, Xilinx Zynq UltraScale+Tm MPSoC development board based on the Linaro 96Boards specification. The 96Boards’ specifications are open and define a standard board layout for development platforms that can be used by software application, hardware device, kernel, and other system software developers.image

 

Features include:

  • Xilinx Zynq UltraScale+ MPSoC ZU3EG A484
  • Micron 2 GB (512M x32) LPDDR4 Memory
  • Delkin 16 GB MicroSD card + adapter
  • Pre-loaded with PetaLinux environment
  • Wi-Fi / Bluetooth
  • Mini DisplayPort (MiniDP or mDP)
  • 1x USB 3.0 Type Micro-B upstream port
  • 2x USB 3.0, 1x USB 2.0 Type A downstream ports
  • 40-pin 96Boards Low-speed expansion header
  • 60-pin 96Boards High speed expansion header
  • 85mm x 54mm form factor
  • Linaro 96Boards Consumer Edition compatible

 

Ultra96 boots from the provided Delkin 16 GB MicroSD card, pre-loaded with PetaLinux. You have the option of connecting to Ultra96 through a Webserver using integrated wireless access point capability or to use the provided PetaLinux desktop environment which can be viewed on the integrated Mini DisplayPort video output.

 

Ultra96 provides four user-controllable LEDs. Engineers may also interact with the board through the 96Boards-compatible low-speed and high-speed expansion connectors by adding peripheral accessories such as those included in Seed Studio’s Grove Starter Kit for 96Boards.

image

 

What do you thinking about roadtesting this board? What would you do with it?

  • Sign in to reply
  • Cancel

Top Replies

  • gam3t3ch
    gam3t3ch over 7 years ago +5
    www.youtube.com/watch Found this video check it out this is a pretty sweet board with a lot of possibilities.
  • bhfletcher
    bhfletcher over 7 years ago in reply to yosoufe +4
    The Ultra96 kit ships with a node-locked, device-locked license voucher for SDSoC. That will get you access to the tool and updates for a year. Avnet is working with Xilinx to create a baseline SDSoC platform…
  • hlipka
    hlipka over 7 years ago +4
    I think whoever is doing this road test is in for some heavy work. We have seen that with the recent MiniZed board and the Basys3, and this board can do even more. It really is a single-board computer…
  • hlipka
    hlipka over 7 years ago

    I think whoever is doing this road test is in for some heavy work. We have seen that with the recent MiniZed board and the Basys3, and this board can do even more. It really is a single-board computer (4 ARM cores) with an attached FPGA. And the latter is quite powerful (with 150k logic cells). Using this for AI or machine learning will be a challenge.

    What I would like to do with that board is building a stand-alone logic analyzer. With the OLS there is a quite powerful FPGA core available (and with the DemonCore there is a variant adding extensive triggering). The Ultra96 adds an even faster FPGA and much more memory to the mix, and the ARM cores can run the GUI. The UltraScale+ comes with its own Mali 400 GPU, and even has DSP elements for post-processing. That would be cool, although probably not the intended use case (the product selector lists flight navigation and missiles...)

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • snidhi
    snidhi over 7 years ago

    Having Arm-based, Xilinx Zynq UltraScale+ it seems this board can take on some processing. To learn about the processing capability of this board for starters I would do a PMOD Sensor based learning project. And with this one can estimate how the board performs with the learning algorithms; something on the lines of IOT sensor based learning.

     

    Cheers image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bhfletcher
    bhfletcher over 7 years ago

    Related to Ultra96, take a look at this blog to learn why we chose a Delkin MLC Utility card rather than an inexpensive retail card for the Ultra96 kit.

     

    Storage Insights #1 - Why Not All SD Cards are Created Equal

     

    Bryan

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • weiwei2
    weiwei2 over 7 years ago

    i was reading this article on Xilinx about A section about training the BNN is in progress and will be added soon.

    May I know if is it available?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to weiwei2

    I don't know. I'll ask around to see if I can get you answer.

     

    Randall

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to weiwei2

    I went back and looked again who created it. Andreas Schuler, not a Xilinx employee I believe. The section you refer to has not been updated since last May.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • bhfletcher
    bhfletcher over 7 years ago in reply to rscasny

    I'm not sure which location is in question on Xilinx.com, but Andreas did get the BNN design posted on the Xilinx Wiki -- https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/18841949/Zynq+UltraScale+MPSoC+Accelerated+Image+Classification+vi…

     

    Is that what you are looking for?

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to bhfletcher

    weiwei2

     

    Cheah,

     

    See Bryan's comment above.

     

    Is this what you are looking for?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • weiwei2
    weiwei2 over 7 years ago in reply to rscasny

    The url given Bryan is the same one I refer to

    https://xilinx-wiki.atlassian.net/wiki/plugins/servlet/mobile?contentId=18841949#content/view/18841949

     

    In on that article it is mentioned a section on training the bnn will be added hence I am interested with it

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • as_mle
    as_mle over 7 years ago in reply to weiwei2

    Hi

     

    Andreas Schuler here.

    The design is basically a transformation of the PYNQ design. As PYNQ is Python and Jupiter Notebook based, the Accererated Image Classification (AIC) is based on Petalinux (with Ubuntu on top) and C.

     

    You can use following Link as a guidline for training and generating binary weights:

    https://github.com/Xilinx/BNN-PYNQ/tree/master/bnn/src/training

     

    We used a script from here:

    German Traffic Sign Benchmarks to read in the road sign images (readTrafficSigns.py), unfortunately we can not publish the modified script as it has no legal disclaimer from the original Autor.

    Further more:

    As we do a brute force search within the image, we need to dismiss random background. To achieve this, we added a "junk class" and ignored it.

     

    Another unfortunate point is: Xilinx changed the hoster of the Wiki, so we try to get the permissions again to update the Wiki, as we already have the update for the next Vivado version.

     

    Andreas

     

    (Employee at Missing Link Electronics, Project Lead of the AIC Demo)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>