RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2757 subscribers
  • Views 3535 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • kas.lewis
    kas.lewis over 8 years ago

    This definitely sounds interesting, for those without the "right" gear, one idea would be to use something like SmartRF from TI that allows for some of these variables to be altered and monitored. Then by measuring something like RSSI or BER depending on positioning of the units some inference of antenna pattern or gain gould be made. All this being said, you would still need a consistent preferably quite environment... anyone up for a drive to the country ??

     

    The same could be done using a spectrum analyzer in a quiet environment to get an idea of antenna pattern. Alternatively the road test could include a decent amount of RF absorbing foam for the roadtester to build their own chamber.... they could then report back on how easy/hard this was and how well or not it worked out. image

     

    Kas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • kas.lewis
    kas.lewis over 8 years ago

    This definitely sounds interesting, for those without the "right" gear, one idea would be to use something like SmartRF from TI that allows for some of these variables to be altered and monitored. Then by measuring something like RSSI or BER depending on positioning of the units some inference of antenna pattern or gain gould be made. All this being said, you would still need a consistent preferably quite environment... anyone up for a drive to the country ??

     

    The same could be done using a spectrum analyzer in a quiet environment to get an idea of antenna pattern. Alternatively the road test could include a decent amount of RF absorbing foam for the roadtester to build their own chamber.... they could then report back on how easy/hard this was and how well or not it worked out. image

     

    Kas