RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 3638 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 8 years ago

    A lot of people will argue that the only way to test an antenna would be with very expensive instrumentation and in an electronically clean environment.  While testing antennas is not my occupation or even something that I do often (more likely never), there are some simple ways to test them.  Way back in the dark ages, when AM and FM broadcasting was viewed as the highest frequencies that people would deal with, a radio station would need to test their signal patterns, by driving around and measuring signal strength using a tuned voltmeter.  These days, the same can be done, but simply by using the RSI (Relative Strength Index) values available within most receivers.  While working on a Zigbee meshed system, our clever RF engineer, would set up a meshed system in an unobstructed warehouse, with nodes populated through out the building.  He could then test a node, by broadcasting messages and collecting RSI values from nodes within the building (the messages needed to be qualified, so that re-transmitted, or bounced signals would be ignored) and build a signal strength profile map.  We mostly used this test to determine if our node placed inside of a fixture was overly attenuated due to all the surrounding materials.

     

    A modification of this method could prove to be helpful in testing antennas by mapping out RSI values gathered from different locations around a transmitter/antenna pair.

     

    Just a thought.

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 8 years ago in reply to genebren

    I agree, plus there are a load of things that are subjective but still highly useful to know, such as how well built the antennas are, if any hinge parts seem reliable (I've seen failed antennas from new, because of manufacturing tolerances in the hinge contact), and does the antenna cause rotation of the center pin when fitting it (e.g. some may prefer antennas where the center pin is not rotated when installing the antenna).

    It is unrealistic to expect the antenna to be subjected to a full suite of measurements as (say) a consultant would do, because such tasks are normally chargeable at tens of thousands of $$. Besides, for a real deployment such antenna matching would be done with the antenna mounted to the product.

     

    As you say, there are plenty of practical things anyone can do. As another example, when soldiers 'create' an antenna by slinging wire over a tree, they make the best of what they can to determine antenna quality, using relatively simple procedures at their disposal since they are in the field. That's at far lower frequencies than (say) WLAN and Bluetooth of course, but still, measuring signal strength by moving around an area is a practical method for these higher frequencies like you mention.

     

    Basically often I'm interested to hear the practical stuff like usability, some of the subjective stuff as mentioned above too, and how particular aspects of a product could benefit an application, and if it functions well for certain roles, rather than a quantified verification of the manufacturer's datasheet.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago in reply to genebren

    I agree, plus there are a load of things that are subjective but still highly useful to know, such as how well built the antennas are, if any hinge parts seem reliable (I've seen failed antennas from new, because of manufacturing tolerances in the hinge contact), and does the antenna cause rotation of the center pin when fitting it (e.g. some may prefer antennas where the center pin is not rotated when installing the antenna).

    It is unrealistic to expect the antenna to be subjected to a full suite of measurements as (say) a consultant would do, because such tasks are normally chargeable at tens of thousands of $$. Besides, for a real deployment such antenna matching would be done with the antenna mounted to the product.

     

    As you say, there are plenty of practical things anyone can do. As another example, when soldiers 'create' an antenna by slinging wire over a tree, they make the best of what they can to determine antenna quality, using relatively simple procedures at their disposal since they are in the field. That's at far lower frequencies than (say) WLAN and Bluetooth of course, but still, measuring signal strength by moving around an area is a practical method for these higher frequencies like you mention.

     

    Basically often I'm interested to hear the practical stuff like usability, some of the subjective stuff as mentioned above too, and how particular aspects of a product could benefit an application, and if it functions well for certain roles, rather than a quantified verification of the manufacturer's datasheet.