RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 3641 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • genebren
    genebren over 8 years ago

    A lot of people will argue that the only way to test an antenna would be with very expensive instrumentation and in an electronically clean environment.  While testing antennas is not my occupation or even something that I do often (more likely never), there are some simple ways to test them.  Way back in the dark ages, when AM and FM broadcasting was viewed as the highest frequencies that people would deal with, a radio station would need to test their signal patterns, by driving around and measuring signal strength using a tuned voltmeter.  These days, the same can be done, but simply by using the RSI (Relative Strength Index) values available within most receivers.  While working on a Zigbee meshed system, our clever RF engineer, would set up a meshed system in an unobstructed warehouse, with nodes populated through out the building.  He could then test a node, by broadcasting messages and collecting RSI values from nodes within the building (the messages needed to be qualified, so that re-transmitted, or bounced signals would be ignored) and build a signal strength profile map.  We mostly used this test to determine if our node placed inside of a fixture was overly attenuated due to all the surrounding materials.

     

    A modification of this method could prove to be helpful in testing antennas by mapping out RSI values gathered from different locations around a transmitter/antenna pair.

     

    Just a thought.

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to genebren

    Way back in the dark ages, when AM and FM broadcasting was viewed as the highest frequencies that people would deal with, a radio station would need to test their signal patterns, by driving around and measuring signal strength

    Hey less of the dark ages stuff there sonny. image

     

    When I worked for Telecom (it seems way back now) that was how we proved our coverage areas.

    We had a number of existing sites, and the appropriate antenna and transmitter would be installed, and then we'd hop in a car and drive all around the Canterbury plains to prove the coverage area was acceptable.

     

    It was interesting when we ventured into UHF, as it behaved very well in the city and even a remote town (148km away) with tall buildings yielded a surprising result.

    This was of course at odds with VHF that is basically a line of sight service, although the path was half water and half open plain.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mcb1
    mcb1 over 8 years ago in reply to genebren

    Way back in the dark ages, when AM and FM broadcasting was viewed as the highest frequencies that people would deal with, a radio station would need to test their signal patterns, by driving around and measuring signal strength

    Hey less of the dark ages stuff there sonny. image

     

    When I worked for Telecom (it seems way back now) that was how we proved our coverage areas.

    We had a number of existing sites, and the appropriate antenna and transmitter would be installed, and then we'd hop in a car and drive all around the Canterbury plains to prove the coverage area was acceptable.

     

    It was interesting when we ventured into UHF, as it behaved very well in the city and even a remote town (148km away) with tall buildings yielded a surprising result.

    This was of course at odds with VHF that is basically a line of sight service, although the path was half water and half open plain.

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down