RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 3629 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • rscasny
    rscasny over 8 years ago

    I want to thank everyone who has contributed their ideas about an antenna roadtest.

     

    I met with the supplier again, so this roadtest is coming closer to a reality.

     

    The supplier is planning on giving me "developer kits" that include the antenna and some kind of dev board for tx/rec.

     

    They also are interested in the PCb mounted antenna. Apparently, it has gotten a lot of designers who had problems placing the antenna on the pcb. Depending where it is placed can impact the antenna.

     

    Another problem they are experiencing are obstacles (coverage/penetration losses).

     

    The final problem they are experiencing is (as expected) plain old improper installation problems.

     

    I'll keep you posted. Thanks, again.

     

    Randall Scasny

    RoadTest Program Manager

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • rscasny
    rscasny over 8 years ago

    I want to thank everyone who has contributed their ideas about an antenna roadtest.

     

    I met with the supplier again, so this roadtest is coming closer to a reality.

     

    The supplier is planning on giving me "developer kits" that include the antenna and some kind of dev board for tx/rec.

     

    They also are interested in the PCb mounted antenna. Apparently, it has gotten a lot of designers who had problems placing the antenna on the pcb. Depending where it is placed can impact the antenna.

     

    Another problem they are experiencing are obstacles (coverage/penetration losses).

     

    The final problem they are experiencing is (as expected) plain old improper installation problems.

     

    I'll keep you posted. Thanks, again.

     

    Randall Scasny

    RoadTest Program Manager

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
Children
  • station240
    station240 over 8 years ago in reply to rscasny

    Ah if it includes an RX/TX board I might be interested.

    Could be a nice little test to map signal coverage inside a house.