RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum UPDATE on Seeking Ideas for RoadTesting Antennas
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 2752 subscribers
  • Views 3629 views
  • Users 0 members are here
  • scasny
Related

UPDATE on Seeking Ideas for RoadTesting Antennas

rscasny
rscasny over 8 years ago

I finally got some information on the antennas that I want to roadtest. These antennas are for Frequency / application :  2.4/5GHz Antenna – typical for Bluetooth, WiFi.

 

Here they are:

 

image

 

2.4GHz / 5GHz Wi-Fi Stand Alone Balance Antenna with MHF Connector, 9.00mm Width, Cable Length 100.00mm

  • Product Name: 2.4/5GHz Balanced Flex Antenna
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Cable Length: 100.00mm
  • Length: 34.90mm
  • Mounting Style Adhesive
  • Net Weight: 0.574/g
  • Packaging Type: PET Film
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 0.10mm
  • Width: 9.00mm

Click Here for More information

 

image

 

2.4GHz SMT On-ground MID Chip Antenna

  • Product Name: 2.4GHz SMT OnGround MID Chip
  • Protocol: BLE, BT, Thread, Wi-Fi, Wireless Hart, Zigbee
  • Type: Wi-Fi Antenna
  • Length: 3.00mm
  • Mounting Style: Surface Mount
  • Net Weight: 0.042/g
  • Polarization: Linear
  • Radiation Pattern: Omnidirectional
  • Thickness: 4.00mm
  • Width: 3.00mm

Click Here for More Information

 

Your thoughts about roadtesting these specific products would be appreciated. Thanks.

 

Sincerely,

 

Randall Scasny

RoadTest Program Manager

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    shabaz over 8 years ago

    Hi Randall,

     

    I'd be happy to try out both antennas for a practical type of RoadTest with Bluetooth LE, since I'm already working on a PCB here:

    Smart Doorbell System – Part 5 – Final Bell Push Circuit and Antenna Design

     

    For the chip antenna, I'll need to create a different revision of the PCB, but it would be just a small change (i.e. remove the Inverted F antenna and have the pads for the chip antenna instead). I might need to have (say) e-mail contact with a Molex technical person to do it properly, although the information on their website is pretty good.

     

    Thanks,

     

    Shabaz.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 8 years ago

    Hi Randall,

     

    I'd be happy to try out both antennas for a practical type of RoadTest with Bluetooth LE, since I'm already working on a PCB here:

    Smart Doorbell System – Part 5 – Final Bell Push Circuit and Antenna Design

     

    For the chip antenna, I'll need to create a different revision of the PCB, but it would be just a small change (i.e. remove the Inverted F antenna and have the pads for the chip antenna instead). I might need to have (say) e-mail contact with a Molex technical person to do it properly, although the information on their website is pretty good.

     

    Thanks,

     

    Shabaz.

    • Cancel
    • Vote Up +3 Vote Down