RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest the Matrix Voice
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2756 subscribers
  • Views 3645 views
  • Users 0 members are here
  • scasny
Related

How Would You RoadTest the Matrix Voice

rscasny
rscasny over 7 years ago

Voice applications are gaining popularity. The apps can range from far field voice captures, acoustic source localization, beamforming, noise suppression, acoustic echo cancellation, voice recognition integration, and more.image

 

So, it should be no surprise to the RoadTester group that I would be approached to roadtest a voice-app dev board. Enter, the Matrix Voice.

 

Last year, we roadtested the Matrix Creator for the Raspberry Pi , which is an expansion daughter board for the Raspberry Pi. The Matrix Voice has the same circular shape as the Creator, but is a simple, easy-to-use, open-source voice recognition platform. It's 3.14 inches in diameter with a radial array of 7 MEMS microphones connected to a Xilinx Spartan 6 FPGA and 64 Mbit SDRAM with 18 RGBW LED's and 16 GPIO pins.

 

There are two versions of the Matrix Voice: one version works with the Raspberry Pi, and the other version has an onboard ESP32 Wi-Fi/BT module with a 32 bit microcontroller, so it can work as a standalone device. Since I know my Roadtesters love the tech details, here's a few specs:

 

  • FPGA : Xilinx Spartan 6 FPGA XC6SLX9
  • 18 RGBW LEDs (link)
  • 8 MEMS audio sensor MP34DB02
  • 16 external GPIO. These are connected to FPGA so they can implement any digital
  • interface e.eg PWM, Servo, UART, I2C etc.
  • Serial Flash 64MBIT - MX25L6406E
  • DDR2 SDRAM 512MBIT - MT47H32M16
  • 3W Stereo Class-D Audio Amplifier and Class-AB Headphone Driver - PAM8019
  • 3.5mm audio output jack

 

Here's a few tech resources for you to examine:

  • Datasheet
  • Github
  • Getting Started Video

 

So here's my question: How Would You roadTest the Matrix Voice? What would you build with the Matrix Voice? What would you like to know about the Matrix Voice. Leave your thoughts and comments below. Thanks.

 

Randall Scasny

RoadTest Program Manager

 

 

Before I go.....

 

I saw this video on youtube where the Matrix Voice was used with Alexa. Some asked:

 

"Alexa, how much wood can a wood chuck chuck if a wood chuck could chuck wood? Watch the video to find out:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Fred27

    I have ISE woking on windows 10 too with bumping 32 and 64 bit dlls around.

    What I can't get to work reliably is the simulator. It blocks after a few simulation steps. And the build process sometimes blocks on a hung command line tool too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to Jan Cumps

    Reprogramming the Spartan 6 is exactly what sprung to mind for me - although I'm sure that's not the sort of Road Test the manufacturer is after.

     

    It is possible to run the latest version of ISE on Windows 10 by copying a few DLLs around. It's also possible to enable it for the larger Spartan 6 devices without having to have the VM on your machine. A bit trickier, but it can be done. I managed to get this working because I started playing with the PanoLogic thin clients and I really didn't want 3 x 6GB installs on my machine (Vivado, ISE, ISE in a VM). Xilinx certainly loves disk space!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 7 years ago in reply to dougw

    Perhaps overhead choir mics above your work area. If you feed them through a compressor you can even off the levels as you move around - set the dynamics to increase compression as you get closer and back the compression off as you move further away.

     

    A number of conference table type applications are moving to 'beam forming' ceiling microphone arrays. However ceilings often have a lot of noise with ventilation and projector fans.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to nixiefairy

    7 runs on Vivado. 6 Is still ISE.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago

    I don't have any esoteric needs, but I have 2 mundane applications that have been bugging me for a long time:

    1. A long range microphone I can locate at my large screen TV and use for Skype calls while sitting across the room. (A wired mic running across the living room just doesn't cut it.)
    2. A mic for my camera that will equalize my voice volume as I blog - no matter how far away I move (up to 8 feet). Wearing a wired mic often gets in the way while doing a demo. Even a wireless Lavalier is cumbersome and distracting in a video.

    My attempts to solve these applications so far have been dismal. (I am open to suggestions)

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rsc
    rsc over 7 years ago

    It would be interesting to add some directional baffles and use the device for determining sound source direction.  With haptic feedback, it could be a good aid for the deaf.

    Scott

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • nixiefairy
    nixiefairy over 7 years ago in reply to Jan Cumps

    Aah I have never used a spartan 6. I've used a spartan 3 with ISE before. So like, I assumed since 6>3 it would be running on Vivado.

    Well that's news to me

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to nixiefairy

    You have to, if you want to develop for a Spartan 6. What would you use?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • nixiefairy
    nixiefairy over 7 years ago in reply to Jan Cumps

    Wait a minute. ISE? Do people even use it anymore? 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • aabhas
    aabhas over 7 years ago

    Matrix voice is a very good add on board for projects using voice interfrace with raspberry pi . It contains good microphone and we can use it to make project something for home automation and try the different sensors inbuilt in it .The standalone version would be helpful where there is need of low cost project.

     

    I would like to road test it by making a personal voice assistant for us using raspberry pi and matrix voice and use the data of inbuilt sensors in it  and try to put my hands on fpga.

     

     

    Aabhas Senapati

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>