RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum How Would You RoadTest the Matrix Voice
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 2757 subscribers
  • Views 3617 views
  • Users 0 members are here
  • scasny
Related

How Would You RoadTest the Matrix Voice

rscasny
rscasny over 7 years ago

Voice applications are gaining popularity. The apps can range from far field voice captures, acoustic source localization, beamforming, noise suppression, acoustic echo cancellation, voice recognition integration, and more.image

 

So, it should be no surprise to the RoadTester group that I would be approached to roadtest a voice-app dev board. Enter, the Matrix Voice.

 

Last year, we roadtested the Matrix Creator for the Raspberry Pi , which is an expansion daughter board for the Raspberry Pi. The Matrix Voice has the same circular shape as the Creator, but is a simple, easy-to-use, open-source voice recognition platform. It's 3.14 inches in diameter with a radial array of 7 MEMS microphones connected to a Xilinx Spartan 6 FPGA and 64 Mbit SDRAM with 18 RGBW LED's and 16 GPIO pins.

 

There are two versions of the Matrix Voice: one version works with the Raspberry Pi, and the other version has an onboard ESP32 Wi-Fi/BT module with a 32 bit microcontroller, so it can work as a standalone device. Since I know my Roadtesters love the tech details, here's a few specs:

 

  • FPGA : Xilinx Spartan 6 FPGA XC6SLX9
  • 18 RGBW LEDs (link)
  • 8 MEMS audio sensor MP34DB02
  • 16 external GPIO. These are connected to FPGA so they can implement any digital
  • interface e.eg PWM, Servo, UART, I2C etc.
  • Serial Flash 64MBIT - MX25L6406E
  • DDR2 SDRAM 512MBIT - MT47H32M16
  • 3W Stereo Class-D Audio Amplifier and Class-AB Headphone Driver - PAM8019
  • 3.5mm audio output jack

 

Here's a few tech resources for you to examine:

  • Datasheet
  • Github
  • Getting Started Video

 

So here's my question: How Would You roadTest the Matrix Voice? What would you build with the Matrix Voice? What would you like to know about the Matrix Voice. Leave your thoughts and comments below. Thanks.

 

Randall Scasny

RoadTest Program Manager

 

 

Before I go.....

 

I saw this video on youtube where the Matrix Voice was used with Alexa. Some asked:

 

"Alexa, how much wood can a wood chuck chuck if a wood chuck could chuck wood? Watch the video to find out:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • vimarsh_
    vimarsh_ over 7 years ago

    Matrix voice is a good add on to the RPi. There are many such hats but this one is the best of it due to that FPGA.

     

    The advantage is we can make a home automation system, a google home for ourselves or make our own assistants with things like snips.ai

     

    It is also smaller than the creator. It also does not have esp32 moreover the sensors are lacking in the simple version. The one with esp32 can be more helpful as it can be programmed standalone and so we can also add functionalities which are difficult with FPGA or simply not possible. Even the creator does not have ESP32 a very common chip to program for standalone operation.

     

    But being small, and the awesome projects and manufacturer support we can create cool home automation projects.

    HA is quite common and also has many exixting solutions so we need to be creative to think where else it can be used? Probably in some alarming system or something else.

     

    We can test it by creating an all-in-one project as that is what the board is capable to do and we can also experiment with FPGA which have good documentation.

     

     

    Vimarsh

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vimarsh_
    vimarsh_ over 7 years ago

    Matrix voice is a good add on to the RPi. There are many such hats but this one is the best of it due to that FPGA.

     

    The advantage is we can make a home automation system, a google home for ourselves or make our own assistants with things like snips.ai

     

    It is also smaller than the creator. It also does not have esp32 moreover the sensors are lacking in the simple version. The one with esp32 can be more helpful as it can be programmed standalone and so we can also add functionalities which are difficult with FPGA or simply not possible. Even the creator does not have ESP32 a very common chip to program for standalone operation.

     

    But being small, and the awesome projects and manufacturer support we can create cool home automation projects.

    HA is quite common and also has many exixting solutions so we need to be creative to think where else it can be used? Probably in some alarming system or something else.

     

    We can test it by creating an all-in-one project as that is what the board is capable to do and we can also experiment with FPGA which have good documentation.

     

     

    Vimarsh