RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Would You Build If I Gave You an SBC, Sensors, Relays, Connectors, a Power Supply and an Enclosure?
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 2755 subscribers
  • Views 3914 views
  • Users 0 members are here
  • scasny
  • ind_tag
  • rpi
  • energy_power
  • rpi_projects
Related

What Would You Build If I Gave You an SBC, Sensors, Relays, Connectors, a Power Supply and an Enclosure?

rscasny
rscasny over 7 years ago

Hi element14 Members.

 

I've been approached by several suppliers who are interested in having some of our members get creative and build something special out of a bunch of parts I would send you. Before I brainstorm on what could be built, let me roughly go through the parts that would be provided to each interested member. I don't have exact part numbers, so what follows is a general list that I would select specific parts based on the BOMs submitted to me. Here goes:

 

EBM Papst – Fan

Omron – Sensor / relays

Panasonic – Bluetooth module / relay

TracoPower – Power Supply

CamdenBoss – Bespoke enscloure

some SBC

Connectors  – Molex / Omron/ Panasonic (Dependent on which sensor & SBC we use)

Battery & Holder

 

Lots of parts! Here's what I think.

  • Fans-- this sounds like some kind of ventilation application, be it for the enclosure a standalone application.
  • Sensors-- first thought: what kind of sensors: more than likely, some kind of environmental sensors, which suggests a monitoring applications
  • Relays -- relay logic, load switching, auxiliary control, which suggest some kind of automation application
  • Power supply -- AC or DC?
  • Enclosures--portability? external environment? An application that's in the open environment?
  • SBC/RPI-- a controller with a wide range of possibilities. What do you want to control? How much load? How Fast? What kind of control loop do you need.
  • Connectors: interconnecting everything you are wiring up in the enclosure.
  • Battery and Holder-- if you aren't stationary, then you will probably need a battery and something to hold it.

 

At this point, what we need is a few system engineers to brainstorm with. I think I would focus on these themes:

 

  • Mobility
  • Remote Sensing
  • Cooling/Ventilation
  • Controlling something for a practical purpose (I'm trying to avoid saying industrial -- it means too many things)
  • Internet of Things--what data do you want to generate and why?

 

Here are my first brainstorming thoughts. What do you think? I'll check back to see what you come up with and respond.

 

Randall

  • Sign in to reply
  • Cancel
Parents
  • marshcmb
    marshcmb over 7 years ago

    Randall,

    When I saw this list I just had to become a member to tell you about an issue I've been thinking of trying to solve, that this parts list could really be used to help.

    I live in a hot environment. Where I work we are not allowed to bring personal electronics into the building. So, on those days where I go to the library to do some stuff I have to leave my computer(s) etc. in the trunk. By 5 PM, those devices are hot to the touch. I will bring them into the library, and give them time to cool down before turning them on. And while the equipment should be able to handle temperature changes, we have seen early death of cell phone that have to be left in cars.

    I am sure other have this problem when visiting client sites and similar situations.

    While I could drive around with a bunch of ice in the trunk, and let that cool the trunk while melting, I don't like the idea that there is no control of the temperature. What I thought of doing was putting two insulated chambers in the trunk. One to hold the ice or other passive coolant (gel packs, dry ice, etc), and the other to hold electronics. The two chambers would be connected by a ventilation hole with a fan. The fan would only operate when the chamber in the electronics side reaches a temperature configurable temperature range (let's say 95 - 105 F | 35 - 40 C perhaps).

    The communications would allow the driver to know the status of the system (temperature of the two chambers, humidity etc.) and you may even be able put in a small heat pump (if there are any to be had) to actively cool down the trunk when electricity is available.

    And the smarter the system, the more fun you can have (track temperatures over time; have a water pump if you are using ice; etc.

    And you can always use the two chambers to hold the venison on the weekend when you are taking it over to Gary's to make the jerky.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 7 years ago in reply to marshcmb

    You have a great project idea.

    Rather than ice, maybe try a hall effect cooler.

    I have a Hall Effect cooler that runs on DC, actually the cooler becomes a warmer if the polarity is swapped.

    It doesnt have any temperature adjustments, but your project could improve that part.

    Heck, you can add a solar panel in the rear window deck to supply the power and avoid killing your car battery.

    It wont likely get too hot if there is no sun.

    Maybe you can have a cooler chamber for electronics, and another for keeping your ice cream cold for the ride home.

    Your IOT connection can help you do data analysis for trunk cooler version 2, and alert you if there is a problem.

    Good luck !

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • robogary
    robogary over 7 years ago in reply to marshcmb

    You have a great project idea.

    Rather than ice, maybe try a hall effect cooler.

    I have a Hall Effect cooler that runs on DC, actually the cooler becomes a warmer if the polarity is swapped.

    It doesnt have any temperature adjustments, but your project could improve that part.

    Heck, you can add a solar panel in the rear window deck to supply the power and avoid killing your car battery.

    It wont likely get too hot if there is no sun.

    Maybe you can have a cooler chamber for electronics, and another for keeping your ice cream cold for the ride home.

    Your IOT connection can help you do data analysis for trunk cooler version 2, and alert you if there is a problem.

    Good luck !

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • robogary
    robogary over 7 years ago in reply to michaelkellett

    Thank you.

    I did mean Peltier, had a Hall Effect brain fart that day.  :-)  

    Appreciate the correction.

    Gary

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 7 years ago in reply to robogary

    I don't think you mean Hall effect but Peltier effect for the cooler.

     

    https://en.wikipedia.org/wiki/Hall_effect

     

    https://en.wikipedia.org/wiki/Thermoelectric_effect

     

    MK

    • Cancel
    • Vote Up +3 Vote Down