RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
RoadTest Forum What Would You Build If I Gave You an SBC, Sensors, Relays, Connectors, a Power Supply and an Enclosure?
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 2671 subscribers
  • Views 3386 views
  • Users 0 members are here
  • scasny
  • ind_tag
  • rpi
  • energy_power
  • rpi_projects
Related

What Would You Build If I Gave You an SBC, Sensors, Relays, Connectors, a Power Supply and an Enclosure?

rscasny
rscasny over 7 years ago

Hi element14 Members.

 

I've been approached by several suppliers who are interested in having some of our members get creative and build something special out of a bunch of parts I would send you. Before I brainstorm on what could be built, let me roughly go through the parts that would be provided to each interested member. I don't have exact part numbers, so what follows is a general list that I would select specific parts based on the BOMs submitted to me. Here goes:

 

EBM Papst – Fan

Omron – Sensor / relays

Panasonic – Bluetooth module / relay

TracoPower – Power Supply

CamdenBoss – Bespoke enscloure

some SBC

Connectors  – Molex / Omron/ Panasonic (Dependent on which sensor & SBC we use)

Battery & Holder

 

Lots of parts! Here's what I think.

  • Fans-- this sounds like some kind of ventilation application, be it for the enclosure a standalone application.
  • Sensors-- first thought: what kind of sensors: more than likely, some kind of environmental sensors, which suggests a monitoring applications
  • Relays -- relay logic, load switching, auxiliary control, which suggest some kind of automation application
  • Power supply -- AC or DC?
  • Enclosures--portability? external environment? An application that's in the open environment?
  • SBC/RPI-- a controller with a wide range of possibilities. What do you want to control? How much load? How Fast? What kind of control loop do you need.
  • Connectors: interconnecting everything you are wiring up in the enclosure.
  • Battery and Holder-- if you aren't stationary, then you will probably need a battery and something to hold it.

 

At this point, what we need is a few system engineers to brainstorm with. I think I would focus on these themes:

 

  • Mobility
  • Remote Sensing
  • Cooling/Ventilation
  • Controlling something for a practical purpose (I'm trying to avoid saying industrial -- it means too many things)
  • Internet of Things--what data do you want to generate and why?

 

Here are my first brainstorming thoughts. What do you think? I'll check back to see what you come up with and respond.

 

Randall

  • Sign in to reply
  • Cancel

Top Replies

  • rsc
    rsc over 7 years ago +11
    Time machine, of course. Scott
  • rsc
    rsc over 7 years ago +11
    Kinda looks like this box of stuff. RPi in a waterproof enclosure, 5VDC and 24VDC Power supplies, 40A SS relay, IMU sensor input, CAN bus output and BT keyboard.
  • luislabmo
    luislabmo over 7 years ago +8
    I agree with DAB , it is a broad list of components and so is the amount of things that can be build with them, but here are some ideas, I think all of them may require parts that are not covered: Some…
Parents
  • BigG
    BigG over 7 years ago

    The mention of peltier modules to create an active thermoelectric system sounds like a rather cool (or hot) idea. image

     

    I know outdoor CCTV enclosures typically require heater blowers to prevent condensation etc. Now as peltier modules can be used to cool things down or heat things up, I was thinking why not use two peliers - one to heat and one to cool (use a couple of NPN transistors or n-channel mosfets to power on/off either etc.) and together with a temperature sensor you should then be able to withstand high temperature during the day and low temperatures at night. In fact, you could also use the SBC to handle image capture as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • BigG
    BigG over 7 years ago

    The mention of peltier modules to create an active thermoelectric system sounds like a rather cool (or hot) idea. image

     

    I know outdoor CCTV enclosures typically require heater blowers to prevent condensation etc. Now as peltier modules can be used to cool things down or heat things up, I was thinking why not use two peliers - one to heat and one to cool (use a couple of NPN transistors or n-channel mosfets to power on/off either etc.) and together with a temperature sensor you should then be able to withstand high temperature during the day and low temperatures at night. In fact, you could also use the SBC to handle image capture as well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • michaelkellett
    michaelkellett over 7 years ago in reply to BigG

    You only need one Thermo Electric Cooler (TEC) and you can reverse the direction of operation electrically.

    TECs can be useful but they are not efficient - and they become less efficient as the temperature gradient increases.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago in reply to michaelkellett

    Thanks for that insight. Nice to learn something new today.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • geralds
    geralds over 7 years ago in reply to michaelkellett

    Yes, they are, like solar cells; calculated "PI-thumb finger".

    2010 I played with Peltier cells, that was very informative but at that time extremely expensive.

     

    I contacted once this manufacturer:

    https://tetech.com/peltier-thermoelectric-cooler-modules/

    Some information:

    https://tetech.com/downloads/

     

    Gerald

    ---