RoadTests & Reviews
  • Products
  • More
RoadTests & Reviews
Review Blogs Top Digital Protocol Evaluation --R&S RTM3K Oscilloscope Road-Test Review
  • Blogs
  • RoadTest Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
  • Share
  • More
  • Cancel
  • Author Author: snidhi
  • Date Created: 28 Jul 2018 10:58 PM Date Created
  • Views 794 views
  • Likes 8 likes
  • Comments 3 comments
Related
Recommended
  • rtm3004
  • logic analzyer
  • spi interface
  • i2c bus
  • rhode & schwartz oscilloscope
  • spi
  • spi decoding
  • uart
  • uart communication

Top Digital Protocol Evaluation --R&S RTM3K Oscilloscope Road-Test Review

snidhi
snidhi
28 Jul 2018

  • Top Hardware Features Evaluation
    • Setup the Oscilloscope for Measurements
    • Experimenting with the SPI Protocol
    • Testing the UART Protocol
    • I2C Protocol Measurements
    • Conclusion

 

Top Hardware Features Evaluation

 

This blog is in continuation from the Rohde & Schwarz Oscilloscope Kit RTM3K-COM4 - Review

 

Setup the Oscilloscope for Measurements

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Fig: Setup the oscilloscope for measurements

 

Experimenting with the SPI Protocol

 

SPI or serial peripheral interface is a four wire bus which is used in synchronous serial communication. The interface is popular with many sensors and was originally developed by Motorola in 1980s.

 

image

Fig: SPI communication

 

In this experiment to test the SPI protocol; I used a Raspberry Pi as the SPI master talking to an Adruino as the slave SPI.

 

image

image

Fig: Test Setup for the SPI Protocol

 

Measurement Results for SPI protocol. A data stream is sent continously from raspberry pi to the Adruino Uno board.

 

uint8_t tx[] = {
       0x55, 0xAA, 0x55, 0xAA, 0x55,
       0xAA,
       0x55, 0xAA, 0x55, 0xAA, 0x55,
       0x0A
};

 

image

Fig: Measurement Result as seen in RTM 3004

 

image

Fig: Result of the SPI Protocol

 

Testing the UART Protocol

 

A simple set up using the MBED board was used to measure the UART RX and TX as shown below.

 

image

Fig: Test Setup

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Fig: Setting up and Measuring the UART TX and RX

 

image

Fig: UART Measurement Result

I2C Protocol Measurements

 

Using the same setup as above I2C protocol was activated and measured as shown below.

 

image

 

image

Fig: I2C Protocol Measurement Results

Conclusion

Clearly the RTM 3004 offers many digital bus decoding protocols; some of which have been presented here. This scope acts as powerful tool for digital designer engineers.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 7 years ago +5
    Great write up! This is the feature that I most miss in my current oscilloscope, and the one that would most likely make me want to upgrade (or augment my current one). I even threw my hat in the ring…
  • snidhi
    snidhi over 7 years ago in reply to genebren +5
    Yes this oscilloscope is indeed a gem in its own right. The digital protocol is amazing. I had also the I2S audio protocol almost working but not quite well in the end. So I keep it for next time. Many…
  • jw0752
    jw0752 over 7 years ago +3
    Hi Sneha, Another excellent experiment on the capabilities of this scope. Thanks John
  • jw0752
    jw0752 over 7 years ago

    Hi Sneha,

    Another excellent experiment on the capabilities of this scope. Thanks

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 7 years ago in reply to genebren

    Yes this oscilloscope is indeed a gem in its own right.

    The digital protocol is amazing. I had also the I2S audio protocol almost working but not quite well in the end. So I keep it for next time.

     

    Many thanks for appreciating my efforts and enjoying my write-ups. It motivates me to keep going image but after a short break for now image

     

    Cheers

    SNidhi

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 7 years ago

    Great write up! This is the feature that I most miss in my current oscilloscope, and the one that would most likely make me want to upgrade (or augment my current one).  I even threw my hat in the ring to roadtest this one (the same that I remove in honor of the great roadtests that I have seen on this instrument).

     

    Gene

    • Cancel
    • Vote Up +5 Vote Down