AVNET Azure Sphere MT3620 Starter Kit

View table of contents ...  

image

Sign Up For the Webinar: IoT Skills: Learn How To Rapidly Secure Your IoT Design with Azure Sphere

 

 

{tabbedtable} Tab LabelTab Content
About

This RoadTest is an opportunity to test and experiment with an IoT microcontroller ecosystem from the device through connectivity to the cloud using the Avnet Azure Sphere MT3620 Starter Kit, the Azure Sphere O/S (based on open source Linux), and the Microsoft Azure IoT Hub.

 

Goals of this RoadTest

There are two goals for this Roadtest:

  • RoadTest the Device: RoadTesters will receive an Azure Sphere MT3620 Starter Kit to unbox, test, and build projects with. We want to you to test the device and put it through its paces.
  • RoadTest the Device to Cloud Connectivity: Roadtesters will take the Azure Sphere MT3620 and connect it to the Azure IoT Hub.  We want to test the cloud security and connectivity to gain insights into its use and capabilities from the point of view of an individual developer.

 

Kit Contents

RoadTesters will receive the AVNET Azure Sphere Starter kit which includes Carrier board with Azure Sphere MT3620 module, a USB Cable, and a Quick Start Card.

Avnet Azure Sphere MT3620 Starter Kit

The Avnet Azure Sphere MT3620 Starter Kit supports rapid prototyping of highly secure, end-to-end IoT implementations using Microsoft’s Azure Sphere--a solution for creating highly-secured, connected Microcontroller (MCU) devices,

 

The kit includes a small form-factor carrier board, featuring a production-ready MT3620 Sphere module, based on the MT3620 SoC, which has built-in Microsoft security, Wi-Fi connectivity, and the combined versatility and power of an Arm® Cortex™-A7 processor with the low overhead and real-time guarantees of two Arm Cortex-M4F microcontrollers.

image

 

The carrier board connects the Sphere module I/Os to two MikroE Click sockets, an I2C Grove connector, a connector supporting the addition of a 128 x 64 OLED graphical display, a 3D accelerometer, 3D Gyro, temperature sensor, and an ambient light sensor. Debugging is accomplished through a USB-to-UART interface, which also provides the necessary 5V power for the board.

 

User applications for the embedded Sphere controller are developed in C using Microsoft’s Visual Studio IDE and the Azure Sphere SDK. The combination of Visual Studio, the versatile carrier card, and the production ready Sphere module delivers a powerful starting point for IoT developers interested in learning, prototyping, and deploying Azure Sphere based solutions.

 

Additional Information

 

Azure Sphere MT3620 Modules

The Avnet Azure Sphere MT3620 Modules support Microsoft’s Azure Sphere end-to-end solution for highly-secured, WiFi connected Microcontroller (MCU) devices. The production-ready, certified modules come in two versions; an on-board chip antenna module for cost-optimized systems, and an external U.FL antenna module supporting two external antennas for applications requiring higher performance, external antennas. Both modules are pin and footprint compatible, allowing for easy design migration and end-product enhancements.

image

By integrating all the necessary support and RF front end circuitry onto the small 33 mm x 22 mm module, design time has been reduced for implementing Sphere-based solutions. More importantly, developers can leverage the modules wireless certifications (pending) for their end-product, saving considerable certification costs and testing time.

image

The Azure Sphere MT3620 modules are based on the MT3620AN SoC, which supports dual-band 802.11 a/b/g/n WiFi connectivity, a 500 MHz Arm® Cortex™-A7 core for user applications, and two general purpose 200MHz Arm Cortex-M4F I/O subsystem cores designed to support real-time requirements. The on-chip peripherals (GPIO, UART, I2C, SPI, PWM and ADC) can be mapped to dedicated I/O pins on the module for connection to external sensors, I/O connectors, or other user application circuits.

 

Additional Information

Important Dates

Enrollment Begin: June 4 2019

Enrollment Ends: June 30 2019

RoadTesters Selected: Aug 5 2019

Product Shipped: Aug 8 2019

RoadTesting Begins: Aug 15 2019

Reminder/Update Email: Sept 15 2019

Submit Reviews By: Oct 15 2019

*The element14 RoadTest Staff will send this reminder/update email.

**If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Manager, , as soon as possible before the deadline.

RoadTesters

deadline Nov 10 2019

Terms and Conditions

Terms and Conditions: AVNET Azure Sphere MT3620 Starter Kit RoadTest

 

These are the terms and conditions which govern the AVNET Azure Sphere MT3620 Starter Kit RoadTest contest. This Contest requires participants to submit an application indicating their previous experience with this type of equipment/component, information on what they would do to test the equipment or component, and the applicant’s desire to post a thorough review of their experience with images, photos, or other supplemental materials. Participants will be required to meet the Conditions for Participation.  The winners of this RoadTest will receive the item(s) listed below. RoadTest Reviews are due no later than 45 days after the receipt of the item(s). No other prizes are offered.

The Principal terms of the Competition

The following words and phrases are used in these terms and conditions and have the meanings given to them below.

Key dates:

Applications Close: 9 PM (GMT) on June 30 2019

Announcement of Winner (estimated): July 8 2019

Prize: AVNET Azure Sphere MT3620 Starter Kit

Competition Site: https://www.element14.com/community/groups/roadtest?ICID=menubar_resources_roadtest

Site or element14 Community: www.element14.com/community

Judges: members of the element14 community team chosen at the Organiser’s discretion.

Judging Criteria, All of the following which will have equal weighting:

· Demonstrated competence with the technologies including links or descriptions of past projects

· Qualifications as indicated by current job role and/or schooling/vocational training;

· A thorough description of how the prize would be tested;

· Likelihood that the Applicant will blog about the prize and provide a review on element14.com;

· Originality;

· Innovation.

Organiser: Premier Farnell plc (registered in England and Wales under company number 876412) whose registered office is at Farnell House, Forge Lane, Leeds, UK

Conditions for Qualification: in addition to meeting the requirements of these terms, all persons applying to take part in the Contest (each one an Applicant) must:

· Provide a RoadTest application describing what he/she would do if awarded the Prize including similar previous projects, product experience and qualifications

Terms: these terms and conditions which govern the Competition and to which the Organiser reserves the right to make changes from time to time and the latest version of these Terms from time to time will be posted to the Site.

Eligibility

Applications:

Selecting Winners:

Liability:

General:

1.1 Save as set out in these Terms, the Contest is open to any natural or legal person, firm or company or group of natural persons or unincorporated body.

1.2 All Applicants must be aged at least 18 at the time of their application.

1.3 Applicants must not enter the RoadTest if doing so or taking part may:

1.3.1 cause the Organiser and/or themselves to be in breach of any agreement (including but not limited to any contract of employment) to which they are a party or in breach of any law, regulation or rule having the force of law to which the Organiser or the Applicant may be subject or any policy of the Organiser or the Sponsor;

1.3.2 Require the Organiser to obtain any licence, authorisation or permission to deal with the Applicant; or

1.3.3 Be in breach of any policy or practice of their employer. Some employers prohibit or restrict their employees from taking part in competitions such as these or receiving prizes under them and the Organiser respects those policies and practices.

The Organiser reserves the right to disqualify any Application made in breach of these Terms and to reject any Application which it reasonably believes may be or become in breach. The Organiser reserves the right to require evidence in such form as the Organiser may reasonably require of any Applicant’s compliance with any of these Terms and to disqualify any Applicant or Participant who cannot provide such evidence reasonably promptly.

1.4 Multiple applications are not permitted.

1.5 Applications may not be submitted by an agent whether acting on behalf of an undisclosed principal or otherwise.

1.6 The Contest is NOT open to:

1.6.1 Any person or entity who is a resident or national of any country which is subject to sanctions, embargoes or national trade restrictions of the United States of America, the European Union or the United Kingdom;

1.6.2 Any employee, director, member, shareholder (as appropriate) or any of their direct families (parents, siblings, spouse, partner, children) (“Direct Families”) of the Organiser and Sponsors; or

2.1 Each Applicant must fully complete and submit a RoadTest Application by the Application Close.

2.2 By submitting a Registration Form, each Applicant:

2.2.1 Authorises the Organiser to use his or her personal data (as defined in the Data Protection Act 1998) for the purposes of running and promoting the RoadTest;

2.2.2 Authorises the Organizer to copy, reproduce and publish their application should they be accepted as a Participant;

2.2.3 Will be deemed to have read, accepted and agree to be bound by these Terms. Applicants are advised to print and keep safe these Terms;

2.2.4 Authorises the Organiser to copy, reproduce and use the Application and/or Review for the purposes of the RoadTest and as otherwise contemplated by these Terms. The Organiser will not be responsible for any inaccuracy, error or omission contained in any reproduction or use of the Project Blogs.

2.2.5 Licenses the Organiser to use the intellectual property in the Project (IP) for the purposes of this Contest. As between the Applicant and the Organiser the IP remains owned by the Applicant.

2.2.6 Grants the Organiser the right to use his or her likeness, photographs, logos, trademarks, audio or video recordings without restriction for the purposes of Contest or the promotion of it or the Site;

2.2.7 Agrees to participate positively in all publicity surrounding the Contest;

2.2.8 Agrees to be responsible for all expenses and costs incurred by him or her in preparing for, entering and participating in the Contest (save for any expenses expressly agreed by the Organiser to be borne by it in these Terms);

2.2.9 Confirms that he or she owns all IP used in his or her application or Project or Blogs and indemnifies the Organiser from any claim by a third party that use of any material provided by an Applicant to the Organiser infringes the intellectual property rights of any third party;

2.2.10 Agrees not to act in any way or fail to act in any way or be associated with any cause or group which would have a negative impact on the reputation of the Organiser and/or the RoadTest.

2.3 All applications submitted to this RoadTest must meet the following criteria:

2.3.1 Applicants must be the author, creator and owner of the proposed review idea. Applicants must not submit someone else’s idea;

2.3.2 The proposed application must be reasonably achievable by the within the time constraints of the Contest;

2.3.3 Applications must not include or propose any of the following, the inclusion of which shall render any proposed application ineligible:

(a) Applications which relate to socially taboo topics, such as illicit drug use or sexual gratification;

(b) Applications that are or could reasonably be considered to be illegal, immoral, discriminatory or offensive as determined by the Organiser;

(c) Applications in relation to them which if accepted would infringe or breach any of the policies or terms of access or use of the Site.

2.4 No Application may contain any of the hazardous substances identified by Article 4 of Directive 2002/95/EC of the European Parliament on the Restrictions on the Use of Substances in Electronic and Electrical Equipment ("the Directive") or the use of such hazardous substances in the in any such Project must not exceed the maximum concentration values set out in the Directive.

3.1 Winners will be selected by the Organiser on the basis of the quality of his or her application and its adherence to these Terms.

3.2 The total number of Winners selected will be at least the minimum number set out above but the actual number is at the sole discretion of the Organizer and/or the Sponsor, if applicable.

3.3 The Organiser will use all reasonable efforts to announce the Winners via an update to the RoadTest page by the date listed above.

3.4 Winners agree to take part in all publicity which the Organiser or the Sponsor wishes to use to promote the RoadTest, the Products featured or other Contests with which the Organiser may be connected from time to time.

3.5 Details of the Winners may also be published in the media.

3.6 Winners are responsible for all applicable taxes, duties or other charges payable in relation to any prize.

3.7

4.1 The Organiser hereby excludes all and any Liability arising out of the Contest or the acceptance, use, quality, condition, suitability or performance of any Prize, even where that Liability may arise from the Organiser’s negligence.

4.2 Nothing in these Terms will affect any Liability of the Organiser for death or personal injury arising from its negligence, for breach of Part II of the Consumer Protection Act 1987 (in the event that any entrant is entitled to claim rights under the Consumer Protection Act 1987) or for any matter in relation to which it would be illegal for the Organiser to exclude or to attempt to exclude its Liability.

4.3 Subject to 4.2, neither the Organiser, any parent company nor any subsidiary of the Organiser or such parent company or any of their directors, officers and employees (together referred to in these terms and the ‘Associates’) makes any guarantee, warranty or representation of any kind, express or implied, with respect to this Competition or the Prizes potentially available under it. Neither the Organiser nor any of its Associates shall be responsible for any Liability that may arise out of or in connection with person’s participation in this Competition, the claiming, redemption or value of any prizes under it, the use or enjoyment of such prizes or any events or circumstances arising out of or in connection with any of them. Any implied warranties of condition, merchantability or suitability or fitness for purpose of any of them are hereby expressly excluded. Wherever used in these Terms, ‘Liability’ shall mean any and all costs, expenses, claims, damages, actions, proceedings, demands, losses and other liabilities (including legal fees and costs on a full indemnity basis) arising directly or indirectly out of or in connection with the matter concerned.

5.1 The RoadTest is organised and sponsored by the Organiser. The Organiser reserves the right to delegate all or any of its powers, rights and obligations arising in relation to the RoadTest to any Associate and certain such rights and powers are assumed by the Organiser on behalf of itself and each Associate. Reference to “Organiser” shall be deemed to include reference to each Associate.

5.2 The RoadTest may be terminated at any time if there are, in the sole opinion of the Organiser, an insufficient number of entries, or if the Applications are not of an appropriate standard for a competition of this nature. The Organiser has the right to cancel or suspend the RoadTest at any time due to circumstances outside its reasonable control.

5.3 The Organiser shall have the sole discretion to disqualify (without correspondence or right of appeal) any Applicant it considers to be adversely affecting the process or the operation of the RoadTest or to be in breach of these Terms or to be acting in a disruptive manner or with intent to annoy, abuse, threaten or harass any other Applicant or Participant.

5.4 The Organiser has the right to amend or add to these Terms from time to time. Revised Terms and Conditions will be posted on the Contest Site and it is a condition of entry to the RoadTest that Applicants agree to comply with these Terms and, if appropriate, such Terms as amended from time to time.

5.5 Headings are for convenience only and do not affect the interpretation or construction of these Terms and Conditions.

5.6 These Terms and the operation of the Contest shall be governed by and construed in accordance with English Law and any claim or matter arising under these Terms shall be subject to the exclusive jurisdiction of the English courts.

RoadTest Reviews
Comments
Anonymous
  • I was on vacation last week. Sorry that I wasn't able to respond to the Acceptance email until today.  image

  • Sure this clarifies, and not only, I think you are aware I will know this aspect. The point is that I read that someone was complaining – not respect your choice – about the problem of the need for a specific platform. I already was having in mind to publish this same note on the other post; I think that as some user read that it is required a windows 10 machine this may block them to participate to the challenge. I suppose this is a way to avoid this problem, for all the interested users, I mean.

     

    Enrico

  • Enrico,

     

    I have not passed on selecting an applicant because of their platform. I actually did select him. After that, he came back to me about his platform. And I told him to post a comment so other members or roadtesters could make a determination. I wanted the answer in public view anyway. In the end, he contacted me and decided not to roadtest at the present time.

     

    What I do require is when I send out the notification email that you are a finalist the applicant has to respond. I will not send out any product unless someone responds to me.

     

    Does that clarify things?

     

    Randall

  • Hello Randy,

     

    I think you are not correct, just to avoid that someone does not enroll due to his platform. Despite I have Max OSX as my main working and development platform I also work with Windows 7 and Windows 10. But based on my experience as most of the hardware development environments are not all compatible when running together I always prefer running different versions of Windows tailored on the specific development environment I will use. For example, a machine where the Visual studio components are setup for Arduino and AVR boards to develop with Atmel Studio has a lot of problems working together with Cypress PSoC Creator, also based on Visual Studio but with different plugins and components. And so on, without considering some licensed software that runs on Windows only like Altium Circuit Studio etc. So I have my collection of VM that I can install (copy) also on different computers.

     

    But the interesting part has to arrive. As usual, I was thinking to prepare a Windows10 clean machine resigned to setup the installation of all the components when instead I found an interesting note on the Microsoft Site on getting started with the AVNet board. They released a 20 Gb (17 Gb download in zip file) version of a Virtual Machine with a Windows1 10 Enterprise developer edition with all the components already setup ready to start developing with the Azure board. The Virtual Machine is downloadable for free (runs on any platform) and the available versions are VMWare, Parallel and VirtualBox (that is free for whom who don't own a commercial license of one of the other two).

     

    The virtual machine includes Visual studio 2019, the drivers and all that is needed. I am approaching now to test it on my Macbook Pro. Then I will post some update.

     

    The link is the following: https://developer.microsoft.com/en-us/windows/downloads/virtual-machines

     

    Enrico

  • I did select 50 people--there were a lot of decent applications.

     

    But if someone who is selected DOES NOT respond to my notification email, I assume that (a) they are not interested or (b) they are hard to communicate with. If I can't communicate with them easily, they are not ideal roadtesters. The supplier often has questions and I need to be able to communicate and get a response from a roadtester in a prompt manner.

     

    Bottomline, I have to pick 17 more applicants.

     

    Randall

  • You could be right, Gough. Only the man himself knows for sure. On the MicroZed road test only one of the original 5 kits were sent out.

  • Leading the Phase 1 check-in leaderboard and now selected for the RoadTest as well ... and I'm still not yet at my 15-day requirement. Looks like you're doing well !

     

    From my reading, I suspect Randall chose 50 applicants and sent out all the e-mails, but of those, only 33 managed to reply and are listed above. The remainder will have to go to reserve applicants, hence they will be filled in as Randall gets affirmative replies from the other applicants.

     

    - Gough

  • I appreciate being selected for this road test. There seem to be a few people struggling to get to grips with this device due to the competitions going on at the moment. And it looked like the flood will continue as the stock catches up with the demand. I might try to get something out quickly that will help with this and then fill it out with more detail as my own experience progresses.

  • Dixon,

     

    I think that 33 is the full list. I'm sure Randall will correct if I'm wrong, but it seems the new approach is to reduce the number sent out if the applications don't seem likely to result in a completed road test. It sounds like a sensible idea, but it is shocking that our of 407 applications there weren't 50 that were adequate. There must be some absolute stinkers in there!. Thanks for doing a tough job, Randall.

  • Hello , I am already working on the challenge; as I plan to add the board possibility to interface with IoT projects for both Arduino and Raspberry Pi based applications in the two books, if you need someone to road test the board under the perspective of the application possibilities depicting a hopefully complete scenario – or at least wide – in terms of projects applications I am available. Consider that both the Pi and this board roadtest for editorial needs, as you know, will be complete around the mid-end of the month of September.

     

    Enrico

  • Thanks for the selection . Congratulations to the other selected road testers. Lucky are are the new 17 to be selected.

     

    The list has many new road testers (obviously it will when the number of Road Test units is 50) and that is wonderful. Great if we get back 50 out of 50 reviews.

  • Important Dates Update

    Enrollment Begin: June 4 2019

    Enrollment Ends: June 30 2019

    RoadTesters Selected: Aug 5 2019

    Product Shipped: Aug 8 2019

    RoadTesting Begins: Aug 15 2019

    Reminder/Update Email: Sept 15 2019

    Submit Reviews By: Oct 15 2019

    *The element14 RoadTest Staff will send this reminder/update email.

    **If a RoadTester is unable to meet the deadline, please notify the RoadTest Program Manager, , as soon as possible before the deadline.

     

     

     

     

  • The following applicants have been selected as official roadtsters:

     

     

     

     

     

     

    If you count the above lists, you will see that it only comes up to 33. The reason why is 17 of the 55 I sent notification emails have not responded. So, I'll being selected an alternate 17 applicants. Please respond to my notification email. It serves two purposes: #1 notifies you and verifies you are available and #2 shows me that I can get in touch wih you if I need to.

     

    Randall Scasny

    RoadTest Program Manager

  • Yes, you will need Windows 10 Anniversary Edition or later, Visual Studio 2019 or later, as per https://docs.microsoft.com/en-us/azure-sphere/install/install

     

    - Gough

  • Yes. You need Windows and Visual Studio.

  • In order to complete the roadtest, do I need a Windows machine?  I have upgraded to Catalina beta on my MacBook and this has temporarily broken VMware and VirtualBox, so I currently have no access to Windows.

  •   wrote:

    I felt some projects were at least 6 months long; a couple were more than that.

    I would guess the ones that promise the earth are the ones that will take the "freebie" and never be heard from again. You must be getting a feel for what sort applicants are good by now. In fact this large dataset of 407 entries (and the similar Pi 4 one) might be good for fine-tuning that.

  • There were fewer incomplete applications than usual, so that's a good sign.

     

    I found there were a lot more complex projects proposed than for most roadtests, as well as applicationsfrom people who wanted to integrate the Azure Sphere ecosystem into something they are working on now, which is great!

    This is good news to hear and 407 applications is a lot to read!

  • To all Applicants.

     

    I read ALL 407 applications.

     

    There were fewer incomplete applications than usual, so that's a good sign.

     

    I found there were a lot more complex projects proposed than for most roadtests, as well as applicationsfrom people who wanted to integrate the Azure Sphere ecosystem into something they are working on now, which is great!

     

    For the first cut, I selected 89 applications out of 407.

     

    I'll work on the 2nd cut. I should post it by tomorrow.

     

    The last comment I have is about time.

     

    Roadtests are 60 days long. That's how the program is structured. If you proposed a much longer timeline, and you are selected as an official roadtester, you will still need to post a review within the 60-day timeframe. In this situation, you can begin the review by summarizing the entire project, say, by phases (e.g. 1, 2, 3, etc.). If you only complete Phase 1, that's okay. Write about phase 1 in detail. Then, make a conclusion about the product based upon what you tested.

     

    I felt some projects were at least 6 months long; a couple were more than that.

     

    Randall Scasny

    RoadTest Program Manager

  • Thank you and for the explanation. Now I am relieved!