MPS MA732 MagAlpha Angle Sensor Kit with Servo Motor - Industrial Sensing

View table of contents ...  

Summary

The TBMA732-Q-RD-00A is the round-version test board for the MagAlpha magnetic position angle sensor MA732. The MA732 sensor detects the absolute angular position of a permanent magnet, typically a diametrically magnetized cylinder on a rotating shaft. It comes mounted on a fully integrated smart motor solution for servo motor applications (EVKT-MSM942038-24). The MA732 is used for general purpose angle measurement, or on devices such as Angle Encoders, Automotive Angle or Speed Sensors, and Robotics.

RoadTest Goal

We want the roadtester to evaluate the MA 732: a 14-Bit, Digital, Contactless Angle Sensor with ABZ Incremental & PWM Outputs. It is capable of fast data acquisition & processing to provide accurate angle measurements at speeds from 0 to 60,000 rpm. The sponsor has prepared a testing and setup procedure (see next section) for ease of use for a hobbyist.

Discussion

How Would You RoadTest the MagAlpha Angle Sensor Kit?

Test Procedure

This kit comes with a servo BLDC motor which can be driven in speed or position mode via RS485. Attached to the rotor is a diametrically magnetized magnet which rotates with the motor rotor. Above this magnet is an MA702 with a 1-2 mm airgap.

Download the following document prepared for this roadtest on how the MA702 angle sensor can be read / evaluated. Instructions for running the motor via an Arduino MEGA and RS485 driver are included.

(MA732 Roadtest Setup Guide and Getting Started)

(MSM zip folder)

Product Variants

MPS offers several product variants:

MA735 MA780 MA820 MA310
MA736 MA782 MA704 MA302
MA734 MAQ470 MA730 MA102
MA732 MAQ430 MA710 MA850
MAQ473 MA800 MA702 MA330

MA732 - This is the product variant used for this roadtest.

Kit Contents

  • TBMA732-Q-RD-00A -- round-version test board for the MagAlpha magnetic position angle sensor MA732, which is mounted on the servo motor
  • eMotion SystemTM Smart Motor Module--servo motor kit
  • Communications kit (EVKT-MACOM)
  • Anmbest RS485 Interface board
  • Arduino Mega2560

Hardware Technical Description

The MPS MagAlpha family of magnetic angle position sensors offers a revolutionary way to measure angles. The MagAlpha range offers unique performance advantages compared to rival magnetic sensing technologies.

MagAlpha sensors use the patented SpinAxisTM Hall measurement technique that provides instantaneous angle position in a digital format. SpinAxisTM uses a phase detection approach that eliminates any need for analog to digital conversion or complex angle calculation used by more traditional technologies. Click here for more information.

MA732 Angular Position Sensor

The MA732 detects the absolute angular position of a permanent magnet, typically a diametrically magnetized cylinder on a rotating shaft. Fast data acquisition and processing provide accurate angle measurements at speeds from 0 to 60,000 rpm. The digital filtering is adjustable to optimize control loop performance when used in servo applications.

The MA732 supports a wide range of magnetic field strengths and spatial configurations. Both end-of-shaft and off-axis (side-shaft mounting) configurations are supported.

The MA732 features magnetic field strength detection with programmable thresholds to allow sensing of the magnet position relative to the sensor for creation of functions, such as the sensing of axial movements or for diagnostics.

On-chip non-volatile memory provides storage for configuration parameters, including the reference zero angle position, ABZ encoder settings, and magnetic field detection thresholds. Click here for more information: 

Features

  • 9-Bit to 14-Bit Resolution Absolute Angle Encoder
  • Contactless Sensing for Long Life
  • SPI Serial Interface for Digital Angle Readout and Chip Configuration
  • Incremental 12-Bit ABZ Quadrature Encoder Interface with Programmable Pulses Per Turn from 1 - 1024
  • PWM Output 14-Bit
  • Programmable Magnetic Field Strength Detection for Diagnostic Checks
  • 3V, 12mA Supply
  • -40°C to +125°C Operating Temperature
  • Available in a QFN-16 (3mmx3mm) Package

TBMA732-Q-RD-00A Round Eval Board for MA732

The TBMA732-Q-RD-00A is the round test board for the MagAlpha magnetic position sensor MA732. This configuration is used for end shaft sensing.

It requires the communications kit (EVKT-MACOM) and the Macom App Software (see below) to evaluate MagAlpha functionality and performance with your set-up, such as noise level, refresh rate, power-up time, and magnetic field dependence.

In addition to this round test board, there is a long format version (LT) where the sensor is mounted on the edge of the board and can therefore be used in both side-shaft and end-of-shaft configurations. Click here for more information.

EVKT-MACOM MagAlpha Communication Kit

The EVKT-MACOM is a communication kit for the MagAlpha magnetic position sensor family. The EVKT-MACOM offers a seamless

connection and operation with MagAlpha test boards (TBMA) and evaluation kits (EVKTKNOB). The EVKT-MACOM kit contains a microcontroller motherboard, a collection of daughter boards adapted to different sensor boards, and the related cables. For more information CLICK HERE

Software

  • No Software Licenses
  • Use documentation in Test Procedure Section

Additional Information

Important Dates 

Begin enrollment: June 24, 2022
End enrollment: July 24, 2022
Select RoadTesters: July 29, 2022
Ship unit date: Aug 16 2022
Begin RoadTesting: Aug 23 2022
Element14 follow up: Sept 23 2022
Post Reviews by: Oct 23 2022

Terms and Conditions

Click Here to read the Terms and Conditions.

RoadTesters

shabaz due date Oct 23 2022

Guillaume_Martin due date Oct 23 2022

bac2348 due date Oct 23 2022

Cristi due date Oct 26 2022

DaveTheWalker due date Oct 26 2022

RoadTest Reviews
Comments
Anonymous
  • Interesting kit but I can't buy it anymore on Farnell. Is there another way to get this kit?

  • Hi,

    To anyone working on this RoadTest, or to anyone who comes across the motor supplied as part of the kit;

    there are some bugs in the source code, here are the changes that are needed to the MSM.cpp file:

    In the writeReg function:

    Change:

    msgBuf[0]= BROAD_SA<<1;
    msgBuf[1]= (regAdd<<1) + 1;

    to:

    msgBuf[0]= (BROAD_SA<<1) | 0x01;
    msgBuf[1]= (regAdd<<1) | 0x01;

    In the readReg function:

    Change:

    msgBuf[0] = BROAD_SA << 1;
    msgBuf[1] = regAdd << 1;

    to:

    msgBuf[0] = (BROAD_SA << 1) | 0x01;
    msgBuf[1] = (regAdd << 1) & 0xfe;

    Note that even when you make the changes, the readReg function might not work (it didn't for me), however it's not necessary for the RoadTest (it's not core to anything, since all that's important is writing to the motor controller, not reading from it). But if you solve the readReg, do let me know since I'm curious.

    Also, I have not tested this on the Arduino environment (I used a Pico instead). But the exact same change would be needed for Arduino too; I can't see that it can work without the changes. With the changes, I can successfully control the motor.

  • Maybe you just don't see it going to the asked position and look when it's already locked. The function available in the library has a revolutions count parameter. You could try setting it to something big. You would probably be able to see it moving before locking into position.

  • Hello! For those who received the kit recently, can you tell me if the sketch with the motor position control works for you? 

    The motor shaft does not rotate at all.

    *The sketch with the speed control works.

  • Guillaume_Martin helped me out with a tip.  You can comment out the "#include "Base.h"" line from the MSM.h file.

    I had actually tried this before, but hit a load more compiler errors and gave up... but I should have read the errors!  It turns out that MSM.cpp is missing the leading "#" from "#include "MSM.h"".  If you reinstate that, it all compiles OK.

    Thanks for the help .  I hope other people can make it work, as well Slight smile

  • I'm trying to work through this roadtest but I have hit an issue.  When I come to try the MSM sketches, I get the error:

    Arduino: 1.8.19 (Windows Store 1.8.57.0) (Windows 10), Board: "Arduino Mega or Mega 2560, ATmega2560 (Mega 2560)"

    In file included from C:\Users\davet\OneDrive\Documents\Arduino\libraries\MSM\examples\Speed_mode\Speed_mode.pde:4:0:
    C:\Users\davet\OneDrive\Documents\Arduino\libraries\MSM/MSM.h:10:10: fatal error: Base.h: No such file or directory
    #include "Base.h"
    ^~~~~~~~
    compilation terminated.
    exit status 1
    Error compiling for board Arduino Mega or Mega 2560.

    From which library does Base.h come?  I haven't been able to find it in the Library manager.

  • I guess they could be at slightly different heights too, so they would never hit each other even if synchronization wasn't good.

  • I had a wild thought, if the angle position regulation was really good, two propellers could be in close proximity to get extra lift in a small space.

    image

  • The sponsor write a special setting up guide for this roadtest. The link is above, but I'll repost it here:

    /products/roadtest/m/files/146190

    One roadtest option would be to set up the kit and write a review based on that.

    Randall

  • This could be a real problem-solver for wood/metalworking, and workshops! There are a ton of tools that need precise positioning, and not everyone is CNC-ready, I'm not.

    I'm wondering if it could be used to measure milling machine axes.

    Basically, such tools have three wheels you're supposed to manually rotate, to move the X, Y or Z axes.

    On my machine, one full turn corresponds to 2mm of axis movement.

    So, if I'm cutting a 20.5 mm long slot, with a 4 mm diameter tool (similar to a drill bit but slightly different), then I need to mentally subtract 4mm from 20.5mm, which gives me 16.5mm, and then I need to turn the wheel 8 and one quarter turn. You can imagine that errors can occur, if you miscalculate or forget how much you have turned : ) Also, you're not necessarily turning the wheel from a set position, because you have to compensate for any backlash (often plenty of that in low-cost tools), so some subtraction is needed for the offset.

    It would be awesome to be able to punch in your tool diameter, and the distance you wish to cut, and then just rotate the wheel until (say) it beeps rapidly and then continuously, like a car reversing indicator : )

    A full-blown digital readout (DRO) would be neat too, but that's a bit more of a major project.

  • Put 4 of these babies on a drone and fly to new heights

  • Go for it :). By the time this kit would arrive, the due date for the Spartan-7 blogs has passed.

  • This seems to be an interesting roadtest!
    I would definitely try applying for this one and try out my luck. Just need to finish the spartan 7 blogs before applying for any other design contests/roadtests.

  • Have you considered promoting this RoadTest on main page? In case of MTi-680 there were 3 applications before if I remmeber correctly and after promotion on home page, number of applicants increased 4× (which is still quite a low, but it is much better than 3). MTi-680it enrollment period ends in 5 days, It would be nice to replace banner with banner for this RoadTest after enrollment period end.

    I am considering applying but I am busy with other tasks, have no (or very few) experimence with motors yet and also It is hard to imagine what I can motorize in my lab. In case when there will be low count of applications at the end of enrollment period I maybe I will try apply with applicaiton based on basic tests without any funny and interesting motor control application.

  • I agree.  Initially, the roadtest didn't have everything needed. So, we regrouped and with the sponsor's assistance put together this kit. While this is a motor control kit, the sponsor would like to get some feedback on the magnetic angular sensor. The roadtest program hasn't roadtested any angular rotation sensors,  but they are a key component. So, if anyone in the community is up for this roadtest, I think it would be an interesting roadtest.

    Randall

  • I am really surprised there don't seem to be a lot of applicants (so far).

    The kit includes is a great motor, great motor controller, great sensor, and they come with an Arduino Mega plus communications link.

    This has to be one of the easiest and most complete motor kits I've ever seen.

  • Ooooooooooooo pwm output, quadature output, and spi. This looks pretty sweet . 

    60k rpm is smoking fast, glad it has selectable ppr. 

  • Apologies for the broken links; after I generated the document, I forgot to go back and relink to the appropriate sections.

    You are correct that all references should be to MA732. The MA702 is the same part (drop in replacement) but without the capability to adjust the back end filter. The default filter setting for the MA732 make it behave exactly as the MA702.

    If you have any questions while experimenting with the setup, feel free to contact me. 

  • I have looked at this Roadtest about 5 months ago when it appeared first time and now it looks much better and more attractive to me. While last time I spend few hours with learning what is this sensor used for, how to use them and so on, now this is much clearer.

    It is nice to see that vendor spend (lot of time) and wrote 30 pages setup guide for Roadtesters. This makes able to apply even total beginners in this area. I think it would be helpful to other MPS customers. Have MPS considered providing the same resources to their customer in the form of some application note or something like this after RoadTest? I also welcome that they spend time with writing Arduino Library for motor control. If I understand it correctly, we received two boards with MCU:

    1) Board with NXP Arm as part of TBMA732-Q-RD-00A used for accessing MA732 sensor features through EVKT-MACOM from software.
    2) Arduino for controlling motor and making some motion sensible by the sensor

    On this RoadTest page I see some confusion of mixing MA702 and MA732 numbers. They most probably come from document provided by MPS. They mention 732 in title but first two paragraphs they mention 702. 702 is different sensor from the same family if I understood it correctly. I think MA732 should be there on all places, shouldn't be?

    In document in sections 2.1.2, 2.2.2 and 2.3.2 are broken links replaced by "Error! Reference source not found.."