AMD Xilinx Kria KV260 Vision AI Starter Kit

View table of contents ...  

RoadTest Goals
A) Produce a 2 to 3 minute unboxing video. Here are two examples: Example 1 Example 2
B) Test the out-of-box experience of the product.
C) Build a project and show how you did it.

Product Variants
• SK-KV260-G — this is the one used in this roadtest
• SK-KV260-G-ED

Description

The first starter kit in the KriaTm portfolio, the KV260 Vision AI Starter Kit is an out-ofthe-box platform for advanced vision application development. It is equipped with a non-production version of the production K26 SOM. This SOM and fansink are mounted to an evaluation carrier card optimized for vision applications, featuring multi-camera support via ON Semiconductor Imager Access System (IAS) and Raspberry Pi connectors. Enabled by a growing ecosystem of accelerated applications for the KV260 Vision AI Starter Kit, developers of all types can get applications up and running in under 1 hour, with no FPGA experience needed. From there, customization and differentiation can be added via preferred design environments, at any level of abstraction—from application software to AI model to FPGA design. With both hardware and software development requirements simplified, the KV260 Vision AI Starter Kit is the fastest and easiest platform for application development with the goal of volume deployment on Kria K26 SOMs.

Features

Kit Contents

  • KV260 Development platform for Kria K26 SOMs
  • Accessory pack for the Kria KV260 Vision AI Starter Kit:
    • KV260 Power Supply & Adapter
    • USB-A to micro-B Cable
    • Ethernet Cable
    • HDMI Cable (Male to Male)
    • MicroSD card and MicroSD to SD Adapter
    • 13MP Auto Focus RGB Camera Module

Additional Information
• Product Brief
• Datasheet
• User Guide
• Getting Started Guide
• Github Applications
• Kria SOM Github
• Avnet Page Brief
• Getting Started Video

Important Dates 

Begin enrollment:  Nov 30 2022
End enrollment:  Dec 30 2022
Select roadtesters:  Jan 3 2023
Ship unit: Jan 26 2023
Begin Roadtesting:  Jan 27 2023
Element14 follow up: Feb 27, 2023
Post Reviews by:  Mar 27, 2023

Official Roadtesters

  • feiticeir0  (due date April 17)
  • skruglewicz (due date Mar 27)
  • digital_pat (due date Mar 27)
  • jasonwier92 (due date Mar 27)
  • work14 (suspend due date as of Feb 28th; roadtester reported board failure)

Terms and Conditions
Click Here to read the Terms and Conditions.

RoadTest Reviews
Comments
Anonymous
  • It is a bummer you are having an issue with your board.  The video interface is a nice feature, but is not needed for all of the samples provided by Xilinx.  I would suggest trying to get the smart camera app up and running since this app had not dependency on the HDMI/DisplayPort monitor.  Then you will be able to enjoy some of the goodness that this board can do.

  • Re: I am having a problem with the Kria KV260 board: no video output

    Here's my problem:

    The Kria KV260 board that I have does not seem to work properly. There is no video output of any sort regardless of HDMI or DisplayPort use. No video output.

    I have tried a number of monitors and cables and other settings, all to no avail. I have also tried to setup and use several versions flavors of VNC and Remote Desktop, but I get no output either.

    I have tried Ubuntu and PetaLinux. No video output.

    Let me also add:

    Let me add some more information regarding what I have done and the problem I am having with the Kria KV260 kit:

    I would like to clarify that there’s no video output from the board via the HDMI or DisplayPort video output. There’s also no graphical interface through any of the VNC flavors that have tried.

    I can still access the board via the serial port and via secure shell (ssh). Therefore the board itself is not dead and I can interface with it, but there is no video output. There’s no graphical interface available.

    Also, I have updated the firmware as recommended, and I have put Ubuntu and PetaLinux on the flash card. Same behavior for both Linux flavors.

    If anyone can offer some help, I'd appreciate it. Thank you.

  • I found the same issue. Xilinx did note the need to update the firmware in their getting started guide. This note did not link to directions, so a level of research was needed just to boot. 

    In Xilinx's defence, it is critical to have the first stage boot loader and the operating system in sync. There are many settings that define how the device works that can only be modified during the first stage. This is a hard problem considering these are stored in different memories, one non-volatile and one removable.

    It would be nice to have a clear link in the note to the instructions to fix this with a "clear use this version with this version of Ubuntu". Even better would be to add the steps to update to the start guide. It would also be nice to have a special image that only installed the updated firmware on boot. So the instructions would be burn this, boot, burn Ubuntu, boot.

    Ultimately the information to fix this was published and available; this allowed both of us to overcome this issue and boot Ubuntu.

  • Some might say I talk to myself too much, but that is okay, because it is true.

    Success!  I have the Ubuntu GUI up and running. I had problems with the ubuntu user password, so I took out the SD Card and put in my computer and edited the /etc/shadow to have no password for root and ubuntu.  Booted back and get maintenance mode where I set the root and ubuntu passwords to my liking.  

    Now to have fun!

  • Answering some of my own questions..

    1. Need to update the firmware. I did this via the firmware button and web interface
    2. Have to change the label on the SD Card (ext4 partition) to "writable"

    Now I have it booted to a root@ubuntu: command prompt

  • Just looking to see if anyone got their board to boot yet with Ubuntu.  From what I can tell you download the special Ubuntu for the Xilinx, but the instructions say download the image. We, there is not an image.  There are two rootfs to be placed on an ext4 filesystem, depending on your preference of compression (and to add to the confusion) and a System-boot based on a FAT filesystem.  So I took an SD card and made a system-boot FAT and put that there and created an EXT4 and put the rootfs there.

    Booting starts here...

    switch to partitions #0, OK
    mmc1 is current device
    Scanning mmc 1:1...
    Found U-Boot script /boot.scr.uimg
    5980 bytes read in 16 ms (364.3 KiB/s)
    ## Executing script at 20000000
    Configuring the cma value based on the board type
    ZynqMP SMK-K26 Rev1/B/A: No match
    ZynqMP SMK-K26 Rev1/B/A: No match
    cma=1000M
    Loading image.fit
    74448580 bytes read in 8963 ms (7.9 MiB/s)
    ## Loading kernel from FIT Image at 10000000 ...
    Using 'conf-zynqmp-smk-k26-revA' configuration
    Trying 'kernel-1' kernel subimage
    Description: Ubuntu kernel

    Booting fails here...

    [ 6.351160] 0x000002240000-0x000002250000 : "SHA256"
    [ 6.364173] 0x000002250000-0x000004000000 : "User"
    [ 6.496472] random: fast init done
    [ 6.501701] da9121 0-0033: Device detected (device-ID: 0x05, var-ID: 0x21, DA9131)
    [ 6.551966] da9121 0-0032: Device detected (device-ID: 0x05, var-ID: 0x20, DA9130)
    [ 6.919637] random: crng init done
    [ 8.751137] async_tx: api initialized (async)
    [ 35.820889] da9131_buck1: disabling

    This is my first attempt and I will be testing more today, but if someone has something working already, please share.

  • KV260 is a pretty good board for computer vision developer.

  • The lab at my work is full of test equipment with noisy fans so I am sure the Kria would blend in nicely.  But at home where I want some peace and tranquility PWM would come in handy for sure.

  • The fan on the Kria is too noisy if you work in a quiet work environment. One of the first things you learn with the Kria out of necessity is to control the fan via PWM using the SoC temperature as a signal.

  • Impressive looking board.  We're all familiar with Moore's Law, but are we entering a new era where fan sizes will double every 18 months.  Wink

    If so it begins with that very substantial orange fan.

  • Good fpga board. Adam Taylor has good videos with this board.

  • I agree with the KR260. I also took my first steps with the KV260, it was hard for me to start working with it because everything was new to me and I had a serious problem working with Petalinux due to the poor internet connection at home. But in the end I managed to finish a project: Kria Kitchen ML Lifeguard - Hackster.io
    I am now more confident with the entire Xilinx development environment.
    A design challenge or experimentation with the KR260 would be great.

  • +1 for KR260.

    Personally my interest is more towards video applications that use MGTs to transfer high bandwidth video from one device to another with low latency. Unfortunately the KV260 does not have the connector relevant to MGTs populated, while the KR260 does. KR260 also has a SFP cage that can be used to get started with MGTs out of the box. If the KR260 becomes available for review, I will definitely sign up as well!

  • Definitely an interesting and convenient kit with example demo apps out of the box. I have my own kit which I got a few months back in a competition on Hackster. Personally the key feature is that Ubuntu is supported officially. The Ubuntu system really made it very comfortable for me to use.

  • This is an interesting board, there are a few example projects on the web.  I played around with one for a few months.  I'll sign up if you get some KR260 Robotics kits to road test.

  • I'm interested in the Kria for different applications - I believe it supports that you can push hardware-implemented algorithms at run-time to this family. The Spartan-7 supports the "deploy hardware acceleration at runtime" too, but not the mechanism the Xilinx deploys for managing deploying it and rolling it out.

  • This is a really powerful piece of kit. I was lucky enough to test out a preview version of this a while ago.

    community.element14.com/.../kria-kv260-vision-ai-review

  • Awesome module. If you have any interest in vision computing, this is a phenomenal head start on a solution.