NXP WaRP7 - Review

View table of contents ...  

RoadTest: NXP WaRP7

Author: tedgrosch

Creation date:

Evaluation Type: Evaluation Boards

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: UDOO NEO FULL

What were the biggest problems encountered?: Inter processor communications.

Detailed Review:

I received a complimentary Warp7 and this is the start of the review I promised. I've spent some time with the Warp7 and here are my observations.

 

I have had this board for about 6 months and haven't had enough time to try everything I want. I hope to have some of my embedded systems students begin building meaningful applications for it, but so far none have wanted to take on the challenge. I have a student signed up for a body area network directed study beginning fall semester.

 

You will need two USB cables and ports. One micro USB is used for power and one is the CLI port, which is the only way to communicate with a new board. Set the serial port to 115200 baud, data bits 8, 1 stop bit, no parity, no flow control.

 

First, the first advantage I noticed was that Linux is already flashed on the board when it arrives. You can power it up and go right out of the box. No downloading images and initializing SD cards. And the boot process is faster than my other platforms that boot from a card. I have not tired to update yet. I included the serial output during the boot up process in Exhibit A.

 

I haven't tried to MikroBus cards because I broke one of the board-to-board connectors trying to separate the CPU from the interface board with attempting to connect the battery.

 

I do not recommend you use the battery. I found the battery impossible to connect tot eh board (even under a stereo-zoom microscope). After a few attempts, I ripped the connector off the board. I soldered the battery wires on the board and it works fine, but now I can't turn the board off. I have to wait for the battery to go dead.

 

The following is a list of the /dev directory which shows the 9 axis IMU enstantiated as devices.

 

root@imx7s-warp:/dev# ls

 

FreescaleAccelerometer ram12                   tty34

FreescaleGyroscope ram13                   tty35

FreescaleMagnetometer ram14                   tty36

autofs ram15                   tty37

block ram2                    tty38

char ram3                    tty39

console ram4                    tty4

cpu_dma_latency ram5                    tty40

disk                    ram6                    tty41

dri ram7                    tty42

fd ram8                    tty43

full ram9                    tty44

fuse random                  tty45

hwrng rtc                     tty46

i2c-0 rtc0                    tty47

i2c-1 shm                     tty48

i2c-3 snd                     tty49

iio:device0 stderr                  tty5

initctl stdin                   tty50

input stdout                  tty51

kmsg tty                     tty52

log tty0                    tty53

loop-control tty1                    tty54

loop0 tty10                   tty55

loop1 tty11                   tty56

loop2 tty12                   tty57

loop3                   tty13                   tty58

loop4 tty14                   tty59

loop5 tty15                   tty6

loop6 tty16                   tty60

loop7 tty17                   tty61

mem                     tty18                   tty62

memory_bandwidth tty19                   tty63

mmcblk2 tty2                    tty7

mmcblk2boot0 tty20                   tty8

mmcblk2boot1 tty21                   tty9

mmcblk2p1 tty22                   ttymxc0

mmcblk2p2 tty23                   ttymxc2

mmcblk2rpmb tty24                   ubi_ctrl

mtab tty25                   urandom

network_latency tty26                   vcs

network_throughput tty27                   vcs1

null tty28                   vcsa

ptmx tty29                   vcsa1

pts tty3                    watchdog

ram0 tty30                   watchdog0

ram1 tty31                   zero

ram10 tty32

ram11 tty33

root@imx7s-warp:/dev#

root@imx7s-warp:/dev# cd ../

root@imx7s-warp:/#

root@imx7s-warp:/# ls

bin         etc         lost+found  opt sbin        usr

boot        home        media       proc        sys         var

dev         lib         mnt         run         tmp

root@imx7s-warp:/#

root@imx7s-warp:/# cd home

root@imx7s-warp:/home#

root@imx7s-warp:/home# ls

root

 

This all for now. Stay tuned. I'm going have a student use it to build a wearable device in a body area network for as a senor elective in fall semester.

 

 

Exhibit A:

Here is the terminal output during boot-up:

 

U-Boot 2016.07-00091-ge6b4241 (Aug 22 2016 - 10:56:52 +0800)

 

CPU:   Freescale i.MX7S rev1.2 at 792MHz

CPU:   Extended Commercial temperature grade (-20C to 105C) at 43C

Reset cause: POR

Board: WARP7

DRAM:  512 MiB

MMC:   FSL_SDHC: 0

*** Warning - bad CRC, using default environment

 

In:    serial

Out:   serial

Err:   serial

Net:   CPU Net Initialization Failed

No ethernet found.

Hit any key to stop autoboot:  2  1  0

switch to partitions #0, OK

mmc0(part 0) is current device

switch to partitions #0, OK

mmc0(part 0) is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

6527184 bytes read in 91 ms (68.4 MiB/s)

Booting from mmc ...

reading imx7s-warp.dtb

33989 bytes read in 12 ms (2.7 MiB/s)

Kernel image @ 0x80800000 [ 0x000000 - 0x6398d0 ]

## Flattened Device Tree blob at 83000000

   Booting using the fdt blob at 0x83000000

   Using Device Tree in place at 83000000, end 8300b4c4

 

Starting kernel ...

 

Booting Linux on physical CPU 0x0

Linux version 4.1.29-fslc+g59b38c3 (jenkins@ci-builder-1) (gcc version 5.3.0 (GCC) ) #1 SMP PREEMPT Wed Aug 17 02:46:24 CEST 2016

CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d

CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache

Machine model: Warp i.MX7S Board

Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB

Reserved memory: initialized node linux,cma, compatible id shared-dma-pool

Memory policy: Data cache writealloc

PERCPU: Embedded 12 pages/cpu @8bb25000 s16908 r8192 d24052 u49152

Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048

Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk2p2 rootwait rw

PID hash table entries: 2048 (order: 1, 8192 bytes)

Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)

Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)

Memory: 178764K/524288K available (8191K kernel code, 430K rwdata, 2928K rodata, 424K init, 450K bss, 17844K reserved, 327680K cma-reserved, 0K highmem)

Virtual kernel memory layout:

    vector  : 0xffff0000 - 0xffff1000   (   4 kB)

    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)

    vmalloc : 0xa0800000 - 0xff000000   (1512 MB)

    lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)

    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)

    modules : 0x7f000000 - 0x7fe00000   (  14 MB)

      .text : 0x80008000 - 0x80ae3f78   (11120 kB)

      .init : 0x80ae4000 - 0x80b4e000   ( 424 kB)

      .data : 0x80b4e000 - 0x80bb9ae0   ( 431 kB)

       .bss : 0x80bbc000 - 0x80c2c840   ( 451 kB)

SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1

Preemptible hierarchical RCU implementation.

            Additional per-CPU info printed with stalls.

            RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.

RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2

NR_IRQS:16 nr_irqs:16 16

Architected cp15 timer(s) running at 8.00MHz (phys).

clocksource arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns

sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns

Switching to timer-based delay loop, resolution 125ns

mxc_clocksource_init 3000000

Ignoring duplicate/late registration of read_current_timer delay

clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns

Console: colour dummy device 80x30

Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=80000)

pid_max: default: 32768 minimum: 301

Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)

Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)

CPU: Testing write buffer coherency: ok

/cpus/cpu@0 missing clock-frequency property

/cpus/cpu@1 missing clock-frequency property

CPU0: thread -1, cpu 0, socket 0, mpidr 80000000

Setting up static identity map for 0x80008280 - 0x800082d8

CPU1: failed to come online

Brought up 1 CPUs

SMP: Total of 1 processors activated (16.00 BogoMIPS).

CPU: All CPU(s) started in SVC mode.

devtmpfs: initialized

VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5

clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns

pinctrl core: initialized pinctrl subsystem

NET: Registered protocol family 16

DMA: preallocated 256 KiB pool for atomic coherent allocations

cpuidle: using governor ladder

cpuidle: using governor menu

DDR type is LPDDR3!

hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.

hw-breakpoint: maximum watchpoint size is 8 bytes.

imx7d-pinctrl 302c0000.iomuxc-lpsr: no functions defined

imx7d-pinctrl 302c0000.iomuxc-lpsr: fail to probe dt properties

imx7d-pinctrl: probe of 302c0000.iomuxc-lpsr failed with error -22

imx7d-pinctrl 30330000.iomuxc: initialized IMX pinctrl driver

MU is ready for cross core communication!

mxs-dma 33000000.dma-apbh: initialized

SCSI subsystem initialized

usbcore: registered new interface driver usbfs

usbcore: registered new interface driver hub

usbcore: registered new device driver usb

  1. 30800000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
  2. 30800000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator

i2c i2c-0: IMX I2C adapter registered

i2c i2c-0: can't use DMA

i2c i2c-1: IMX I2C adapter registered

i2c i2c-1: can't use DMA

i2c i2c-3: IMX I2C adapter registered

i2c i2c-3: can't use DMA

Linux video capture interface: v2.00

pps_core: LinuxPPS API ver. 1 registered

pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>

PTP clock support registered

MIPI CSI2 driver module loaded

Advanced Linux Sound Architecture Driver Initialized.

Bluetooth: Core ver 2.20

NET: Registered protocol family 31

Bluetooth: HCI device and connection manager initialized

Bluetooth: HCI socket layer initialized

Bluetooth: L2CAP socket layer initialized

Bluetooth: SCO socket layer initialized

Switched to clocksource arch_sys_counter

NET: Registered protocol family 2

TCP established hash table entries: 4096 (order: 2, 16384 bytes)

TCP bind hash table entries: 4096 (order: 3, 32768 bytes)

TCP: Hash tables configured (established 4096 bind 4096)

UDP hash table entries: 256 (order: 1, 8192 bytes)

UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)

NET: Registered protocol family 1

RPC: Registered named UNIX socket transport module.

RPC: Registered udp transport module.

RPC: Registered tcp transport module.

RPC: Registered tcp NFSv4.1 backchannel transport module.

imx rpmsg driver is registered.

Bus freq driver module loaded

futex hash table entries: 512 (order: 3, 32768 bytes)

VFS: Disk quotas dquot_6.6.0

VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)

NFS: Registering the id_resolver key type

Key type id_resolver registered

Key type id_legacy registered

jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.

fuse init (API version 7.23)

io scheduler noop registered

io scheduler deadline registered

io scheduler cfq registered (default)

MIPI DSI driver module loaded

MIPI DSI driver module loaded

imx-sdma 30bd0000.sdma: no event needs to be remapped

imx-sdma 30bd0000.sdma: loaded firmware 4.2

imx-sdma 30bd0000.sdma: initialized

pfuze100-regulator 0-0008: Full layer: 1, Metal layer: 1

pfuze100-regulator 0-0008: FAB: 0, FIN: 0

pfuze100-regulator 0-0008: pfuze3000 found.

  1. 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 270, base_baud = 1500000) is a IMX

console [ttymxc0] enabled

  1. 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 271, base_baud = 5000000) is a IMX

imx sema4 driver is registered.

[drm] Initialized drm 1.1.0 20060810

[drm] Initialized vivante 1.0.0 20120216 on minor 0

brd: module loaded

loop: module loaded

input: fxos8700 as /devices/platform/soc/30800000.aips-bus/30a50000.i2c/i2c-3/3-001e/input/input0

fxos8700 device driver probe successfully

input: fxas2100x as /devices/platform/soc/30800000.aips-bus/30a50000.i2c/i2c-3/3-0020/input/input1

fxas2100x 3-0020: fxas2100x device driver probe successfully

CAN device driver interface

ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver

ehci-mxc: Freescale On-Chip EHCI Host driver

usbcore: registered new interface driver usb-storage

usbcore: registered new interface driver usb_ehset_test

30b10200.usbmisc supply vbus-wakeup not found, using dummy regulator

30b20200.usbmisc supply vbus-wakeup not found, using dummy regulator

30b30200.usbmisc supply vbus-wakeup not found, using dummy regulator

mousedev: PS/2 mouse device common for all mice

input: 30370000.snvs:snvs-powerkey as /devices/platform/soc/30000000.aips-bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input2

snvs_rtc 30370000.snvs:snvs-rtc-lp: rtc core: registered 30370000.snvs:snvs- as rtc0

i2c /dev entries driver

IR NEC protocol handler initialized

IR RC5(x/sz) protocol handler initialized

IR RC6 protocol handler initialized

IR JVC protocol handler initialized

IR Sony protocol handler initialized

IR SANYO protocol handler initialized

IR Sharp protocol handler initialized

IR MCE Keyboard/mouse protocol handler initialized

IR XMP protocol handler initialized

imx2-wdt 30280000.wdog: timeout 60 sec (nowayout=0)

Bluetooth: HCI UART driver ver 2.3

Bluetooth: HCI UART protocol H4 registered

Bluetooth: HCI UART protocol BCSP registered

Bluetooth: HCI UART protocol ATH3K registered

usbcore: registered new interface driver bcm203x

usbcore: registered new interface driver btusb

usbcore: registered new interface driver ath3k

sdhci: Secure Digital Host Controller Interface driver

sdhci: Copyright(c) Pierre Ossman

sdhci-pltfm: SDHCI platform and OF driver helper

/soc/aips-bus@30800000/usdhc@30b40000: voltage-ranges unspecified

sdhci-esdhc-imx 30b40000.usdhc: No vqmmc regulator found

mmc0: SDHCI controller on 30b40000.usdhc [30b40000.usdhc] using ADMA

/soc/aips-bus@30800000/usdhc@30b60000: voltage-ranges unspecified

sdhci-esdhc-imx 30b60000.usdhc: No vmmc regulator found

sdhci-esdhc-imx 30b60000.usdhc: No vqmmc regulator found

mmc0: queuing unknown CIS tuple 0x80 (2 bytes)

mmc0: queuing unknown CIS tuple 0x80 (3 bytes)

mmc0: queuing unknown CIS tuple 0x80 (3 bytes)

mmc0: queuing unknown CIS tuple 0x80 (7 bytes)

mmc0: queuing unknown CIS tuple 0x80 (3 bytes)

mmc2: SDHCI controller on 30b60000.usdhc [30b60000.usdhc] using ADMA

mmc0: queuing unknown CIS tuple 0x80 (6 bytes)

caam 30900000.caam: Entropy delay = 3200

caam 30900000.caam: Instantiated RNG4 SH0

caam 30900000.caam: Instantiated RNG4 SH1

caam 30900000.caam: device ID = 0x0a16030000000000 (Era -524)

caam 30900000.caam: job rings = 3, qi = 0

mmc0: new high speed SDIO card at address 0001

mmc2: MAN_BKOPS_EN bit is not set

mmc2: mmc_select_hs200 failed, error -74

: switch to mmc2 failed

mmc2: new MMC card at address 0001

mmcblk2: mmc2:0001 V10008 7.05 GiB

mmcblk2boot0: mmc2:0001 V10008 partition 1 4.00 MiB

mmcblk2boot1: mmc2:0001 V10008 partition 2 4.00 MiB

mmcblk2rpmb: mmc2:0001 V10008 partition 3 4.00 MiB

mmcblk2: p1 p2

caam algorithms registered in /proc/crypto

caam_jr 30901000.jr0: registering rng-caam

platform caam_sm: blkkey_ex: 8 keystore units available

platform caam_sm: 64-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: 64-bit black key:

platform caam_sm: [0000] bb c3 99 6f c3 66 a4 0e

platform caam_sm: [0008] 99 1d 45 76 02 e8 1f f7

platform caam_sm: 128-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: 128-bit black key:

platform caam_sm: [0000] a7 8d e0 c9 e9 62 79 dc

platform caam_sm: [0008] 00 5a 05 59 49 2f 83 a5

platform caam_sm: 192-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: 192-bit black key:

platform caam_sm: [0000] ac cd e4 7c 88 c4 c9 11

platform caam_sm: [0008] 4e c9 6b a8 e2 7d 93 15

platform caam_sm: [0016] 45 e4 a0 2b 63 1e 9a 78

platform caam_sm: [0024] 28 25 f6 d9 73 31 27 c5

platform caam_sm: 256-bit clear key:

platform caam_sm: [0000] 00 01 02 03 04 0f 06 07

platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f

platform caam_sm: [0016] 10 11 12 13 14 15 16 17

platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f

platform caam_sm: 256-bit black key:

platform caam_sm: [0000] 20 64 83 a6 d7 1b 4f 6e

platform caam_sm: [0008] fc f9 dd 68 34 43 90 0d

platform caam_sm: [0016] 63 32 1f b3 48 0b 75 73

platform caam_sm: [0024] 19 66 86 25 b6 01 22 fc

platform caam_sm: 64-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 196-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit unwritten blob:

platform caam_sm: [0000] 00 00 00 00 00 00 00 00

platform caam_sm: [0008] 00 00 00 00 00 00 00 00

platform caam_sm: [0016] 00 00 00 00 00 00 00 00

platform caam_sm: [0024] 00 00 00 00 00 00 00 00

platform caam_sm: [0032] 00 00 00 00 00 00 00 00

platform caam_sm: [0040] 00 00 00 00 00 00 00 00

platform caam_sm: [0048] 00 00 00 00 00 00 00 00

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 64-bit black key in blob:

platform caam_sm: [0000] a4 01 3c 5c 52 25 b0 a9

platform caam_sm: [0008] 55 24 ea 1b 5c db 86 c2

platform caam_sm: [0016] 56 9b 30 17 87 8c 09 b3

platform caam_sm: [0024] 58 93 ce 8e e7 d2 12 30

platform caam_sm: [0032] 01 54 e0 9f e3 af 7f c1

platform caam_sm: [0040] 58 91 16 5a a6 1c 06 84

platform caam_sm: [0048] f9 97 0f 13 5d 3c 65 9d

platform caam_sm: [0056] 00 00 00 00 00 00 00 00

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 128-bit black key in blob:

platform caam_sm: [0000] 70 4a dd b7 3e 3b b2 04

platform caam_sm: [0008] c9 8e 71 fa 92 74 73 bb

platform caam_sm: [0016] 5c b4 07 e9 64 9c 16 aa

platform caam_sm: [0024] 5d 18 0c 8d 92 30 1d eb

platform caam_sm: [0032] de c3 d6 30 14 a4 51 52

platform caam_sm: [0040] 43 b9 a9 56 4f 27 84 0f

platform caam_sm: [0048] 24 c1 50 14 1e 8c 12 10

platform caam_sm: [0056] a9 e4 95 d0 38 fe 68 43

platform caam_sm: [0064] 00 00 00 00 00 00 00 00

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 192-bit black key in blob:

platform caam_sm: [0000] 2d 74 58 5c 44 b6 cb 43

platform caam_sm: [0008] c5 8a d1 d3 22 d4 73 ba

platform caam_sm: [0016] 34 1e 87 e9 0a b1 26 1d

platform caam_sm: [0024] 80 78 ec 8c 45 7f 89 1d

platform caam_sm: [0032] bc bc 5b 5a 66 0e 86 d9

platform caam_sm: [0040] be 5b 46 03 78 46 2e 4b

platform caam_sm: [0048] 27 5e 16 81 b6 c2 d9 70

platform caam_sm: [0056] e0 5c c0 4c 22 7c ff 88

platform caam_sm: [0064] 45 49 36 35 84 df 1d d6

platform caam_sm: [0072] 00 00 00 00 00 00 00 00

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: 256-bit black key in blob:

platform caam_sm: [0000] ff 75 9a 9b 2d 02 65 42

platform caam_sm: [0008] dc 3d 69 04 0f 98 43 14

platform caam_sm: [0016] ec 31 d5 ac 2d 39 d6 d8

platform caam_sm: [0024] c9 e6 fd 98 49 06 09 81

platform caam_sm: [0032] 0b 7f 44 ba 28 68 5d ff

platform caam_sm: [0040] ac 38 14 06 99 6d 23 7d

platform caam_sm: [0048] 33 20 6a f8 53 44 74 80

platform caam_sm: [0056] 1d 3c f5 dc 77 f9 dd 0a

platform caam_sm: [0064] f7 93 f8 87 41 52 b5 60

platform caam_sm: [0072] b1 b5 81 09 3c fd 1d ff

platform caam_sm: [0080] 00 00 00 00 00 00 00 00

platform caam_sm: [0088] 00 00 00 00 00 00 00 00

platform caam_sm: restored 64-bit black key:

platform caam_sm: [0000] 2c 28 8a d2 50 a4 e9 ad

platform caam_sm: [0008] d0 f2 da 40 be 5e fb 45

platform caam_sm: restored 128-bit black key:

platform caam_sm: [0000] a7 8d e0 c9 e9 62 79 dc

platform caam_sm: [0008] 00 5a 05 59 49 2f 83 a5

platform caam_sm: restored 192-bit black key:

platform caam_sm: [0000] ac cd e4 7c 88 c4 c9 11

platform caam_sm: [0008] 4e c9 6b a8 e2 7d 93 15

platform caam_sm: [0016] d3 0c ae dc b9 77 be f4

platform caam_sm: [0024] 12 ad 8e 00 20 ee 0b cd

platform caam_sm: restored 256-bit black key:

platform caam_sm: [0000] 20 64 83 a6 d7 1b 4f 6e

platform caam_sm: [0008] fc f9 dd 68 34 43 90 0d

platform caam_sm: [0016] 63 32 1f b3 48 0b 75 73

platform caam_sm: [0024] 19 66 86 25 b6 01 22 fc

snvs-secvio 30370000.caam-snvs: can't get snvs clock

snvs-secvio 30370000.caam-snvs: violation handlers armed - non-secure state

usbcore: registered new interface driver usbhid

usbhid: USB HID core driver

NET: Registered protocol family 26

NET: Registered protocol family 10

sit: IPv6 over IPv4 tunneling driver

NET: Registered protocol family 17

can: controller area network core (rev 20120528 abi 9)

NET: Registered protocol family 29

can: raw protocol (rev 20120528)

can: broadcast manager protocol (rev 20120528 t)

can: netlink gateway (rev 20130117) max_hops=1

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

cpu cpu0: dev_pm_opp_get_opp_count: device OPP not found (-19)

sgtl5000 3-000a: sgtl5000 revision 0x11

sgtl5000 3-000a: Using internal LDO instead of VDDD

asoc-simple-card sound: sgtl5000 <-> 308a0000.sai mapping ok

dhd_module_init in

input: gpio-keys as /devices/platform/gpio-keys/input/input3

snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:01 UTC (1)

ALSA device list:

  #0: imx7s-sgtl5000

EXT3-fs (mmcblk2p2): error: couldn't mount because of unsupported optional features (240)

EXT2-fs (mmcblk2p2): error: couldn't mount because of unsupported optional features (244)

EXT4-fs (mmcblk2p2): recovery complete

EXT4-fs (mmcblk2p2): mounted filesystem with ordered data mode. Opts: (null)

VFS: Mounted root (ext4 filesystem) on device 179:2.

devtmpfs: mounted

Freeing unused kernel memory: 424K (80ae4000 - 80b4e000)

 

INIT: version 2.88 booting

 

Starting udev

udevd[174]: starting version 3.1.5

random: udevd urandom read with 22 bits of entropy available

EXT4-fs (mmcblk2p2): re-mounted. Opts: data=ordered

bootlogd: cannot allocate pseudo tty: No such file or directory

ALSA: Restoring mixer settings...

No state is present for card imx7ssgtl5000

Found hardware: "imx7s-sgtl5000" "" "" "" ""

Hardware is initialized using a generic method

No state is present for card imx7ssgtl5000

Fri Aug 19 19:48:55 UTC 2016

 

INIT: Entering runlevel: 5

 

Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device

Starting system message bus: dbus.

Starting Connection Manager

Starting rpcbind daemon...done.

Starting bluetooth

bluetoothd

Starting syslogd/klogd: done

* Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

   ...done.

Starting Telephony daemon

Starting Linux NFC daemon

Running local boot scripts (/etc/rc.local).

 

 

Poky (Yocto Project Reference Distro) 2.1.1 imx7s-warp /dev/ttymxc0

 

 

imx7s-warp login: root

7[r[999;999H[6n8root@imx7s-warp:~# pwd

/home/root

root@imx7s-warp:~#

root@imx7s-warp:~#

Anonymous