Microchip dsPIC33C Digital Power Starter Kit

View table of contents ...  

RoadTest: Microchip dsPIC33C Digital Power Starter Kit

Author: MARK2011

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: As a comparable solution apart from the older brother from Microchip - MPLAB STARTER KIT FOR DIGITAL POWER (DM330017-2) or dsPIC30F based DM300023 dsPICDEM kit - nothing particular comes to my mind. I don't know other digitally controlled SMPS kits. Well there is STEVAL-ISA172V2 2 kW fully digital AC-DC power supply (D-SMPS) evaluation board but it is only one function device. Without programming and development possibilities.

What were the biggest problems encountered?: The transport/ packing issue at the beginning but it can be neglected. The only doubt is that I realized the system isn't flexible enough. I hoped to modify firmware of chips and use some power management examples from Microchip. I couldn't cope. According to the first review of papers I was sure I will use that kit exploring PowerSmart Digital Control Library Designer as well as Microchip Power Board Visualizer. That also failed.

Detailed Review:

Microchip dsPIC33C Digital Power Starter Kit roadtest

 

Introduction

Microchip - one of leading  electronic manufacturers known for years, from microcontrollers is expanding the scope of its activities year by year.

Recently, it has been “spoiling” the environment of electronics and developers with more and more interesting development and educational kits.

And so, the kit for testing the use of dsPIC SMPS systems in energy converter systems has entered the roadtest program.

Thank you Microchip, thank you element14 for the proposal to test these solutions.

The dsPIC

Following Microchip definition, dsPIC33C Digital Power Starter Kit demonstrate and helps to understand principle of Digital Signal Controller (DSC) - the  integration a Microcontroller (16-bit MCU) with a Digital Signal Processor (DSP)

In our case benefits of DSCs  are employed in Switch Mode Power Supply (SMPS) device. Switching regulator is employed here to efficiently  convert the power but unlike popular SMPS solutions which are generally analog, our kit demonstrate idea of digitally controlled SMPS  (D-SMPS)

The board is intended to show that digitally (DSC) controlled  SMPS is even easier to introduce and control as analog.

If you need some theory: basics of “switchers”

https://www.avnet.com/wps/portal/abacus/solutions/technologies/power/the-design-engineers-guide/switched-mode-power-supplies/

My board uses dsPIC33CK256MP505 as the “heart” but is also  supported by many other sophisticated components. details below.

image

Overall technical overview

Best description of the kit with all supported instructions and documents is available at:

https://microchip-pic-avr-examples.github.io/dpsk3-power-boost-voltage-mode-control/index.html

or directly on github site

https://github.com/microchip-pic-avr-examples/dpsk3-power-buck-voltage-mode-control

I need to emphasize that during my (to be honest - significantly prolonged) R-T I noticed the supporting content changes. Microchip still adds some new information or chapters.

Copying above information in that report is unnecessary thus I follow to next interesting part:

Unboxing - quality of delivery, packing

In the following film I gathered the most impressive pictures I remember from the beginning of my adventure with  dsPIC33C Digital Power Starter Kit.

We encountered an unpleasant issue as one of the big capacitors appeared damaged after unpacking the board.

As shown in pictures the orange box is the perfect place for safe transportation of the board unless you put the supply unit with multistandard adapters.

In my opinion that crowd in the box caused the disaster.

Summary of parameters and features of the board/ microcontroller(s) and peripherals

The dsPIC33C Digital Power Starter Kit SMPS consists of one DC/DC synchronous Buck Converter, one independent DC/DC Boost Converter, independent resistive loads, protection circuitry, USB/UART converter/bridge and on-board programmer/debugger circuitry.

Both power stages are controlled by the dsPIC33CK256MP505.

Loads and protection circuitry are controlled by an auxiliary PIC24FJ64GA004 microcontroller.

benefits of above solution is superbly described in

image

Digital Power Converter Basics using dsPIC33 Digital Signal Controllers

https://skills.microchip.com/digital-power-converter-basics-using-dspic33-digital-signal-controllers 

That tutorial helps understand most nuances of DSCs implemented in digital power converters

The following film shows the parade of most important components of the board:

Introducing the main actors of the film :

dsPIC33CK256MP505 100 MIPS 16-bit dsPIC® DSC core with integrated DSP

belongs to modern dsPIC33CK family 

https://www.microchip.com/en-us/product/dsPIC33CK256MP505 

https://ww1.microchip.com/downloads/en/DeviceDoc/dsPIC33CK256MP508-Family-Data-Sheet-DS70005349J.pdf 

PIC24FJ64GA004 PIC24 16-bit microcontroller, 64 KB Flash memory, 8 KB RAM

https://www.microchip.com/en-us/product/PIC24FJ64GA004 

ATSAME70N21  32-bit ARM Cortex-M7 processor with Floating Point Unit

https://www.microchip.com/en-us/product/ATSAME70N21 

USB2422  2-Port USB 2.0 Hi-Speed Hub Controller

https://ww1.microchip.com/downloads/en/devicedoc/00001726b.pdf 



Simplified description of the equipment

image

image

image

Documentation 

Microchip provides us with all necessary papers and documentation. Most are available on the site above.

The starting point for explore, experiments or development is here:

https://www.microchip.com/en-us/development-tool/dm330017-3

dsPIC33C Digital Power Starter Kit User’s Guide

image

https://ww1.microchip.com/downloads/en/DeviceDoc/dsPIC33C-Digital-Power-Starter-Kit-Users-Guide-DS50002867B.pdf 

Software (MPLAB X + MCC + dedicated libraries),

As the development environment to program debug and test PIC controllers, Microchip offers the brilliant solution : MPLAB… which word depicts it well? program suite? realm?

nevermind I love that tool.

Just like when discussing documentation also here I shouldn't copy MPLAB descriptions  or tutorials

All is clearly given at Microchip’s sites and other related websites.

https://www.microchip.com/en-us/tools-resources

https://en.wikipedia.org/wiki/MPLAB

image

image

Brief view of MPLABX screen

imageimageimage

besides the main environment, many compilers, my favorite tool to support most PICs is MCC 

https://www.microchip.com/en-us/development-tools-tools-and-software/embedded-software-center/mplab-code-configurator 

Additional tool, precisely“Embedded Software Development Framework” is HARMONY

Initially I was not sure if Microchips HARMONY supports dsPIC33.I just forgot it is designed for 32bit PICs architecture So - unfortunately not but using MCC with libraries programing of all dsPIC33 family is more and more comfortable.

 

Other software intended to use with Microchip’s DSC solutions I planed to introduce:

 

Microchip Power Board Visualizer

Microchip Power Board Visualizer Supporting dsPIC33 DSCs  Link

Software Library:

Microchip Power Board Visualizer Supporting dsPIC33 DSCs

https://www.microchip.com/en-us/software-library/power_board_visualizer 

image

http://www.microchip.com/SWLibraryWeb/product.aspx?product=POWER_BOARD_VISUALIZER 

wrong link?

image

Power Board Visualizer 1.0 Installation Guide

https://ww1.microchip.com/downloads/aemDocuments/softwarelibrary/power_board_visualizer/Power_Board_Visualizer_Installation_Guide.pdf

Power Board Visualizer User’s Guide

https://ww1.microchip.com/downloads/aemDocuments/documents/MCU16/ProductDocuments/UserGuides/Power-Board-Visualizer-User-Guide-50003115.pdf

https://ww1.microchip.com/downloads/en/DeviceDoc/Power-Board-Visualizer-User-Guide-50003115.pdf

 

PowerSmart Digital Control Library Designer

UG20181026O

 https://microchip-pic-avr-tools.github.io/powersmart-dcld/#dcld_1 

https://microchip-pic-avr-tools.github.io/powersmart-dcld/files/181026o_dcld_beta_user_guide.pdf 

image

image

MPLAB® PowerSmartTm SDK Digital Control Library Designer Configuration Tool & Code Generator

https://microchip-pic-avr-tools.github.io/powersmart-dcld/ 

image

MPLAB® PowerSmartTm Digital Control Library Designer User’s Guide

https://microchip-pic-avr-tools.github.io/powersmart-dcld/files/181026o_dcld_beta_user_guide.pdf

https://microchip-pic-avr-tools.github.io/powersmart-dcld/#dcld_1 

https://microchip-pic-avr-tools.github.io/powersmart-dcld/files/181026o_dcld_beta_user_guide.pdf

MPLAB PowerSmartTm SDK for Microchip dsPIC33® Digital Signal Controllers

Digital Control Library Designer (PS-DCLD)

 

 

And last not least : details of PICkit4 and its software 

(it is onboard programmer in our kit)

MPLAB® PICkitTm 4 In-Circuit Debugger

https://www.microchip.com/en-us/development-tool/PG164140

Writing about documentation, tutorials and all useful  supporting materials would consume time and space in that report. I need to cut it down here and describe my more practical activity.

Run the board

The firmware lets the board operate in two main modes.

Loads – Can be configured for either Static mode or Dynamic mode. 

If Dynamic mode is selected, a switching frequency can be configured in application SW.

The Buck Converter stage is rated for a maximum of 7.6W. However, the maximum

on-board configurable resistive load is 3.3W. The output voltage and output current

should remain within their Safe Operating Area (SOA) to avoid protection circuitry

tripping.

The Boost Converter stage is rated for a maximum power of 6W. However, the maximum

on-board configurable resistive load is 3W. The output voltage and output current

should remain within the Boost Converter Safe Operating Area (SOA) to avoid damage

to the board. The output voltage of the Boost Converter (Boost_Out) can be pro-

grammed from a 10V to 17.8V output, with a default programmed voltage of 15V

Basic modes of operation collected in the table below

image

 

I collected some waveforms of above described power modes from buck converter.

Review starts from static load with 10% P=0.45W these waveforms are mostly stable

then with 100% (3W)  on charts with larger step we see periodic (around 1s) distorsions

Dynamic mode is overally stormy al all load levels.

below - film with full review of all modes of buck converter

below - film with full review of all modes of boost converter

Faults when supplying inappropriate voltage or supply capacity is weak

Watch behavior of protection system when overheating

Installation of software/applications - impressions/ remarks

After playing with basic application, the time has come to check programming abilities, upload the main firmware, modify or adapt it. First I conducted steps from the guide.

dsPIC33C Digital Power Starter Kit Demo Code  

image

https://ww1.microchip.com/downloads/en/DeviceDoc/dsPIC33C_Digital%20Power%20Starter%20Kit%20Demo%20Code.zip 

image

 

Programming the chip - first check the programmer debugger compatibility

image

image

image

New task - export firmware  (from dsPIC) using IPE

image

image

image

And the other way - uploading the firmware

There are two chips on the board to be programmed:

both dsPIC32 as well as support device: PIC24

 

dsPIC33C_Digital Power Starter Kit Demo Code.zip

view of folders used with MPLABX:

image

image

image

image

image

code examples

Following review of available simple application/code example from Microchip datasheets, GitHub resources etc

Microchip code examples

image

https://www.microchip.com/doclisting/TechDoc.aspx?type=codeexamples&productfamily=16-BIT

image

and on the  github

https://github.com/microchip-pic-avr-solutions

One remark concerning use of supporting tools in programming

 curiosity solutions very convenient when using some PICS as well dsPICs can’t be implemented in our module

image

OTHER CODE EXAMPLES

There are several SMPS code examples available on the Microchip website. (www.microchip.com/SMPS)

https://www.microchip.com/en-us/solutions/power-management-and-conversion/intelligent-power

 

Solar MPPT Battery Charger for the Rural Electrification System

https://ww1.microchip.com/downloads/en/Appnotes/00002321A.pdf

 

Microchip Developer Help

16-bit PIC® and dsPIC® Microcontrollers

https://microchipdeveloper.com/16bit:start

image

Step-by-Step dsPIC33CH Programming Example dsPIC33CH128MP508S1

 

Step-by-Step dsPIC33CH Programming Example

dla dsPIC33CH128MP508 dual core

https://microchipdeveloper.com/16bit:ch-example

image

 

Simple project application

Project: Review communication channels

 Basic aplications for dsPIC33 I made it simple using MCC

image

image

image

image

My UART project

Simple project to test programming capabilities of MPLAB/MCC and behave of dsPIC33 

image

image

image

image

image

image

image

image

image

image

image

image

image

Adaptation of projects from: microchip-pic-avr-examples

Many dsPIC projects are available in

dsPIC33C High-Resolution PWM Configuration I    dspic33ck-power-pwm-complementary

https://github.com/microchip-pic-avr-examples/dspic33ck-power-pwm-complementary 

image

Run Microchip Power Board Visualizer 

image

image

image

image

image

download the example file

imageimage

with project "DP Development Board demo project 1.0.0.0"

image

image

image

image

image

image

And one big doubt at the end of that stage…

despite promising declaration at the kit documentation/ manual site:

image

Our board isn’t supported by  Microchip Power Board Visualizer

Thus I could play with it only theoretically but connections and management isn’t available.

 

PowerSmart Digital Control Library Designer

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

image

Above tool seems to be great support in development and debugging power applications based on dsPIC. Unfortunately although it is mentioned in our kit documentation, my dsPIC33C Digital Power Starter Kit (based on dsPIC33CK256MP505) can’t be supported. I considered which way to reprogram/ modify the code of both dsPIC and PIC24. But, at least with my skills I had to give up.

That is also general notice. Our board isn’t very flexible in the scope of modify applications and build DSC projects.

My plans to adapt some projects and create  e.g. -

AC to DC | DC to DC | DC to AC | Wireless Charger and Receiver | Solar | Battery Management

https://www.microchip.com/en-us/solutions/power-management-and-conversion/intelligent-power/products/full-digital-power 

image

https://www.microchip.com/en-us/solutions/power-management-and-conversion/intelligent-power/smps-solar-power 

- were too ambitious.

Short summary

Nevertheless, the kit is doing a good job to introduce into the realm of digitally controlled SMPSs.

It should emphasize the degree of protection, ergonomy and overall elegance of the board.

Hoping that my report isn't chaotic very much and readable.

I'm open for discussion, every comment is welcome

Thank you

Marek

Anonymous