RoadTest: Pi-Top - A Raspberry Pi Laptop
Author: vlaine
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: If you compare the Pi-Top to a regular laptop, you would be tempted to list the Chromebook or a cheap Windows laptop as comparable products. However the Pi-Top is something else. The main purpose of this device is to teach software AND hardware development with a portable unit. You could see it as a Lego MindStroms / mini laptop combo. The best equivalent would be the Pi-TopCEED or to build your own using a Raspberry Pi 3 B+ running Pi-TopOS. You can also visit the Plytop Shell project https://www.element14.com/community/community/raspberry-pi/blog/2018/04/11/the-plytop-shell?CMP=SOM-FACEBOOK-PRG-RASPI-BLOG-RJOHNSON-PLYTOP-COMM-GBL
What were the biggest problems encountered?: 1. My tab key is defective, but the customer support team replied within 20 minutes and directly offered to swap the unit. 2. In Pi-TopCODER, some circuit diagram where not clear enough. I could not distinguish which resistor goes where because they all looked the same. I had to analyze the circuit to get my answer (no kid friendly). 3. In Pi-TopCODER, the tutorial had some bugs. As an example, one tutorial gave an incorrect GPIO port number. In an other tutorial, an IF condition had a && operator instead of an And operator. It was giving a syntax error. 4. The spell checker was not installed by default for LibreOffice. I had to install it manually
Detailed Review:
The following are not included with the Pi-Top. You need to purchase them separately
The Pi-Top comes with Pi-TopOS pre-installed on a 8Gb micro SD Card.
However, I suggest that you get a larger card (64Gb) and install the latest version yourself.
If your SD card is larger than 32Gb (SDXC), follow this guide to format the entire card to Fat32.
https://www.raspberrypi.org/documentation/installation/sdxc_formatting.md
** Note that you can also format it using a camera. Quick, easy and always my favorite choice.
The Pi-TopOS is free and available to anyone who wants to install it on it's Raspberry Pi.It is regularly updated and since the last update, it is based on Raspberry Stretch instead of Jessie.If you tried Pi-TopOS before, give it an other try because ithey say it now runs smoother and faster.The latest Raspberry Pi 3 B+ is now supported.
This video is a small portion of the current review.
Sorry about :
Please don't complain about the 2 issues above. I am already desperate about that.
I thought it would be a good idea to do a video review, but after seeing the result I'm not so sure anymore.
Please don't destroy me.
Important: the Raspberry Pi 3 B+ is a very sweet and appreciated bonus
included for this review. It is normally not included when you purchase a Pi-Top.
| {gallery:autoplay=false} Box Content |
|---|
Everything I received |
Here's what I found in my shipping box: There was a Pi-Top AND a Raspberry Pi 3 B+ as a BONUS :-D |
The Bonus Raspberry Pi 3 B+: Closeup view of the bonus Raspberry Pi 3 B+. I am repeating myself, but when you purchase a Pi-Top you have to purchase the Raspberry Pi separately. |
Opening the box |
There is a black pocket in the cover. What's in there ? |
It's the the cutout for the pi-topCODER Smart Robot, Music Maker, Space Race activities: See the links below if you want to print them yourself |
Let's go deeper in the box |
I found two manuals: Getting Started and Inventor Guide. See links below. |
Getting Started manual index |
There's something in the Getting Started manual. What is it ?: Oh! they included a Sandisk 8Gb Micro Sd Card and SD Adapter. It already as pi-Top on it. This was unexpected and very nice. |
Inventor Guide manual index |
18V, 2.5A power adapter with international plugs |
AU, EU, UK and US plugs |
Here are the links for the pi-topCODER activities cutouts, if you want to print your own:
Manuals:
| {gallery:autoplay=false} Inventor's Kit |
|---|
Wow I didn't know the Inventor's kit was included with the Pi-Top: I thought it was sold separately. I am very excited at this point. |
Included components |
The box is filled with goodies |
Closeup view of most of the content: Note that the LEDs are not the typical 5mm I normally use. They are 10mm large. If you decide to build your own Pi-Top and print your own activity cutouts (because yes you can), take that into consideration. |
CloseUp View of the pi-topPROTO+ board: It gives an easy access to the raspberry pi GPIO, VCC, Ground and 2 analog ports. |
pi-topPROTO+ board |
All sort of resistors: 100Ω, 150Ω, 330Ω, 470Ω, 1KΩ and 10KΩ (5 of each) |
Jumper cables and a metal wire for the space race activity |
I was out of banana, so I took a Raspberry for scale 
| {gallery:autoplay=false} The Pi-Top |
|---|
Front view |
Back view |
Back view, closeup: It's still empty |
Left side view: Nothing to see |
Right side view: You can lock the Pi-Top with a standard laptop lock cable |
Bottom view |
Inside view: The screen and the touchpad are very large. I love it. |
| {gallery:autoplay=false} Installation |
|---|
Slide the keyboard to open the Pi-Top |
You will find the multi tool on the rail, attached by a magnet |
It is both an SD card removal tool and a screwdriver |
Unscrew the cooling bridge: The multi tool seems to be working |
Slide the hub |
Hub fully slided |
Remove this part. It was used to protect the cooling bridge during shipping |
Part removed |
Install the Raspberry Pi: If you give a little angle to the Raspberry Pi, as shown above, it will be easier to install |
It's time to screw the Raspberry Pi |
Multi tool is ok, but... I gave up. I was unable to screw the Raspberry Pi with the multi tool so I took my favorite screw driver. |
Slide the hub. Make sure the HDMI and the audio port are connected properly |
Install the cooling bridge: Apply a gentle pressure where my fingers are located to make sure the 2 ports are properly connected. |
Screw the cooling bridge |
Reward yourself by removing this slooooowly |
The Raspberry Pi ports are perfectly aligned |
Time to boot the Pi-Top |
This is the initial configuration |
Select your language: The selection is limited. If you want to change the OS language, you can do it later in the standard Raspberry Pi settings. However, Pi-Top applications embedded in the Pi-Top Dashboard (like Pi-Top coder and CeedUniverse) will keep the language configured here. |
Read and accept the license of agreement |
Select your keyboard language: The selection is limited. If you want to change the OS language, you can do it later in the standard Raspberry Pi settings. However, Pi-Top applications embedded in the Pi-Top Dashboard (like Pi-Top coder and CeedUniverse) will keep the language configured here. |
Configure your Wi-Fi: If you have the new Raspberry Pi 3 B+, you will have access to the 5Ghz WiFi :-) |
Pi-Top will check for updates: It will also check for updates periodically |
Apply the updates |
Press Enter to install |
That's it. The Pi-Top is ready to go |
| {gallery:autoplay=false} My Gallery Title |
|---|
Pi-Top Dashboard:When you boot Pi-topOS, the Pi-Top Dashboard opens automatically. The Dashboard gives an easy to navigate view / launcher for the major applications that comes with the OS. It is an app so you can be closed if you prefer the Raspberry Pi Desktop |
Raspberry Pi Desktop on the Pi-Top |
Programming |
Office Tools |
Internet |
Games |
Accessories |
Education |
Graphics |
Python Shell |
Node-RED: Node-RED is a programming tool for wiring together hardware devices, APIs and online services in new and interesting ways. https://nodered.org/ |
| {gallery:autoplay=false} CeedUniverse |
|---|
CeedUniverse main screen: This game has a story mode or an arcade mode. |
Arcade mode: It gives you a quick access to the games you find in the CeedUniverse story mode. All the puzzles are there in one place. |
Data Types game: This is a agility game. Different data type values (int, float, bool, string) will appear in the middle of the circle and move to the outer circle. Your goal is to change your type to match the value coming and catch it before it disappear. Each data type is color coded to help the player. By the end of this game, I can promise you will be a master of those 4 types. |
Nano Bot: The goal is to teach about function. The goal is to lead the nanobot to the destination by selecting the next steps. |
Nano Bot Functions: You will learn that a function can be called multiple times |
Nano Bot Functions Within Functions: You will also learn that a function can call a function |
Crack Locks: the goal of this game is to lean Python. A Python code is presented and you have to modify a few variables win |
Crack Locks: The complexity increase with each level |
Crack Locks: In the last level, you have to write the entire code in Python |
CeedUniverse Story Mode: In the story mode, your character is an astronaut. It's spaceship crashed on a mysterious planet. Your goal is to repair your spaceship by traveling through the planet and resolving puzzles related to software development. Image Source: Games of 2018: British Games | Kotaku UK |
Story Mode Puzzle: I found a puzzle. Each puzzle is also available in the Arcade Mode. |
PiTopCODER is an application designed to teach about Python development.
Combined with the Inventor's kit, it also teach about GPIO and electronic circuits.
| {gallery:autoplay=false} My Gallery Title |
|---|
Pi-TopCODER Sections: Pi-TopCODER has 3 sections. The tutorial is located in the left section. It contains instructions and code samples. The middle section is the development dashboard. This is where you code. The right section is the console. If you print information this is where you will see it. |
Tutorial: the tutorial is in the left section |
Components information: If the project includes hardware, you can click on the name of each component to see what the component looks like and with is it's function in a circuit |
pi-topPROTO+: the connections clearly displayed in the left section. If you can count holes, you can do it |
Middle section: You can manually write the code in the middle section OR you can click the green arrow in the left section and the code will be automatically pasted to the middle section. |
Console: As you can see, "blinking" was printed to the console (right section) |
Cutouts: This is my teenage girl, Alicia, having fun with the Smart Robot cutout. Everything is precut. You just have to glue. She used 2 sided tape. She's shy so you won't see her face. |
Smart Robot: The smart robot is assembled and Alicia is starting with the first activity "Hello World". The goal is to make the LEDs blink |
Coding: The first activity is almost over. You can see that she is very concentrated |
Smart Robot is almost finished: The connections and the hardware is getting more complex with each chapter. This is the last chapter of the Smart Robot activities |
Proximity Sensor: Good job Alicia. The proximity sensor is working. The LEDs are blinking when detecting a presence |
Smart Robot last activity closeup |
My goal was to determine if this laptop could be used for school. My teenage girls need a fast browser, Youtube, and document editors.
The LibreOffice spell checker is not installed by default. I installed English US and French dictionaries.
sudo apt-get update sudo apt-get install myspell-en-us sudo apt-get install myspell-fr
I decided to compare the same relatively complex document in LibreOffice, Google Docs and Office365.
I also tried Youtube and cought my daughter on the Pi-Top instead of her old slow Windows 10 laptop.
See the result in the image gallery below
| {gallery:autoplay=false} Office Applications |
|---|
Libre Office Writer: The document is as expected. No issue |
Libre Office Writer Spell Checker: The spellchecker shows too many choices. Often, the correct word is in the 3rd or 4th position. It could be better. Also, it does not correct grammar. -1 for this test. |
Google Docs : The document is as expected. There is no lag in Chromium and if you open in full screen, you forget you are in a browser |
Google Docs Spell Checker: the result is as expected. Only one word is proposed and it's the one I want. Google docs also verify grammar. +1 |
Office 365: The document is as expected. There is no lag in Chromium and if you open in full screen, you forget you are in a browser |
Office 365 Spell Checker: the result is as expected. Only one word is proposed and it's the one I want. Office365 also verify grammar. +1 |
Chromium is fast and doesn't lag: At some point I had Google Search, Office365, Google Docs, Youtube all open at the same time and it was still strong. +1 |
Youtube doesn't lag thanks to the new Raspberry Pi 3 B+ and it's faster WiFi. I only had a few lags in full screen with HD resolution. Other than that, it was strong. +1 |
I caught Florence, my older teenage girl, on the Pi-Top instead of her old and slow Windows 10 laptop: Her Windows 10 laptop was recently formatted but it remains slow. She decided to try the Pi-Top and preferred it to her Windows laptop. That's a very good sign |
LibreOffice Impress: Florence was creating a presentation about elephants using LibreOffice Impress |
I had issue pressing the tab key.
Upon further investigation I found out that the key is larger than the hole.
I removed the key to be sure and reinstalled it after.
I wrote to the pi-top support support@pi-top.com and they replied within 20 minutes.
They explained that it was a first and they offered to swap the pi-Top on the spot.
I asked to keep it until I finished my review. I will swap it after. They had no problem with that.
My conclusion: very good support. You can purchase their product with confidence.
If you are interested, here's their reply :
"Thanks so much for getting in touch and sorry to hear your received a pi-top with a very unusual tab key on your keyboard. I've not come across this before as our pi-top's go through a number of tests so I'm surprised to see how this one slipped through 
Of course as this is likely to be preventing you from using that key we would happily replace your pi-top unit with a new one. In order to do this we would collect this unit so we can get out engineers to investigate further and simultaneously deliver a new unit the same day.
Please accept my apologies for any inconvenience caused and if you're happy to go ahead with the collection and replacement of your unit, kindly confirm the details below so I can book this on with our courier straightaway."
| {gallery:autoplay=false} Issue with the tab key |
|---|
Tab key is hard to press and sits on top of the hole |
The tab key is definitely larger than the hole |
If you want to use the Pi-Top as a regular laptop, I suggest to read the Raspberry Pi Magazine #59: PC Challenge.
It contains lots of tips and tricks about that and it's free to download.
https://www.raspberrypi.org/magpi/issues/59/
Direct download: https://www.raspberrypi.org/magpi-issues/MagPi59.pdf
If like me you prefer natural scrolling on your touchpad, here's the recipe.
Navigate to the 40-libinput.conf file in /usr/share/X11/xorg.conf.d
and change the first section as follows:
Section "InputClass"
Identifier "libinput pointer catchall"
MatchIsPointer "on"
MatchDevicePath "/dev/input/event*"
Driver "libinput"
Option "NaturalScrolling" "true" #ADD THIS LINE
EndSection
This laptop is definitely strong enough to be used as a laptop for students.












The Pi-Top Dashboard has built in shortcuts for Google Docs. It opens in Chromium and you can run it in full screen by pressing F11 to get an immersive experience. The spell checker is perfect and checks for grammar errors. It can open documents created with Word or LibreOffice. It's free. If you have an internet connection available, I would suggest to use it over LibreOffice because of the spell checker.







Total is $376.24$ - $404.98 (or $459.68 - $494.39 CAD)
It's not cheap. Of course for this price you will compare the Pi-Top to regular laptop.
My teenage girls Windows laptop cost about this price.
Since we have the Pi-Top, they stopped using their Windows laptop because it's too slow and they want to bang their head on the wall every time they use it.
Sometimes, better technical specs doesn't give you a better performance.
The Pi-Top OS is what makes this little unit so powerful. It is light and won't consume too much memory or CPU.
There are cheaper options if the Pi-Top doesn't match your budget :
After testing the Pi-Top, I learned that I should have purchased it sooner.
If you still hesitate about purchasing it, build your own.
It's the cheapest option and you will know for sure if your are ready for the Pi-Top.
Every school should have a lab with Pi-Top units (I would recommend Pi-TopCeed for school).
Every home user who can afford it should go directly to the Pi-Top laptop because it's hard to be tied to our desk when the couch is so inviting.
In the rating, I gave an 8 to Product Performed to Expectations because of the lack of a built in speaker and my deception with the LibreOffice spell checker.