RoadTest: PICOSCOPE 5444D MSO - USB Oscilloscope
Author: genebren
Creation date:
Evaluation Type: Test Equipment
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: see below Market Survey section
What were the biggest problems encountered?: I found the PicoScope 6 software to be somewhat difficult to use and/or understand. The instinctive user experience of using a scope with knobs is completely lost in button icons and, pull downs and screen presentations. But having said that, this is a very capable and useful oscilloscope. The more I used it and consulted the manuals, the more comfortable I became.
Detailed Review:
First off, Thanks! I am extremely grateful to element14 and Pico Technologies for selecting me as a roadtester for the PicoScope 544D MSO.
This is my first attempt at a roadtest, so I hope that I can successfully manage to inform and rate this instrument fairly.
Market Survey
There are many fine standalone, bench oscilloscopes available. In the area of 4-channel, mixed signal oscilloscopes here are some of the competitive models:
Getting this level of performance in a highly mobile format, like the PicoScope 5444D MSO, there are no other comparable devices. The compact size however, does come with a few disadvantages. The limited voltage input range of +/- 20 Volts, with 1X probes and/or coax cables is one of those limitations. Granted, 10X probes give you the ability to get +/-200 volts, but for some people this is not a workable option. The pricing of the PicoScope 5444D MSO does get very close to the lower end pricing of some standalone oscilloscopes (i.e. Rigol MSO7024).
Unboxing
The shipping package arrived in good shape, with no obvious damage.
Removing the packing slip and cutting the tape, reveals the packing materials (simple but effective crumpled paper).
Digging deeper into the package, below the first layer of crumpled paper, the actual product box is in view.
With the product box removed from the shipping package, a quick inspection shows the product box has survived the shipping with no apparent damage. Opening the product box, the PicoScope 5444D MSO is seen carefully cradled in a cardboard surround.
Removing the upper-level cardboard surround, we can see the lower-level accessory box and the contents below.
Finally, all of the unboxing is done and here are all the accessories.
Software download (Window 7 example)
The current version of the PicoScope 6 software is available on the Pico Technology website (https://www.picotech.com/downloads ).
Selecting the Download, the following pop-up appears:
Selecting the 'Save File' option causes the installer to download. Once the file (installer) is downloaded, clicking on the downloaded file from within the browser causes Windows to prompt with a 'Security Warning'.
Accepting the 'Run' option starts the install process which prompts with the Language selection pop-up.
Selecting the default of English (as I am an English speaker/reader), causes the InstallShield Wizard to ask you to 'accept' their license, which allow the install to continue (when you click on 'Install').
After a while, the Status Bar appears, and after another while, the process begins.
Then Windows will ask if the really wanted to install this program.
Then later in the install, Windows will ask you again to make sure that you really want to load this program (This message appeared a couple of times, until I got tired and just clicked on the 'trust' button).
And finally, the software is installed (did I mention how much I love the Windows install process?
)
After connecting up the hardware and doing a little playing around with settings, I was able to attach a scope probe and make a measurement. I am currently working on a client's project, so I had some interesting signals to look at. I really like the 'measurements' that you can setup to interpret the signal. Here we see that the square wave has the following parameters: High pulse width of 19.2us, Frequency of 26.01khz, Duty cycle of 49.94%, with a rise time of 17ns. This is good news and a great start to seeing what this product can do.
Operation and user experience
As per my roadtest application, here is my plan for testing out the performance and functions of the PicoScope 5444D MSO Oscilloscope.
Conclusions