RoadTest: Arduino Portenta H7 Development Board
Author: ajayvishaal
Creation date:
Evaluation Type: Development Boards & Tools
Did you receive all parts the manufacturer stated would be included in the package?: True
What other parts do you consider comparable to this product?: Arduino mkr 1010, Arduino Nano BLE Sense
What were the biggest problems encountered?: I didn't face any major issues. However getting started with the board and setting up the Arduino IDE and Arduino Pro IDE in Linux as well as Windows to work with Portenta took some time.
Detailed Review:
Introduction:
First of all I wanna Thank Element14 for giving a great oppourtunity to roadtest the Arduino Portenta Board. I was a very good roadtest journey. It paved a way for me to explore many new things.I'll be sharing all my experience in this review and I hope I'm giving my best in writing the roadtest review. I received the board in a neat package
| {gallery} Arduino Portenta Board |
|---|
![]() |
Getting Started:
The New Arduino Portenta has a lot of feature to explore. Some of the features includes
Installing the board in the Arduino IDE and Arduino Pro IDE was easy, but then I faced some issues in uploading the code to the portenta. I got some error like this dfu-util: Invalid DFU suffix signature. At first I've no idea about this issue. Then I started googling and found solution for this issue. Since I'm using Ubuntu 18 os there were some packages blocking the Arduino IDE. However I managed to remove those packages and then I started with the Hello World Program of arduino. I flashed the basic blink program in the Arduino Pro IDE to check if the issue persists. Fortunately everything worked fine.
Arduino PRO IDE:
Arduino Pro IDE is a new enhanced version of classic Arduino IDE with a lot of features for advanced developers. The Arduino Pro IDE(Alpha) is available for Linux/Windows as well as Mac OS.The Alpha release is for testers and not yet recommended for production use. The new features of the Arduino Pro IDE include:
The Pro IDE has a GUI similar to Visual Studio Code. This IDE is very much suitable for programming and debugging this advance Arduino Board. The Arduino Pro IDE's GUI is given below:
| {gallery} Arduino Pro IDE |
|---|
Testing:
I've planned to test the board by implmenting in a robotic application. Due to the lesser supporting documents regarding the implementation of AI in the portenta. I'm still working on it. Also, I'm working on tensorflow lite packages inorder to deploy TFLite in Portenta. But I managed to test the wifi functionality of the board. Since the Portenta has an Inbuilt Wifi and Bluetooth module, It is very much useful for the user to deploy the Arduino Portenta board in IoT based applications.
I've tested the portenta board by connecting it to my mini robo arm. I've just done motor control test. The results are satisfactory. However this simple process also makes the board to get hot. Also When I uploaded the blink code in the board, the board gets hot. I'm attaching some of my testing pictures here,
| {gallery} Testing |
|---|
Future Works:
Conclusion:
I think I've done my best in reviewing the board. However, I've planned to make many updates while exploring the features of the board. Some of my conclusions are as follows:
The above are some of my conclusions. But this is not the end. I will be updating my exploration journey with the Portenta Board whenever I'm trying something new with it.
Thank You!