AVNET 96Boards Dual Camera Mezzanine + Ultra96-V2 - Review

View table of contents ...  

RoadTest: AVNET 96Boards Dual Camera Mezzanine + Ultra96-V2

Author: sudiptasen

Creation date:

Evaluation Type: Development Boards & Tools

Did you receive all parts the manufacturer stated would be included in the package?: True

What other parts do you consider comparable to this product?: Intel - Altera -Development Kit

What were the biggest problems encountered?: Lack of documentation, and not easy to find the latest versions of any software. We had to write our own software to make it useful. We had to build our own Linux (Petalinux) to be able to compile with comfort and ease.

Detailed Review:

Our goal with the kit was two fold. One to do a multi-camera image detection (using 4 camera sources) and then also to be able to run different sensors to the kit and then be able to control the cameras and the sensors simultaneously. The Kit was able to do that very comfortably. When I say comfortably, that is the HW was able to detect the 4 sources and the FPGA was able to compile and run the IR very cleanly with horsepower to spare.

 

When we first see the kit, the cool part is that there are multiple power supply headers for different countries. That is a very good idea, because we were able to send the kit to other folks across the world and the different power supply connectors are a huge help. Thank you to AVNET for supplying that.

 

The initial impression of the kit was the wonderful packaging of the kit, which makes it easy to open an it does not seem flimsy at all. The box and the kit was very well packed.

 

 

 

 

.image

 

 

 

The kit initially has the micro-SD card and the instruction sheets. You have to immediately go to the Xilinx web site and get more details. The Xilinx web site is essential to be able to get all the support materials. We have used Xilinx products before and so, it was not that complex once you know how to navigate the web site. Thus we have given them a 7/10 rating. For the price and performance this is a FANTASTIC kit. But, it is essential that you follow the instructions of the SoC on the Xilinx web site. That is essential.

 

Attached is a picture of how the item looks like when you open it.

 

image

 

This is how the board looks like with the documentation. It looks small, but , my goodness, it DOES pack a mean punch. It hits far far above its price point. We work with multiple SoC parts, and for IIOT applications and machine vision, this is by far the best value for money.

 

Now, for the ease of connecting other parts and other sensors to the board, there is a connector on the board, and  the Ultra96 family of connectors can fit. Please check this part : https://www.96boards.org/product/sensors-mezzanine/ . That is an extra part we also found was very easy to attach and program using the Ultra96-V2 board. I am attaching a picture of the Grove board, which would also highlight how easy and wonderful the mezzanine connector is  .

 

image

 

Please see pictures of the Ultra96-V2 along with the Grove Mezzanine board (which makes this kit into an even more cool product).

 

The two board can be placed on top of one another and I am attaching two pictures, one of the boards attached and one of the usage of the ports of the Ultra96-V2 board. We used the Micro-SD to boot the unit and also used a 32GB USB drive (We used USB 2.0 drive as speed of transfer was not really our concern) . The mezzanine experiment detail is explained here in the pictures, The dual-camera experiment is shown from the implementation perspective, as you will see in subsequent screenshots.

 

image

 

The MicroSD for the Boot-linux and the USB 2.0 Drive attached . The Petalinux (default) which is supplied is OK at best, we had to build our own Petalinux version (from source code links available) and that took some time. That specifications were NOT supplied very well anywhere to be found. We had to make the code from scratch and that took a lot of time and effort. Wee wish that there were some easier and more universally available code with which to work . But, after some effort, we were able to get this to work and the boot system finally looked like this . The Petalinux which is supplied by the board is not very easy to modify and it messes up the build. So, we decided to build out own by reading the Petalinux documentation. That gave us all the flexibility that we needed.

 

 

image

 

The build of the ports are very sturdy, and the Mini_display Port to HDMI cable is essential to get if you want to use a monitor which is essential. The MicroSD was used for booting and the USB Drive (in RED colour here) was used to  transfer and load the Image samples to the Main memory. After the transfer, we programmed the board to run off the images stored in memory and not to do too many transfers to the 32Gb card, and hence a USB 2.0 storage was absolutely fine.

 

With these as the start of the system, we used the system to boot up to a Image recognition system which this Xilinx Zynq UltraScale+ MPSoC ZU3EG A484 was tested by Xilinx. Their image recognition SW has been tested by a company called DeePhi and last we checked, all the DeePhi code is working on Xilinx UltraScale+ MPSoC ZU3EG . This board is very very useful, as it is one of the few on which this code has been tested. That helped jump start our experiments a great deal. The link to download the programming of the FPGA is available on the Xilinx web page and we could make it compile on the Ultra96-V2 on our own Petalinux build.

 

After attaching the display, we , of course, gave complete acknowledgement to DeePhi for their codec and here is our boot screen.

 

image

 

Then the requirement was to load 4 separate video streams and be able to run a few different types of image classification to see if the FPGA could handle multiple different streams

 

 

We picked :

- mobilenet

- Inception v1

- Resnet

 

At first we tried to run two streams and then ramped up to 3 and then 4 streams . All of them worked fine. We also added the Mezzanine camera module as another control input. I apologize that I do not have pictures of the camera module input stream.

 

The screen shows the 4 terminals being opened on the Ultra96-V2.

 

image

 

After that we have the 3 streams running simultaneously

 

image

 

And then with slightly increasing the available memory to access ( simple Linux call ) we got the Ultra96-V2 to process image classification on 4 streams simultaneously

 

image

 

From the CPU utilization, it can be a little misleading. The 3 stream case has the 4th ARM core at 99.3% , but that is code execution only. In the 4 stream case, all the ARM cores are being used in image classification in some way.

 

The Quad ARM cores can be utilized to their fullest and the result shows. The FPGA , which is at the heart of the Ultra96-V2 is more than capable of handling the following :

 

- 4 image classification streams

- 3 separate inputs from I/O sources

- External Camera input from Mezzanine card

 

Our tests are conclusive. And this AVNET part works very well

 

Here is the final screen with all the parts of the Ultra96-V2 being stressed to the max.

 

image

 

In Summary of this amazing part from AVNET

 

Summary:

 

1. Very well built product with lots of room for modification

2. Not very good documentation with the kit, but excellent information on the SoC (the core FPGA) available on line with XILINX

3. The Ultra96 form factor stays true to the 96Boards.org concept and it very useful for prototyping

4. The thing to remember is that for the price, (sub $300), you get a LOT of features and practicality. It is meant to be a prototype board which can be taken into production, once you use this board to verify, validate and prove out your design.

5. This is definitely not intended for being a production level (I wish that we could get AVNET to build this as a production level part), as we have an airport security system, who would gladly buy 1000-s of these boards.

6. The mezzanine card and the connectors are very strong and firm, and there is no "loose" parts. The board is very well built and can take a lot of punishment

7. The power supply is a little bit too big, and I am sure that you can find a smaller power supply with the same amperage

8. In all, a very well designed product.

 

Many thanks to AVNET for this wonderful design and many thanks to Randall for his help and advice

 

With best wishes

 

Sudipta Sen

March, 2021

Anonymous
  •   wrote:

    Yes, of course we did test the camera as we had promised to do. But in my report I had apologized saying that we did not put any pictures of the camera test in the report.

    You're supposed to be road testing the Dual Camera Mezzanine. If you don't include anything about the camera then you haven't tested it.

  • Dear Jon,

     

    We used a SONY IMX camera sensor (and made our own modules) to fit the Mezzanine card slot, for OUR experiment.

    Our requirement was for a Security System and SONY sensors (colour / high resolution) was essential.

    After the tests with the Mezzanine sensor ( for the road test portion), it was found that the sensor was not "powerful" enough for the work in hand, and we were asked to move to a SONY IMX series sensor.

    And of course, we  had  to multiplex the video streams, which is easy.

     

    Thank you for your note.

     

    Best wishes

    Sudipta

  • Dear Sir,

     

    Greetings from Sudipta Sen. Yes, of course we did test the camera as we had promised to do. But in my report I had apologized saying that we did not put any pictures of the camera test in the report. We apologize, as we needed to add 4 camera sources (and the Mezzanine camera board was not powerful enough to handle the resolution). My apology is written in the report. I am attaching the portion that I had written, "We also added the Mezzanine camera module as another control input. I apologize that I do not have pictures of the camera module input stream.".

     

    Thank you for your note.

     

    Best wishes

     

    Sudipta

  • FYI. You are taking a big risk putting that nice board directly onto a carpet....unless I'm wrong and they have brought out new colours of anti-static matting!

     

    That said, when I was a teenager I used to dump my collection of CMOS out of an old icecream tub and onto a carpet to sort through them...whilst I never had an obvious failure I probably impaired the performance long term (i.e. reduced the MTBF, ability to operate at the higher voltages).

  • I have a similar question since I have still been struggling to get anything, such as OpenCV,  to recognize the video input from the Dual Camera Mezz board.  I would be interested in how this was set-up with Deephi which appears to be part of Vitis-Ai now.  Perhaps me giving that a try may show different results from my other experiments.

     

    One thing though, the images on the screen appear to be in color yet the Dual Camera Mezz only produces Monochrome images.  Perhaps another camera module was used such as the  D3Camera or Delta Camera Kit.  But then again it is referenced there were 4 camera inputs where the Dual Camera Mezz only has 2 cameras.

  • I'm a little confused by your road test. Did you even use the Dual Camera Mezzanine that you're supposed to be testing? image