RoadTests & Reviews
  • Products & Partners
  • More
RoadTests & Reviews
Documents Atmel Xplain
  • Blogs
  • Forum
  • Documents
  • RoadTests
  • Reviews
  • Polls
  • Files
  • Members
  • Sub-Groups
  • More
  • Cancel
  • New
Join RoadTests & Reviews to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: awinning
  • Date Created: 10 Nov 2009 1:43 PM Date Created
  • Last Updated Last Updated: 7 Oct 2021 1:15 AM
  • Views 1078 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Atmel Xplain

Atmel’s Xplain evaluation and demonstration kits are not yet available to buy, so the lucky recipients will be among the very few members of the public to actually possess them.

 

The Xplain is an easy-to-use evaluation and demonstration kit for the Atmel’s ATxmega128A1, offering a complete hardware solution for evaluating the highly accurate analog functionality of the device. The ADC can be used to read a temperature sensor and a potentiometer, and the DAC can be used to generate sound on a mono speaker.

 

Xplain also demonstrates how to interface external memories; the kit features 8MByte SDRAM and 8MByte DataFlash connected to the ATxmega128A1. Eight push buttons and eight LEDs are available for user interaction.

 

The kit is powered from USB. The USB interface is a communication gateway between the ATxmega128A1 and an USB COM port.

 

ATxmega128A1

The ATxmega128A1 is part of Atmel’s XMEG A1 family of low power, high performance and peripheral rich CMOS 8/16-bit microcontrollers, which are based on the AVR enhanced RISC architecture. By executing powerful instructions in a single clock cycle, the XMEGA A1 achieves throughputs approaching 1MIPS per MHz, allowing the system designer to optimize power consumption versus processing speed.

 

The AVR CPU combines a rich instruction set with 32 general purpose working registers. All the 32 registers are directly connected to the Arithmetic Logic Unit (ALU), allowing two independent registers to be accessed in one single instruction, executed in one clock cycle. The resulting architecture is more code efficient, while achieving throughputs many times faster than conventional single-accumulator or CISC based microcontrollers. The XMEGA A1 devices have five software selectable power saving modes.

 

The device is manufactured using Atmel’s high-density nonvolatile memory technology. The program Flash memory can be reprogrammed in-system through the PDI or JTAG. A Bootloader running in the device can use any interface to download the application program to the Flash memory.

The XMEGA A1 devices are supported with a full suite of program and system development tools including: C compilers, macro assemblers, program debugger/simulators, programmers and evaluation kits.

  • xplain
  • demonstration
  • atxmega128a1
  • atmel
  • kits
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 16 years ago in reply to e14 Contributor

    Hi

    As AVR Studio recognise AVR Dragon as a programmer, it also associates the full family of Xmega AVR.

    So I think probably works, perhaps Updating your programmer will be necessary.

    There's no problem with JTAGICE MkII

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 16 years ago

    hi is it possible to program AVRXPLAIN with AVR Dragon programmer?

    I want to try Xmega, because I have lot of experience in other ATMega and I want to see the difference among these.

    But I have only Dragon programmer and I'd like to know if it's possible to reuse it.