Browse By Tags

  • Changing the "angle" list.

    Hello, I would like to change the "angle" list. Is there a command such as " SET DRILL_MENU " for changing the angle list (I would like 45° steps). I found nothing in the documentation, and I tried SET ANGLE_MENU, but it doesn't work..... anyone have…
  • Eagle Settings - Curved-Angled Bends

    As I have to operate from my laptop when visiting China AND having religiously searched every menu I am stuck with an Eagle that is only making 90 degree corners. Could someone kindly point me to where these settings are located? Thank you. A desktp Cadence…
  • Is there a way to move lines and objects in a straight angle

    Other drawing software has the option to lock the direction of movement by pressing and holding a key like the controll key. You move the mouse but when you hold the ctrl key the object of movement only moves straight in 90-degrees or 45 or 180, you get…
  • Freie Linie oder Track in NICHT 45 od 90° Winkeln

    Tach zusammen, vielleicht ist es ja eine dämliche Frage weil ich erst knapp zwei Wochen mit Circuit Studio arbeite, aber es treibt mich bereits in den Wahnsinn. Kann es sein, dass es nicht möglich ist Linien oder Tracks in freien Winkeln zu verlegen?…
  • Measuring speed, angle and height

    Hi all, I am discussing a possible project, but I am not certain how feasible it is. The project consists of using an Arduino, plus some sensor (or sensors) to measure the speed, angle and height of a flying object over a 6 x 30 cm surface. Although I…