Browse By Tags

  • Identity Protocol - Part 2 - Django Server

    Recap: The idea is simple enough: stop making people swipe a card and type a PIN at every single door. Instead, the ID card (a MAX32630FTHR + ATECC508A in your pocket) unlocks once via PIN, then silently does challenge-response crypto over Bluetooth…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-9 Project Submission

    Project Submission: The main problem which I want to address is the procedure after the company or brand gives the contract to an advertisement company like : 1) Replace the old posters which are on different heights and it can also be dangerous to replace…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-6

    TFT Example Code: I have taken this example from Cypress Website which is named as "CE223726 – PSoC 6 TFT Display Interface with EmWin Graphics Library" This code example demonstrates how to display graphics on a TFT display using EmWin Graphics Display…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-4

    Due to this COVID-19 pandemic situation, I got my Hardware very late, so I will skip the writing about PSoC introduction/architechture and their specification which is also available on the Internet. Let's jump to the practicals and directly hands-on…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-3

    IoT Protocols : 1) CoAP (Constrained Application Protocol): CoAP is designed to easily interface with HTTP for integration with the Web while meeting specialized requirements such as multicast support, very low overhead, and simplicity for constrained…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-2

    Here I have created the DataBase part of the Project which is responsible to store Customer data as well as the website content. To getting started with DataBase design I want to introduce the " PostgreSQL: the most advanced Open source Relational Database…
  • Connected Cloud Challenge - IoT based Advertisement BillBoards/Hordings - #BlogPost-1

    I have decided to divide this project into 4 parts as below : 1) User Interface (Website) 2) AWS IoT 3) DataBase 4) BillBoard (PSoC 6) and As I have discussed earlier that Due to Hardware not received so that I am working on User-interface First. Here…