Browse By Tags

  • Recherche de connecteurs pour moto Honda et Suzuki

    Bonjour, Dans le cadre d'une étude, je souhaite connecter mon application sur le faisceau électrique d'une moto ( marque Honda (model CBR 600 RR, Suzuki GSXR 1000)). Les connectiques sont vraiment difficile à trouver et je penses qu'ici, un constructeur…
  • Transform The Smartphone Challenge Returns

    In 2016 MotoMods and Indiegogo launched "Transform the SmartPhone 2016" contest, in which Motorola and Indiegogo helped you to create a custom, snap on, add on for the Motorola Z family of phones. Current Mods include Amazon Alexa Speaker set, a Projector…
  • Moto Mods Developer Part 9 - Updating the Hardware Manifests file

    See part 8 here. Before we compile Nuttx, we need to change the hardware manifest file. The .mnfs file for Blinky is located in ./nuttx/apps/greybus-utils/manifests as created above. Add the following lines to the end of the document: At the top of the…
  • Interview with Livermorium Founder, Chen. - Transform the Smartphone Challenge

    Interview with Livermorium Founder, Liangchen Chen. Now that Transform The Smartphone Challenge Returns 2018 is live, we thought it was time to sit down and interview the winners of the last Moto Mods accessory competition. In this Interview, element14…
  • Need help with your Moto Mods?

    As a former Motorola employee, and senior member of the Moto Mod architecture, design, and validation team, I can offer my unique expertise in all things Moto Mod. I can help with design, development, bring-up and troubleshooting of HW, SW, Test, & Manufacturing…