3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Recommendation for a kit to build my first 3d printer.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 346 subscribers
  • Views 2101 views
  • Users 0 members are here
Related

Recommendation for a kit to build my first 3d printer.

majorkuso
majorkuso over 11 years ago

I would like some recommendations on a kit so I can build a 3d printer. would it be possible to build one with similar resolution as the robox? I was looking into the reprap prusa i3 models.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to Workshopshed +3
    Or even much more complex objects like this Most of the parts for the Thorn gun from the game Destiny and as you say, it sucks when it fails part through
  • bobthechemist
    bobthechemist over 11 years ago +2
    Hi, Looks like I'm late to the party, but I thought I'd chime in. I purchased a makerfarm i3v 8" model at the beginning of the summer. I went with a kit primarily for the opportunity to build something…
  • Workshopshed
    Workshopshed over 11 years ago +1
    Hi James, I don't have any specific recommendations but some thoughts on the factors to consider. I think there are 4 key reasons to want to build a kit you enjoy building stuff you can learn more about…
Parents
  • bobthechemist
    bobthechemist over 11 years ago

    Hi,

     

      Looks like I'm late to the party, but I thought I'd chime in.  I purchased a makerfarm i3v 8" model at the beginning of the summer.  I went with a kit primarily for the opportunity to build something, but price was also a consideration, as I could not find a satisfactory model below my price point.  The building process was pretty straightforward and the only real problems I encountered were NOOB style (e.g. not tightening set screws).  It took roughly three weeks for me to build, calibrate and get to know my printer sufficiently to print functional parts such as the gears to Greg's extruder.  I've designed a few things ( http://www.thingiverse.com/bobthechemist/about ) and have been able to print a number of basic designs. 

    The greatest challenge I've had is bridging, which was only recently resolved by the addition of a cooling fan.  In my case, I was pleasantly surprised that the kit I purchased had all of the non-printable parts for this design, which either speaks to the suppliers forethought or the maker-communities ingenuity.  I can now print this bridge successfully in PLA.

    In the several months since I've been printing with a kit-based printer, I've only had one functional problem, where I ended up clogging the hot end during a filament switch from ABS to PLA.  In this case, I ended up applying too much pressure to the filament and the hot end leaked.  Since I built the printer, it was pretty straightforward to remove the problem parts for repair, which required a lengthy soaking of the metal hot end components in a sonication bath containing methylene chloride.  (I have a laboratory outfitted to do such things, and would not recommend this for an at-home user.)  My point here is that I *don't* know if this type of problem would also happen with a commercial instrument that has sufficient bells and whistles to assist the user in changing filaments.

    In the end, a major purpose for purchasing a kit rather than a commercial printer was the engineering design aspect of the hobby.  Not only did I want to build the unit, but I wanted a platform to modify, hack, break and repair.  If these tasks sound at all appealing, then I would recommend the kit approach.  (Now, given that I'm replying to your post 2 months late, I suspect you've already made your decision.)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bobthechemist
    bobthechemist over 11 years ago

    Hi,

     

      Looks like I'm late to the party, but I thought I'd chime in.  I purchased a makerfarm i3v 8" model at the beginning of the summer.  I went with a kit primarily for the opportunity to build something, but price was also a consideration, as I could not find a satisfactory model below my price point.  The building process was pretty straightforward and the only real problems I encountered were NOOB style (e.g. not tightening set screws).  It took roughly three weeks for me to build, calibrate and get to know my printer sufficiently to print functional parts such as the gears to Greg's extruder.  I've designed a few things ( http://www.thingiverse.com/bobthechemist/about ) and have been able to print a number of basic designs. 

    The greatest challenge I've had is bridging, which was only recently resolved by the addition of a cooling fan.  In my case, I was pleasantly surprised that the kit I purchased had all of the non-printable parts for this design, which either speaks to the suppliers forethought or the maker-communities ingenuity.  I can now print this bridge successfully in PLA.

    In the several months since I've been printing with a kit-based printer, I've only had one functional problem, where I ended up clogging the hot end during a filament switch from ABS to PLA.  In this case, I ended up applying too much pressure to the filament and the hot end leaked.  Since I built the printer, it was pretty straightforward to remove the problem parts for repair, which required a lengthy soaking of the metal hot end components in a sonication bath containing methylene chloride.  (I have a laboratory outfitted to do such things, and would not recommend this for an at-home user.)  My point here is that I *don't* know if this type of problem would also happen with a commercial instrument that has sufficient bells and whistles to assist the user in changing filaments.

    In the end, a major purpose for purchasing a kit rather than a commercial printer was the engineering design aspect of the hobby.  Not only did I want to build the unit, but I wanted a platform to modify, hack, break and repair.  If these tasks sound at all appealing, then I would recommend the kit approach.  (Now, given that I'm replying to your post 2 months late, I suspect you've already made your decision.)