3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Closed-loop control for low-cost 3D printers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 48 replies
  • Subscribers 346 subscribers
  • Views 12117 views
  • Users 0 members are here
  • closed-loop
  • servo-control
  • 3d-printer
Related

Closed-loop control for low-cost 3D printers

morgaine
morgaine over 12 years ago

A challenge given to Ben Heck in March of last year was "Challenge - cheap 3D printer" (design a 3D printer more cheaply), and that thread continues to receive replies to this date.  Unfortunately nobody in that thread actually addressed the matter as a design issue.  Instead, most of the replies (including from Ben) seem to have addressed an entirely different question, how to build the same kind of 3D printer as you can buy today, but for less money.

 

Those are two completely different questions.  It was pointed out by Ben that because of the race to the bottom by a huge number of manufacturers, the current designs can't be made a lot cheaper while still retaining the same speed and accuracy.  That's probably correct with respect to current standard designs, but it says nothing at all about different designs.

 

So, this thread suggests a different design approach that may offer a solution, and it's a pretty natural step to take.

 

A useful observation with which to start is that the accuracy and precision obtainable with today's RepRap-style models stems from the design of their stepper motors and the limitations inherent in screw drives and belts and pulleys and the rigidity of their physical construction.  Because of this, if you retain the existing design model but in the quest for lower cost you compromise on one of these areas, you are very likely to lose the necessary degree of printing accuracy even if you are performing steps at very high resolution, so that's not likely to be a good way forward.  Printing with high precision in the wrong place is not helpful.

 

That observation about accuracy and precision leads us directly to a solution though.  Engineers know full well how to gain high and definable accuracy without each of the components being manufactured to extreme tolerances, and that's by using closed-loop control with negative feedback, the basis of servo-systems.  In a closed-loop system, the only thing that needs to be highly accurate and with known precision is determination of current position, and the heart of that need be nothing more costly than a very accurately printed graticule which can be produced for pennies.  Given the ability to know where the operating head is located very accurately in each relevant axis (not necessarily Cartesian), the only other requirement for maintaining that limit of accuracy is rigidity of coupling between sensors and operating head, ie. the hot end in a 3D printer.  Very importantly, there is no need for rigidity in the motor assemblies --- as long as they're moving the head in the right direction, that's good enough.

 

So, I'll recast the original question differently and tie it to this specific way forward:

 

"How can we design a 3D printer based on closed-loop control to gain high accuracy and overcome low cost construction through use of negative feedback?"

 

It's mostly a matter of examining alternative physical arrangements to find one with good rigidity while also having low suspended mass and being amenable to construction with today's open-loop 3D printers as a stepping stone.  It's worth pointing out that virtually all 2D inkjet printers already use closed-loop control --- if you take one apart you'll find a positional sensor and fine graticule in there somewhere to provide very high accuracy in one dimension at the lowest cost.

 

Once we start thinking about closed-loop control for 3D printers, many possible advantages start to appear:

 

  • As already mentioned, it compensates for low-quality parts, so prices could fall much lower.
  • Closed loop operation compensates for latitude at assembly time as well, also leading to lower costs.
  • Very much higher accuracy than we have today is possible, and that cannot be done open loop.
  • Motors of many different kinds can be used, AC, DC, brushed, brushless, linear, and also steppers.
  • If steppers are used in a closed-loop system, you can overdrive them without worrying about "lost steps" because the steps aren't used for position control anyway, yet you still retain the advantage of high holding torque.
  • Much higher speeds are possible than we have today because of the two-fold advantage of wider motor choice and arbitrarily high acceleration while the control loop seeks to its desired position.
  • Accuracy and precision are more independently controllable in closed-loop systems.  This provides more opportunities for cost reduction through tradeoffs, as well as dynamic optimization in favour of speed, for example on in-fill.  In open-loop printers with stepper motors, the step size places a limit on precision of positional control, but this is very rarely reflected in the accuracy of actual positioning which is primarily determined by physical construction.

 

I'm sure there are many other benefits.

 

The main disadvantage is that this direction requires new thinking, new solutions.  And there's the challenge! image

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +3
    The topic above is deliberately open-ended and proposes nothing more than closed-loop control, hopefully to encourage people to think laterally and very widely instead of being shackled by a specific construction…
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor +2
    I'm talking about making the work head's position be determinable to high levels of accuracy --- the distinction between accuracy and precision is important in this context, because we need to know the…
  • vsluiter
    vsluiter over 12 years ago in reply to morgaine +2
    Hi Morgaine, It's what Nanotec is already selling for industrial use: stepper motors driven as 2-phase brushless DC motors. Very nice features as high torque, high accuracy, low noise....
Parents
  • morgaine
    morgaine over 12 years ago

    Just to whet our appetites for head position sensing a little, here's the Performance page for Renishaw's RESOLUTETm range of absolute optical encoders,  claiming "1 nm resolution, 100 m/s maximum speed, accuracy to ±1 µm" for the linear versions.

     

    It's fair to say that 1 µm accuracy is excessive for our current needs and industrial pricing is probably excessive for our pockets, but the much simpler encoder strips and sensors in inkjet printers are available as spares at very reasonable prices (or indeed for nothing as salvage from dead machines) and are likely to do the job perfectly well.  Experimenting with these in a 3D printer setting would be interesting.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to morgaine

    ... Just keep in mind where you're measuring...  As you pointed out to me before, measuring at the motor shaft is not 'closed loop' enough for you. Would measuring the movement at the spindle be? Or would you need the movement of the printer head? That's going to pose a nice mechanical challenge aswell (mounting the sensors). The stiffness of the construction would have to be enormous to get a good measurement and control. Not to mention the speed of the control loop.

     

    Not to say that it's not possible, but this looks a bit as an 'academic' way of building measurement on measurement while loosing track of what you tried to accomplish. I'd put my money on a feed-forward model-based controller for short-term improved resolution printer. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • vsluiter
    vsluiter over 12 years ago in reply to morgaine

    ... Just keep in mind where you're measuring...  As you pointed out to me before, measuring at the motor shaft is not 'closed loop' enough for you. Would measuring the movement at the spindle be? Or would you need the movement of the printer head? That's going to pose a nice mechanical challenge aswell (mounting the sensors). The stiffness of the construction would have to be enormous to get a good measurement and control. Not to mention the speed of the control loop.

     

    Not to say that it's not possible, but this looks a bit as an 'academic' way of building measurement on measurement while loosing track of what you tried to accomplish. I'd put my money on a feed-forward model-based controller for short-term improved resolution printer. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 12 years ago in reply to vsluiter

    An error signal measured at each spindle does not contain error components from anything except that single axis of the transport, so such feedback cannot correct for anything else.  Even worse, if the encoder is on the actual motor shaft (rather than further along the transmission) then it contains no error signal at all relative to the motor assembly since the shaft is an almost rigid part of it compared to the rest of the transport which has many flexure modes.  That wouldn't be useful feedback in our context.

     

    I'm reminded of the Schneier term "security theater" as a verbal analogy.  If a system that is described as "closed loop" isn't taking feedback from its output then it's just engaging in "feedback theater", aiming for bullet points without actually correcting for the major output errors in the system.  Needless to say, feedback theater is not the goal for us.

     

    It's certainly an interesting mechanical challenge, but some candidate solutions are pretty obvious and simple.

     

    For example, camera-based solutions provide no mechanical drag at all and have a very simple structure.  The back-of-envelope numbers I gave in post #18 of this thread suggest that it's numerically viable for very small workspaces, and can be extended to cater for larger ones (but not yet ideal).

     

    Another approach which is quite appealing has a tiny camera mounted on the work head and pointing straight up through a macro lens focused on a 2D printed pattern which covers the entire top inner surface of the printer.  Again this imposes no mechanical stresses nor alignment difficulties, so it seems very experimenter-friendly.  Finding a good 2D tracking pattern would be an interesting project, and it might well be possible for absolute coordinates to be encoded within it.

     

    Mechanical position sensing is more problematic as you mentioned, but everything is hard until the moment that it's easy. image  I'd probably examine optical solutions in the first instance though, at least until a good mechanical design emerges.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to morgaine



    Mechanical position sensing is more problematic as you mentioned, but everything is hard until the moment that it's easy.

    Have you ever considered a career in marketing image? I know another good one: 'where do you want to go today?' image

    I'd probably examine optical solutions in the first instance though, at least until a good mechanical design emerges.

     

    Looking forward to your prototype / proof of concept!