3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum New Robox Materials/colours
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 341 subscribers
  • Views 1151 views
  • Users 0 members are here
Related

New Robox Materials/colours

celrobox
celrobox over 11 years ago

Hey Everyone,

 

We're happy to announce we are launching more colours and materials for the Robox!

 

We're increasing our range of standard PLA and ABS colours with the addition of sky blue and slime green and a new PLA only ThermoChrome filament that changes from purple to pink depending on its temperature.

 

We're also adding to our available materials repertoire with our first wood effect filament and an all new addition in the form of HIPS material.

 

You can read more about these filaments in our blog post here. Feel free to ask any questions below!

 

Cheers,

Simon

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 11 years ago +1
    Excellent. Any chance of scoring some samples to members ? It would be nice to experiment with this stuff.
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Yes, I agree with ipv1 , we would love to try out the new materials and report back in the form of videos and posts on our experiences Peter
  • ipv1
    ipv1 over 11 years ago in reply to Workshopshed +1
    The crystal clear has my attention as well. To my understanding, the transparent ABS will not exactly produce transparent prints but rather white-ish prints which can diffuse light. If you print just one…
Parents
  • celrobox
    celrobox over 11 years ago

    Hi Guys,

     

    I'm afraid we do not have any of this material set aside for samples or road tests right now. If we do this with future materials I will let you know!

     

    Andy, Nylon is a much tougher material than both ABS and PLA, it also generates less friction, so it is perfectly suited for things like gears or moving assemblies. If printed at a high infill some nylons are machinable post printing but I cannot comment on whether this will be possible with our nylon yet!

     

    I have printed with the woody beech but i'm afraid I don't have any pictures to hand. I'll try and get some for you today or monday!!

     

    IP, the crystal clear ABS is actually mABS, it has an acrylic added to the ABS to make it clear (abs is naturally creamy white). Solid parts are not entirely clear, but you can see the infill inside them. Parts printed with 0% fill and one perimeter come through as near clear, but not entirely see though. Apparently using a filler such as XTC-3D epoxy (XTC-3DRegistered High Performance 3D Print Coating | Bentley Advanced MaterialsBentley Advanced Materials) will bring single perimeter 0% fill parts to near enough clear.

     

    The thermochrome materials are most exciting me with wearables, such as watch straps or jewelry that change color depending on environment!

     

    Cheers,

    Simon

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ipv1
    ipv1 over 11 years ago in reply to celrobox

    Too bad. It would have made for a fun exercise. image

    Maybe in the future, there would be some available for us minions to experiment with. My Robox uses a green filament and the results were pretty awesome. I tried some third party clear filament but t like you said a layer or two come out transparent and then starts to become milky after that thickness. I guess its more of an art about what materials and how thick.

     

    I am making a double helix with RGB leds and will print it in clear ABS to get some good effects. Will post pictures when I do.

    Cheers,

    IP

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to ipv1

    I'd like to play with some translucent materials, Faberdashery do some that you can buy in 10m lengths. First to print myself a reel http://www.thingiverse.com/thing:547553/ (unless Robox can sell me one)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • celrobox
    celrobox over 11 years ago in reply to Workshopshed

    Unfortunalty when using an FFF printer to 3D print with clear materials, its quite difficult to get them completely clear, this is due to the way light passes through each layer. Using the larger (0.8mm) nozzle on draft mode on the Robox will improve this, as the more cylindrical the bead of filament, the less refractions occur as the light passes through the material.

     

    I have seen a few clear parts printed with intended LED use, and even though the part is milky, the LED light passes through with quite a nice 'warm' glow dispersed through the part.

     

    Andy, Unfortunatly Farnell don't stock them, but it is possible to buy an empty smart reel from the CEL store (Empty Filament Reel with blank EEPROM - RBX01-RL - Filament). You can then create your own material profile and write it to the reel so its ready to go every time, as soon as it is installed. You can re write this reel multiple times.

     

    Cheers,

    Simon

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 11 years ago in reply to celrobox

    Thanks both useful things to know

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 11 years ago in reply to celrobox

    Thanks both useful things to know