3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum UV LED display
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 340 subscribers
  • Views 685 views
  • Users 0 members are here
  • help
  • 3d
  • uv
  • etcetera
  • led
  • sla
  • stuff
  • printing
Related

UV LED display

fuzion_reaktor
fuzion_reaktor over 12 years ago

Hello element 14 people, I am here to ask you a question regarding LCD displays. I am currently trying to replace the back-light with UV LEDs in an attempt to build a miniature SLA 3D printer like the kick-starter project iBox nano. What I am having trouble with is figuring out how to run the LEDs properly. I could leave them on continuously and have them powered by a generic power supply rather than the LCD, but having the ability to control the LEDs will be very useful if not a necessity. I probably could just replace the back-light LEDs with the UV ones but they are the wrong sizes and I need them to be much more powerful. Is there a way I could use the back-light as a signal to activate a separate circuit for the UV LEDs, or a way I could amplify the power from the back-light so as to run the UV LEDs properly? I'd give you specifics on the voltages and currents involved here but I don't yet have the LEDs or display (display is a generic 3.5" composite input unit). I'm more curious if this is possible to do relatively simply, or whether or not it could be too complicated or destroy my LCD (and hopes and dreams).

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • fuzion_reaktor
    fuzion_reaktor over 12 years ago

    Apologies the voltages involved are

     

    1 * UV LED(1) 3.2-3.8V forward voltage, 600-700ma, just one

    OR

    1 * UV LED(2) same as one but 700ma+

    OR

    10-25 * UV LED(3) 3.0-3.2V forward voltage, 20ma, 5v reverse voltage, 10ua reverse current

     

    LCD: 3 5" TFT LCD Color Screen Car Rear View Monitor DVD DVR for Car Backup Camera | eBay (I'm not sure exactly what LCD is in it)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • fuzion_reaktor
    fuzion_reaktor over 12 years ago

    Apologies the voltages involved are

     

    1 * UV LED(1) 3.2-3.8V forward voltage, 600-700ma, just one

    OR

    1 * UV LED(2) same as one but 700ma+

    OR

    10-25 * UV LED(3) 3.0-3.2V forward voltage, 20ma, 5v reverse voltage, 10ua reverse current

     

    LCD: 3 5" TFT LCD Color Screen Car Rear View Monitor DVD DVR for Car Backup Camera | eBay (I'm not sure exactly what LCD is in it)