3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Multi use machine.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 341 subscribers
  • Views 1048 views
  • Users 0 members are here
  • multi
  • use
  • machine
Related

Multi use machine.

e14 Contributor
e14 Contributor over 11 years ago

Hi,

 

I am trying to build a multi use machine that is able to do:-

 

1. 3D printing.

2. spindle engraving/milling of soft wood.

3. laser cutting/engraving.

 

at the moment i am almost finished the main mechanical parts and i am getting ready to install the electronics, my main problem is that from what i see on the net almost all mills/engravers are run via Mach3 and most 3D printing is done via Rep Rap, I have both of the boards available to me and was going to install both of them and then just unplug the one i was not using but i would like to be able to just install one system for all usages which i think will have many less faults than installing both which is the only way i can think of at the moment, does anyone have any ideas as to how i can do it with just one system?

 

 

regards Poppy Ann.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bradnorwood +2
    Hi Brad, I would love to build 3 machines but I live in a small one bedroom bungalow and just do not have the room to have three of them, I have been thinking of either building a decent size shed in the…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bradnorwood +1
    Hi Brad, I was not going to mount all three heads at the same time I was going to make it so I fit the required head as needed but even if I fitted three at the same time the motor I have along with the…
  • bradnorwood
    bradnorwood over 11 years ago in reply to bradnorwood +1
    One of the cool things about a 3d printer is you have an opportunity to make parts for the printer, what would be neat is to make a circle or ring that held all 3 tools and could be rotated by motor or…
Parents
  • bradnorwood
    bradnorwood over 11 years ago

    You should make some posts and pictures of your progress, sounds interesting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bradnorwood
    bradnorwood over 11 years ago in reply to bradnorwood

    One of the cool things about a 3d printer is you have an opportunity to make parts for the printer, what would be neat is to make a circle or ring that held all 3 tools and could be rotated by motor or hand.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bradnorwood

    Hi Brad, I sort of got mixed up with my posts i just posted some photos of the machine but i put them in a different discussion, you can see them here:- How do you program the 3D printers

     

    hope these give you some idea of what it looks like i may modify it as i have been thinking of making it a moving table machine and not a moving gantry machine as i have built it but i only get coverage of around half of the table the way it is but if i alter it i can get to be able to use all of the table i expect that for a 3d printer it should be ok as it still has a decent size print area.

     

    regards Poppy Ann.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to bradnorwood

    Hi Brad, I sort of got mixed up with my posts i just posted some photos of the machine but i put them in a different discussion, you can see them here:- How do you program the 3D printers

     

    hope these give you some idea of what it looks like i may modify it as i have been thinking of making it a moving table machine and not a moving gantry machine as i have built it but i only get coverage of around half of the table the way it is but if i alter it i can get to be able to use all of the table i expect that for a 3d printer it should be ok as it still has a decent size print area.

     

    regards Poppy Ann.