3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum how to make the filament extrude and stick to the hot bed w/ a i2 printer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 341 subscribers
  • Views 653 views
  • Users 0 members are here
Related

how to make the filament extrude and stick to the hot bed w/ a i2 printer

e14 Contributor
e14 Contributor over 11 years ago

I'm having problems with making prints. I have a i2 printer and the filament won't extrude and when it comes out its only a little bit or it skips. The filament won't stick to the bed either. Can anyone advice on what I need to do . Thanks

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 11 years ago +2
    The bed on my printer is made from PEI (polyetherimide) thermoplastic probably made by Ultem. This bed material does not need any surface treatment to work. When the bed is heated to 65 degrees, the printer…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    You should definitely go through the checklist by Cheung Weng. Filament jamming is common. Based on the checklist, the following would be how I typically go about troubleshooting for my printer usually.

     

    Just to build on the checklist for points 1-4:

    1. Check if the distance between nozzle and hot bed is too close.

    - Ensure your print bed is clean. Put a piece of A4 paper under the nozzle. Home Z. Once the nozzle comes down, move the A4 paper around a bit. Adjust the z-axis until the paper the paper and slide with minimum effort.

    2. Raise the temperature of extruder.

    - Extrude filament for 10mm. If it is extruding properly, then wait 5-10 mins. Try again. Then retract the filament to check if the end has more than 5mm which is still soft, the nozzle may be too hot. Having an extruder fan will help in this situation. Once you start printing, the temperature may need to be readjusted.

    3. Check if the nozzle is jammed.

    - If nozzle is jammed, if filament is pla, I would typically change the nozzle or us that nozzle for other higher temperature filament such as nylon. At high temperature, the pla would melt and be extruded together with nylon when I start the flushing process. For ABS, there are some chemicals which you can use to melt it away.

    4. Check if the extruder motor driver is fine.

    - There may be a case where due to insufficient cooling, either your motor is too hot or stepper driver is too hot.

     

    For warping or filament not sticking to heatbed after everything else is remediated, I typically use glue stick and do without heatbed for low temperature materials. In somecases, I would use glue stick in combination with heatbed to increase the "sticking". if you still want to use heat bed, do ensure your power supply is sufficient as heatbed draws a lot of current.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    You should definitely go through the checklist by Cheung Weng. Filament jamming is common. Based on the checklist, the following would be how I typically go about troubleshooting for my printer usually.

     

    Just to build on the checklist for points 1-4:

    1. Check if the distance between nozzle and hot bed is too close.

    - Ensure your print bed is clean. Put a piece of A4 paper under the nozzle. Home Z. Once the nozzle comes down, move the A4 paper around a bit. Adjust the z-axis until the paper the paper and slide with minimum effort.

    2. Raise the temperature of extruder.

    - Extrude filament for 10mm. If it is extruding properly, then wait 5-10 mins. Try again. Then retract the filament to check if the end has more than 5mm which is still soft, the nozzle may be too hot. Having an extruder fan will help in this situation. Once you start printing, the temperature may need to be readjusted.

    3. Check if the nozzle is jammed.

    - If nozzle is jammed, if filament is pla, I would typically change the nozzle or us that nozzle for other higher temperature filament such as nylon. At high temperature, the pla would melt and be extruded together with nylon when I start the flushing process. For ABS, there are some chemicals which you can use to melt it away.

    4. Check if the extruder motor driver is fine.

    - There may be a case where due to insufficient cooling, either your motor is too hot or stepper driver is too hot.

     

    For warping or filament not sticking to heatbed after everything else is remediated, I typically use glue stick and do without heatbed for low temperature materials. In somecases, I would use glue stick in combination with heatbed to increase the "sticking". if you still want to use heat bed, do ensure your power supply is sufficient as heatbed draws a lot of current.