3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum 5v arduino regulator friend after installing jumper caps
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 340 subscribers
  • Views 1012 views
  • Users 0 members are here
Related

5v arduino regulator friend after installing jumper caps

e14 Contributor
e14 Contributor over 10 years ago

right after I set up the jumper caps under each motor driver and the extra fifth place for a motor driver, although I do not have a fifth motor (I am confident i put them in the right way), i fried the 5v regulator in the Arduino mega 2560 after connecting the 12V power supply, and i think it also ruined the RAMPS board. I think this because I purchased a new Arduino, downloaded the firmware, and after connecting it to the RAMPS board, it wont turn on. I think this is because i tried calibrating the voltage of each motor driver (via the trimpot) before putting on the jumper caps. Could that have been the reason that the 5v regulator burned? Thank you again for your help.

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    I would have thought with a stepper controller added to an Arduino Mega, it would be powered seperatly, you description makes me think you where trying to power it from the same power as the Arduino.


    Can you confirm how everything was connected

     

     

    Not having hte caps that you describe should not have fried anything on the arduino but as John has said, too much load and the fact that the regulator will be dissipating a lot of heat dropping 12V down to 5V when under load (Several watts) it may have over heated but nornally they would simply shut down till things cool off

     

    Was this a genuine Arduino MEGA or a cheap clone ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    I would have thought with a stepper controller added to an Arduino Mega, it would be powered seperatly, you description makes me think you where trying to power it from the same power as the Arduino.


    Can you confirm how everything was connected

     

     

    Not having hte caps that you describe should not have fried anything on the arduino but as John has said, too much load and the fact that the regulator will be dissipating a lot of heat dropping 12V down to 5V when under load (Several watts) it may have over heated but nornally they would simply shut down till things cool off

     

    Was this a genuine Arduino MEGA or a cheap clone ?