3D Printing
  • Technologies
  • More
3D Printing
3D Printing Forum Hi I'm having some problem with my 3d printer
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join 3D Printing to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 6 answers
  • Subscribers 347 subscribers
  • Views 2657 views
  • Users 0 members are here
  • stl
  • problem_solving
  • help!
  • 3d print
Related

Hi I'm having some problem with my 3d printer

mads391i
mads391i over 9 years ago

Hi I've just bought a cheap Chinese 3d printer.

When I connect printer to my computer it comes to life (all lights are blinking and motors move on spot a bit) but when I try to print cura says detecting baud rate and nothing happens. I'm using windows 10 if that matters; also tried with my mac didn't help. It is a ctc dual-extruder 3d printer.

I've read that should make change something about Marlin but I don't know anything about it.

 

Specs on 3d printer if you need:

Electronics

· CTC Board single-piece motherboard

· 5 axis, 1/16 micro-stepping motor control

· 4x20 LCD character display and multi-direction control pad

· Universal Power Supply: 100-240V, 50/60Hz

Software: ReplicatorG

· Compatibility: Windows.

· Print from SD card or over USB

· Input file type: STL, gcode,x3g

  • Sign in to reply
  • Cancel

Top Replies

  • awardautomation
    awardautomation over 9 years ago +3 suggested
    Can you give more details about the "motherboard"? What markings are on the main microprocessor? If you are unsure, post a photo of it. If it uses an atmel chip, chances are good its arduino compatible…
  • fvan
    fvan over 9 years ago +2 suggested
    "Marlin" is the firmware used by some 3D printers. Typically, this is flashed on an Arduino compatible chip on the printer's control board. Could you be more detailed about: I've read that should make…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to awardautomation +2 suggested
    Also good to know where the printer was bought and what is the original brand. Most of the cheap Chinese sellers are resellers as gearbest. Enrico
Parents
  • danielw
    0 danielw over 9 years ago

    Just a few thoughts...

     

    Is there a suitable driver for the serial port on your PC?  I had an Arduino clone a few years back and I had to download a serial driver for it as the standard serial drivers wouldn't see it?

     

    Have you got replicator G working?  Looking at replicator G it can control a Makerbot.  So maybe change the G code Flavour in Cura to makerbot and see if that gets it to connect.

     

    If you haven't, Try Replicator G just to see if it'll spring into life... ReplicatorG is a simple, open source 3D printing program - ReplicatorG

     

    I've included a couple of links below to CTC Printer.  Do these look anything like your machine?

    http://www.ctcprinter.com/product_list.php

    http://www.ctcprinter.com/product_detail.php?ProId=32

     

    On the second link (product pages for one of the printers) it says to install Python and Replicator G

    It also seems to have  a support section.

     

    I would also suggest If you slice and put GCode on an SD card will it print? But if you don't have the g-code flavour right it'll produce odd, and I suppose potentially, disastrous results if it tries to do something it can't..

     

    I don't have a CTC printer but this  is the sort of thing I'd do for any machine I was trying to get going.

     

    Dan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • danielw
    0 danielw over 9 years ago

    Just a few thoughts...

     

    Is there a suitable driver for the serial port on your PC?  I had an Arduino clone a few years back and I had to download a serial driver for it as the standard serial drivers wouldn't see it?

     

    Have you got replicator G working?  Looking at replicator G it can control a Makerbot.  So maybe change the G code Flavour in Cura to makerbot and see if that gets it to connect.

     

    If you haven't, Try Replicator G just to see if it'll spring into life... ReplicatorG is a simple, open source 3D printing program - ReplicatorG

     

    I've included a couple of links below to CTC Printer.  Do these look anything like your machine?

    http://www.ctcprinter.com/product_list.php

    http://www.ctcprinter.com/product_detail.php?ProId=32

     

    On the second link (product pages for one of the printers) it says to install Python and Replicator G

    It also seems to have  a support section.

     

    I would also suggest If you slice and put GCode on an SD card will it print? But if you don't have the g-code flavour right it'll produce odd, and I suppose potentially, disastrous results if it tries to do something it can't..

     

    I don't have a CTC printer but this  is the sort of thing I'd do for any machine I was trying to get going.

     

    Dan.